For Immediate Release

Vicor Corporation Introduces High Density AC-DC Front-End Power Module

VI BRICK® AC Front End module delivers an isolated, PFC regulated, 330W 48V output in a business card size footprint

001x001px_alpha.png
001x001px_alpha.png
001x001px_alpha.png

pr-ac-front-end-module.jpgElectronica 2012 – Munich, Germany – November 12, 2012 – Vicor Corporation (NASDAQ: VICR) today announced the
VI BRICK® AC Front End module for high, density, high efficiency AC to DC power conversion. This new module is a complete AC–DC converter which operates over the universal AC input range of 85-264 V to deliver a fully isolated and PFC regulated 48 V output. In a low profile package measuring 3.75 x1.91 inches (95.3mm x 48.6mm) and only 0.38 inches (9.55 mm) in height, the AC Front End module provides a power conversion density of 121 W/in3 (7.5W/cm3) or 54 W/in3 for a complete supply that includes all necessary components including hold-up capacitance.

 

Every electronic product or system that operates off of an AC utility line must incorporate an AC-DC front-end to convert the AC utility voltage into the smooth DC voltage required by electronic circuitry. As the “firewall” between the utility and the customer’s electronics, a contemporary front-end must perform complex tasks – such as power factor correction and noise reduction – to meet the stringent requirements of international regulatory agencies. The Vicor AC Front End module, with its integrated rectification, filtering and transient protection, enables customers to configure a complete front end system that meets IEC 61000-3-2 harmonic noise and Class B EMI conducted emission limits supplying 330W to external output storage capacitance. Its comprehensive performance features give customers the ability to simplify their regulatory certification processes and streamline their power system designs.

 

With its proprietary Double-Clamp ZVS high switching frequency topology, the AC Front End module achieves consistently high efficiency – up to 92% – across its entire AC input voltage range, including operation down to 85VAC and cuts power losses by more than 50% compared to competing offerings. The AC Front End also simplifies the customers’ cooling requirements, reducing both the size and cost of cooling components.

 

“From the wall plug to the point of load, Vicor provides low profile, high density, high efficiency power components that enable the most versatile and tightly-integrated power systems on the market today,” said Rob Russell, Vice President, Brick product line, Vicor. “This AC Front End module based on performance-proven VI Chip technology now expands Vicor’s brick product line into AC-DC applications.”

 

The new VI BRICK® AC Front End module is compatible with a wide variety of downstream DC–DC power conversion components including Vicor’s comprehensive portfolio of high-density, high efficiency, VI Chip and VI BRICK converters. When used with downstream DC–DC converters which support secondary-side energy storage and efficient power distribution, the AC Front End module provides superior power system performance and connectivity from the wall plug to the point of load and enables customers to design reliable and cost-effective power systems.

 

Electronica 2012 attendees can visit Vicor in Hall A6 at Stand 560.

 

Availability & Supporting Resources
Vicor’s new VI Brick AC Front End modules will be available to customers in consumer (-20°C to 100°C), telecom (-40°C to 100°C) and military (-55°C to 100°C) temperature grades. For preliminary datasheet and other technical documentation, visit Vicor. The product will be available through distribution at the end of the year. For pricing information and sample availability, email custserv@vicr.com or call 1-800-735-6200.
001x001px_alpha.png
001x001px_alpha.png
PR-Wordmark-301.jpg
 
Follow Vicor on Social Media
Twitter: @VicorPower »
Vicor Corporation on LinkedIn »
Vicor PowerBlog »
001x001px_alpha.png

About Vicor Corporation
Headquartered in Andover, Massachusetts, Vicor Corporation designs, manufactures and markets innovative, high-performance modular power components, from bricks to semiconductor-centric solutions, to enable customers to efficiently convert and manage power from the wall plug to the point of load. Complementing an extensive portfolio of patented innovations in power conversion and power distribution with significant application development expertise, Vicor offers comprehensive product lines addressing a broad range of power conversion and management requirements across all power distribution architectures, including CPA, DPA, IBA, FPA™ and CBA. Vicor focuses on solutions for performance-critical applications in the following markets: enterprise and high performance computing, telecommunications and network infrastructure, industrial equipment and automation, vehicles and transportation and aerospace and defense electronics. www.vicorpower.com

###

Vicor and FPA are trademarks of Vicor Corporation.


Contact
Colin Boroski
Rainier Communications
508-475-0025 x 142
cboroski@rainierco.com