For Immediate Release

Vicor Corporation to Showcase New Innovations in Power Management at Electronica China 2013

New product announcements and solution demonstrations spanning from AC to Point of Load on tap from Vicor at booth E1.1412

001x001px_alpha.png
001x001px_alpha.png

Shanghai, China – March 7, 2013 – Vicor Corporation (NASDAQ: VICR) today announced its participation in Electronica China 2013, the international trade fair for electronic components, systems and applications, hosted at the Shanghai New International Expo Centre, March 19 - 21. Among the highlights planned for Electronica China 2013, Vicor will unveil the newest additions to its portfolio of high- performance, high-efficiency power management solutions, and host demonstrations designed to showcase the latest innovations in power electronics from AC to the Point of Load.

 

At Vicor’s booth, attendees can visit with Vicor’s expert team of power management architects to learn more about solutions and trends such as 400 Vdc bus conversion solutions for high-voltage power distribution, enhancements to Vicor’s Factorized Power Architecture™ (FPA™) for current multiplication at the point of load, and Zero-Voltage Switching (ZVS) point-of-load DC-DC regulation.

 

Among the Vicor products in the spotlight at Electronica China 2013 will be its VI Brick® AC Front End™ module for high-density, high-efficiency AC-DC power conversion, operating over the universal AC input range of 85 – 264 V to deliver a fully isolated and PFC regulated 48 V output in a low profile package measuring 95.3 mm x 48.6 mm and only 9.55 mm in height. Vicor’s award-winning Picor® Cool-Power® ZVS Buck Regulator product line for high-efficiency point-of-load DC-DC regulation will also be featured, alongside exciting new Vicor products and technologies to be unveiled publically at the event.

 

Electronica China 2013 attendees can visit Vicor in booth E1.1412. To schedule a meeting with Vicor at the event, please visit Vicor’s website.

 

Electronica China is one of the world's leading conferences for technology components, systems and applications, drawing a high volume of exhibitors and attendees from around the globe. For more information about Electronica China 2013, visit http://electronica-productronica-china.com/

 

 

001x001px_alpha.png
001x001px_alpha.png
PR-Wordmark-301.jpg
 
Follow Vicor on Social Media
Twitter: @VicorPower »
Vicor Corporation on LinkedIn »
Vicor PowerBlog »
001x001px_alpha.png

About Vicor Corporation
Headquartered in Andover, Massachusetts, Vicor Corporation designs, manufactures and markets innovative, high-performance modular power components, from bricks to semiconductor-centric solutions, to enable customers to efficiently convert and manage power from the wall plug to the point of load. Complementing an extensive portfolio of patented innovations in power conversion and power distribution with significant application development expertise, Vicor offers comprehensive product lines addressing a broad range of power conversion and management requirements across all power distribution architectures, including CPA, DPA, IBA, FPA™ and CBA. Vicor focuses on solutions for performance-critical applications in the following markets: enterprise and high performance computing, telecommunications and network infrastructure, industrial equipment and automation, vehicles and transportation and aerospace and defense electronics. www.vicorpower.com

###

Vicor and FPA are trademarks of Vicor Corporation.


Contact
Colin Boroski
Rainier Communications
508-475-0025 x 142
cboroski@rainierco.com