For Immediate Release

Vicor Corporation’s High Voltage ChiP BCM Named Power System Product of the Year at Elektra Awards

Elektra European Electronics Industry Awards recognize leading product and technology innovation

001x001px_alpha.png
001x001px_alpha.png
001x001px_alpha.png

Andover, MA – December 5, 2014 – Vicor Corporation (NASDAQ: VICR) today announced that its high voltage Bus Converter Module (BCM®) based on the Converter housed in Package (ChiP) platform was named by the organizers of the Elektra Awards as the Power System Product of the Year, 2014.

 

The Elektra European Electronics Industry Awards, organized by Electronics Weekly, celebrate the achievements and contributions of individuals and companies to the European electronics industry. Vicor’s ChiP BCM was recognized for its outstanding electrical performance that enables engineers to simplify the design and increase the energy efficiency in applications such as datacenters by distributing power using high voltage DC (HVDC).

 

ChiP packaging technology enables a new generation of ultra-high density, thermally-adept power components by leveraging Vicor’s world-class power expertise and manufacturing capabilities. The ChiP BCM converts an input voltage of 260 to 410 V to a 50 V output at 1.75 kW, with 98% peak efficiency. With a power density of 2750 W/in3 (167 W/cm³), the ChiP BCM delivers five times the performance of competing solutions, enabling customers to achieve previously unattainable system size, weight and efficiency targets.

 

The award winners were announced on November 26 at a gala ceremony in London, UK. Vicor’s PowerBench® Whiteboard was also recognized, shortlisted in the Design Tools and Development Software category.

 

001x001px_alpha.png
001x001px_alpha.png
001x001px_alpha.png
PR-Wordmark.jpg
 
Follow Vicor on Social Media
Twitter: @VicorPower »
Vicor Corporation on LinkedIn »
Vicor PowerBlog »
001x001px_alpha.png

About Vicor Corporation
Headquartered in Andover, Massachusetts, Vicor Corporation designs, manufactures and markets innovative, high-performance modular power components, from bricks to semiconductor-centric solutions, to enable customers to efficiently convert and manage power from the power source to the point of load. www.vicorpower.com

###

Vicor, BCM and PowerBench are trademarks of Vicor Corporation.


Contact
Colin Boroski
Rainier Communications
508-475-0025 x 142
cboroski@rainierco.com