What is the difference between remote and local sense?
Do the Vicor modules need a heat sink?
What is PFC, and what does it mean to me?
Why can't I use a MI-IAM (Input Attenuator Module i.e., MI-A22-MU) with a VI-200 DC-DC converter
(i.e., VI-2W0-MW)?
Can I solder wires directly to the pins of the Vicor module? And if not, what products can I use for
direct wire connections?
If I am not using the Gate In, Gate Out, or Trim pins on VI-200 / VI-J00 converters and the PC, PR
or SC on the Maxi, Mini and Micro converters, can I leave them floating?
Do I need filtering on the input and/or output side of the power converters?
Can the Three-Phase MegaPAC operate from a single-phase input?
Why does the output power decrease if I trim the output voltage down?
What is the switching frequency of your VI-200 / VI-J00 and Maxi, Mini and Micro converters?
Do your modules load share?
Power conversion modules generally require bypass capacitors from line to chassis (earth ground) to meet Agency EMI Standards by shunting common-mode noise currents and keeping them local to the converter. In cases where the converters are operating from rectified AC line voltage, the failure of a bypass capacitor could result in excessive leakage current to the equipment chassis, thus creating a ground fault and shock hazard. For this reason, a special classification of capacitor, referred to as a "Y-capacitor" is recommended. These capacitors contain a dielectric with unique "self healing" properties to help prevent against excessive leakage.
To meet general EMI/RFI requirements, Vicor recommends the use of Y-capacitors with all power conversion modules. Y-capacitors meet IEC384-14, EN132400 and UL1283 standards.
All applications utilizing DC-DC converters should be properly bypassed, even if no EMC standards need to be met. Bypass power input and output pins to each module baseplate. Lead length should be as short as possible. Recommended values vary depending on the front end, if any, that is used with the modules. In PC board-mount applications, each of these components is typically small enough to fit under the module baseplate flange.
Vicor sells its products through a network of 29 independent sales representative organizations in North and South America; internationally, 52 independent distributors are utilized. Sales activities are managed by a staff of Regional and Strategic Sales Managers and sales personnel based at the Company’s world headquarters in Andover, Massachusetts, its Westcor division in Sunnyvale, California a Technical Support Center in Lombard, Illinois, in VIA locations in Oceanside, California and Cedar Park, Texas and in its Technical Support Center subsidiaries in Munich, Germany; Camberley Surrey, England; Milan, Italy; Paris, France; Hong Kong and Tokyo, Japan.
Top »Local Sense involves using the power supply output power terminals as the sense points to provide feedback to the internal voltage regulation circuitry. Remote sense involves detection of output voltage at a point remote from the power supply, enabling the power supply to regulate output voltage and to compensate for voltage drop typically associated with long power cables. This permits greater accuracy of regulation than local sensing. The sense connections (from the sense pins) determine the regulation point, either at the converter output (local sense) or at the load (remote sense) to compensate for voltage drop. It is important to "close" the sense lines, i.e., +S to +Out, -S to –Out, as described above for proper operation of the module; and it is an absolute MUST for Maxi and Mini modules.
Top »This depends on a variety of factors within the application such as the maximum ambient temperature specific to the module’s location, availability of forced convection cooling, loading characteristics and the converter’s efficiency. It is important to note that the advantage of a baseplated module versus the limitation of the open frame or bare-board converters is the flexibility of easily adding a heat sink to the baseplated module if needed.
Top »Today’s electronic devices present a non-linear load to the ac source; that is, they do not draw a sinusoidal current when supplied from a sinusoidal voltage. The phase relationship between voltage and current may be very close but the shape of the current waveform differs greatly from the shape of the voltage waveform. This also results in a higher apparent power and a correspondingly reduced power factor. However, since there is no significant phase difference, the power factor can-not be said to be either lagging or leading.
Active Power Factor Correction (PFC) is the technique of controlling the current flow into the device to track the applied voltage waveform. A specific example of a non-linear load is a line-operated switching power supply with a capacitor input filter. This type of load draws no current until the line voltage is near the peak; then draws a large pulse of current as the voltage passes through the waveform peak. Power Factor Correction (PFC) would require the power supply to force the input current to have the same wave shape as the ac voltage source.
Advantages of PFC switching power supplies with a boost converter are: reduced input current for a given load power, improved ride-through energy storage because the energy storage capacitor is always charged to the maximum voltage, 85 – 264VAC operation without re-strapping the input, and compliance with EN61000-3-2. For additional information regarding PFC please see the Applications Notes section of the Vicor web site.
Recently, Amendment 14 to EN61000-3-2 was issued. One of the effects of this amendment was to reclassify AC-DC power supplies from Class D to Class A. Of significant importance in this reclassification is the elimination of the variable limit placed on harmonic currents. In its place, there is now a fixed limit based only on the maximum input power of the Class – which is 1,000 watts. Since, in effect, AC-DC power supplies drawing less than 1,000W have had their harmonic current limit increased, there are now alternatives to active PFC for achieving EN compliance. The most simple, robust, reliable and inexpensive method of harmonic current reduction can now be employed in many lower power systems – passive attenuation.
Another major advantage of this passive method is that, as the nomenclature implies, it doesn’t rely on active components – which contribute to a system’s EMI level – so it acts as additional line filtering that actually improves system EMI performance. The “passive alternative”: smaller, simpler, cleaner, cheaper is available as Vicor’s ENMods or Westcor’s FlatPAC-EN. Although passive harmonic current attenuation can improve power factor to about 0.8, it doesn’t approach the near unity power factor of active PFC implementations such as Vicor’s VI-HAM or Westcor’s LoPAC Family.
Top »The primary reason is related to input voltage range compatibility, i.e., the MI-A22-MU is designed for 18 – 50 V operation and the VI-2W0-MW is designed for 18 – 36 V operation, this is a critical difference especially for input transient protection. With respect to EMI / RFI, the obvious impact of the input range mismatch has prevented this filter from being offered with this converter and thus performance has not been characterized to the MI-IAM’s published specifications and as such, cannot be guaranteed.
Top »Vicor does not recommend direct wire connections to the module pins of it’s converters as the mechanical loading and thermal stress from bench soldering may cause potential reliability concerns. The modules are intended to be used in PCB applications with controlled soldering techniques per the Soldering Methods and Procedures Application Note. If chassis mounting is preferred Vicor offers packaging options for the VI-200/VI-J00 Series (MI-200/MI-J00) as BusMod, MegaMod or ComPAC products and for Maxi, Mini and Micro converters with VIPAC Arrays and VIPACs, which will facilitate discrete wire connections.
Top »This depends on how the converters are being applied; however, some applications do not require the functionality that these pins provide. Hence these pins can be left as a "no connect". See the Vicor Applications Manual and Maxi, Mini and Micro Design Guides for more information.
Top »All switching power supplies generate signals that could potentially interfere with other electronic circuits as a result of the switching action. Vicor’s quasi-resonant, zero-current-switching topology generates far less conducted and radiated noise than other topologies in both magnitude and frequency spectrum. EMI filtering can reduce the noise by an additional 40 – 60 dB. Depending upon your application, additional filtering may be needed to meet agency and/or load requirements. Some basic guidelines to follow for successful EMI filtering are:
Vicor power converters have isolated outputs so they can be referenced to a common node creating either positive or negative rails. To create a negative 5 V output for example, the +Out of the module would be connected to the common return (earth ground, chassis ground, etc). The -Out would then be treated as the "supply".
Top »The Three-Phase MegaPAC can be powered from a single-phase source as long as the input voltage is between 180 – 264 Vac. Although it is possible to connect the Line and Neutral wires to any of the J1 Line inputs, the most common wire scheme is listed below. For safety purposes, it is important to first verify that the input circuit is OFF, before handling any of the input wires. After confirming there is no input voltage on the wires, configure the J1 Input Power Connector as shown below.
Please refer to the Three-Phase / 4 kW MegaPAC Design Guide for information regarding single-phase power deratings.
Top »Vicor power converters have a fixed output current limit. The output power rating divided by the rated output voltage (Po/Vo) is the rated output current (Io). Since the maximum current is fixed, a reduction in voltage reduces the output power. For example, a 5 V / 50 W module can deliver 10 A. If the converter’s output voltage is trimmed down to 2.5 V, the converter can still only deliver up to a 10 A maximum; therefore, the available maximum power is now 25 W.
Top »Vicor VI-200 / VI-J00 and Maxi, Mini and Micro power converters use frequency modulated, quasi-resonant, zero-current switching in contrast to the pulse-width-modulated (PWM) switchers. As such, the operating frequency is both input line and output load dependant, and could range from under 100 kHz at light load, high line, to around 1 MHz at full load, low line. As a result, Vicor’s zero-current switching has much lower conducted and radiated noise levels than conventional pulse-width-modulation (PWM) converters, typically 20 – 40 dB lower.
Top »Another aspect of the Vicor topology is that two or more power trains driven at the same frequency will inherently load share if their outputs are tied together. Load sharing is dynamic and guaranteed to be within a few percent. The VI-200 family has associated booster modules, VI-Bxx-xx (designated with the same input voltage range, output voltage and power level as the associated Driver, VI-2xx-xx). Booster modules may be slaved to a Driver, allowing construction of multi-Kilowatt arrays. Only a single connection is needed between converters with all converter outputs connected together; no trimming or adjustments are required to achieve load sharing. This is documented in more detail in the Vicor Applications Manual.
Vicor’s Maxi, Mini and Micro power converters have the capability of being configured in a fault-tolerant, power sharing "democratic" array. Maxi, Mini and Micro power converters can be configured into arrays in which each power converter naturally shares in the power delivered to the load. The arrays are inherently "democratic" in the sense that the "master" module (which provides synchronous control of the array) is automatically determined without any user intervention whatsoever. Furthermore, the array is inherently "N+M" fault tolerant: uninterrupted synchronous operation will continue despite any number of modules failing or being taken off-line, provided only that as the remaining modules in the array have sufficient aggregate power capability to support the load. Configuring the array is extremely simple, consisting of low voltage, capacitively coupled, connections between converter modules. For additional information regarding parallel operation of our Maxi, Mini and Micro converters, please see the Application Notes section of our web site.
Top »Safety agency conditions of acceptability require that the module (+) input terminal be fused and the baseplate of the converter be connected to earth ground. The location of the fuse must be in series with the positive (+) input lead. Fusing the negative input lead does not provide adequate protection as the PR and PC terminals of the Maxi, Mini and Micro converter (Gate In and Gate Out of the VI-200 / VI-J00 converters) are referenced to the –Input. If a fuse located in the –Input lead were to open, the PR and PC terminals (Gate In and Gate Out) would rise to the potential of the +Input. This could damage any converter or circuitry connected to these pins. The fuse should not be located in an area with a high ambient temperature, as this will lower the current carrying rating of the fuse.
Top »| Term | Acronym | Definition |
| AC-DC | Pertaining to electronic equipment capable of operation from either an alternating - current or direct current primary power source. |
|
| AC-DC CONVERTER | A device to convert alternating current to direct current. Often referred to as an off-line converter where the ac voltage is rectified to dc, perhaps including power factor correction or other processing.
|
|
| AC-OK Signal | The signal used to indicate the loss of AC input voltage from the 115/230V line. |
|
| ALTITUDE TESTING | Generally performed to determine the proper functioning of modules at specified altitudes. MIL-STD-810. |
|
| AMBIENT TEMPERATURE | The temperature of the environment, usually the still air in the immediate proximity of the power supply. |
|
| APPARENT POWER | A value of power for AC circuits that is calculated as the product of rms current times rms voltage, without taking power factor into account. |
| Bus Converter Module | BCM | A VTM V•I Chip that has been optimized for IBA applications. The BCM provides an isolated intermediate bus voltage to power niPOLs from a pre-regulated DC source. The BCM is superior in all respects to conventional brick-type IBCs. |
| BANDWIDTH | A range of frequencies over which a certain phenomenon is to be considered. |
|
| BASEPLATE | All modular products have an aluminum mounting base at which Vicor specifies operating temperatures and which should be affixed to a thermally conductive surface for cooling. |
|
| BELLCORE SPECIFICATION | A telecommunications industry standard developed by Bellcore. |
|
| B-IPOLAR TRANSISTOR | A transistor that operates by the action of minority carriers across a P/N junction; it is a current controlled device as opposed to a voltage controlled device. |
|
| BOBBIN | A device upon which the windings of a transformer or inductor are wound; it provides a form for the coil and insulates the windings from the core. |
|
| BOOSTER CONVERTER | A “slave” module in a driver/booster combination, connected to the driver module. Several boosters can be connected to a driver module. |
|
| BREAKDOWN VOLTAGE | A voltage at which dielectric insulation fails by excessive leakage current or arcing. In reference to power supplies, the breakdown voltage is the maximum AC or DC voltage that can be applied from input to output and/or chassis. |
|
| BRIDGE CONVERTER | A DC-DC converter topology (configuration) employing two or four active switching components in a bridge configuration across a power transformer. |
|
| BRIDGE RECTIFIER | A full–wave rectifier circuit employing four rectifiers in a bridge configuration. |
|
| BROWNOUT | A reduction of the AC mains distribution voltage, usually caused deliberately by the utility company to reduce power consumption when demand exceeds generation or distribution capacity. |
|
| BURN-IN | Operating a newly manufactured power supply, usually at rated load, for a period of time in order to force component infant mortality failures or other latent defects. |
| CANADIAN STANDARDS ASSOCIATION | CSA | Defines the standards and safety requirements for power components. |
| CAPACITIVE COUPLING | Coupling of a signal between two circuits due to discrete or parasitic capacitance between the circuits. |
|
| CENTER TAP | An electrical connection made at the center of a transformer or inductor winding, usually so as to result in an equal number of turns on either side of the tap. |
|
| C-GRADE | Industry standard where the operating temperature of a device does not drop below –20 degrees Celsius. |
|
| CHASSIS MOUNT CONFIGURATION | A configuration where the modules or AC front ends are mounted directly to the chassis. |
|
| COMMON–MODE NOISE | Noise present equally on two conductors with respect to some reference point; often used specifically to refer to noise present on both the hot and neutral AC lines with respect to ground. |
|
| COMPAC | A Vicor DC input power supply that provides EMC filtering and transient suppression for industrial, military, and telecommunications markets. |
|
| CONSTANT–CURRENT POWER SUPPLY | A power supply designed to regulate output current for changes in line, load, ambient temperature, and drift resulting over time. |
|
| CONSTANT–VOLTAGE POWER SUPPLY | A power supply designed to regulate output voltage for changes in line, load, ambient temperature, and drift over time. |
|
| CONTROL CIRCUIT | A circuit in a closed-loop system, typically containing an error amplifier, that controls the operation of the system to achieve regulation. |
|
| CONVERTER | An electrical circuit that accepts a DC input and generates a DC output of a different voltage usually achieved by high–frequency switching action and employing inductive and capacitive filter elements. |
|
| CREST FACTOR | In an AC circuit, the mathematical ratio of the peak to rms values of a waveform. Crest factor is sometimes used for describing the current stress in AC mains supply wires, since for a given amount of power transferred, the RMS value, and hence the losses, become greater with increasing peak values. Crest factor gives essentially the same information as power factor, and is being replaced by power factor in power supply technology. |
|
| CROSS REGULATION | The effect of a load change on one output to the regulation of another output. It usually applies only to non postregulated (quasi) outputs. |
|
| CROWBAR | An overvoltage protection method that shorts the power supply output to ground in order to protect the load when an overvoltage fault is detected. |
|
| CURRENT LIMITING | An overload protection circuit that limits the maximum output current of a power supply in order to protect the load and/or the power supply. |
|
| CURRENT MODE | A control method for switch-mode converters where the converter adjusts its regulating pulsewidth in response to measured output current and output voltage, using a dual loop control circuit. |
|
| CURRENT MONITOR | An analog power supply signal that is linearly proportional to output current flow. |
| EFFICIENCY | The ratio of total output power to input power expressed as a percentage. Normally specified at 75% full load and nominal input voltage. |
|
| ELECTRONIC LOAD | An electronic device designed to provide a load to the outputs of a power supply, usually capable of dynamic loading, and frequently programmable or computer controlled. |
|
| ELECTROMAGNETIC COMPATIBILITY | EMC | Relating to compliance with electromagnetic emissions and susceptibility standards. |
| ELECTROMAGNETIC INTERFERENCE | EMI | Unwanted noise generated during the operation of a power supply or other electrical or electronic equipment. |
| EQUIVALENT SERIES RESISTANCE | ESR | The value of resistance in series with an ideal capacitor that duplicates the performance characteristics of a real capacitor. |
| FACTORIZED BUS | Vf | An output voltage produced by a PRM or DC–DC converter, which can be controlled to stabilize or vary the output of one or more VTMs. |
| FACTORIZED POWER ARCHITECTURE | FPA | FPA is a novel power distribution architecture that separates the classic functions of a DC-DC converter, as typically used in Distributed Power Architecture systems, into independent regulation and isolation/transformation building blocks. Although, in its "pure" form, FPA would be implemented with a variety of V•I Chip, traditional power products, such as DC-DC converters, niPOLs and box switchers, can be part of an FPA system. |
| FAULT TOLERANT CONFIGURATION | A method of parallel operation, using output isolating diodes, in which the failure of a single supply (module) will not result in a loss of power. The total current of the parallel system must not exceed the load requirements to a point where the failure of a single unit will not result in a system overload. |
|
| FIELD EFECT TRANSISTOR | FET | A majority carrier-voltage controlled transistor. |
| FINMOD | A flangeless/finned packaging option available on Vicor’s VI / MI Family converters and accessory modules. |
|
| FLATPAC | A Vicor AC-DC switcher available with one, two or three outputs, with total power rating from 50 to 600W. |
|
| FLOATING OUTPUT | An output of a power supply that is not connected or referenced to any other output, usually denoting full galvanic isolation. Floating outputs can generally be used as either positive or negative outputs. Non floating outputs share a common return line and are hence DC referenced to one another. |
|
| FOLDBACK CURRENT LIMITING | A type of protection circuit where the output current decreases as the overload increases. The output current reaches a minimum as the load approaches a short circuit condition. |
|
| FORWARD CONVERTER | A switching power supply in which the energy is transferred from the input to the output during the “on” time of the primary switching device. |
| GATE IN | The Gate In pin of the module may be used to turn the module on or off. When Gate In is pulled low (<1 Volt @ 4 mA, referenced to –Vin), the module is turned off. When Gate In is floating (open collector) the module is turned on. The open-circuit voltage of the Gate In pin is less than 10 Volts, referenced to –Vin. A Gate In/Gate Out connection is necessary to run driver/booster configurations. |
|
| GATE OUT | The Gate Out pin is the clock pulse of the converter. It is used to synchronize booster modules to a driver module for high power arrays. |
|
| GROUND | An electrical connection to earth or some other conductor that is connected to earth. Sometimes the term “ground” is used in place of “common,” but such usage is not correct unless the connection is also connected to earth. |
|
| GROUND LOOP | An unintentionally induced feedback loop caused by two or more circuits sharing a common electrical ground. |
| HAVERSINE | A waveform that is sinusoidal in nature, but consists of a portion of a sine wave superimposed on another waveform. The input current waveform to a typical off-line power supply has the form of a haversine. |
|
| HEADROOM | Used in conjunction with series pass regulators, headroom is the difference between the input and output voltages. |
|
| HEATSINK | A medium of high thermal mass that can absorb (sink) heat indefinitely with negligible change in temperature. Heatsinks are not necessarily needed with Vicor modules, and their use is highly dependent on the individual application, power and ambient temperature. |
|
| HIGH LINE INPUT | The maximum steady-state input voltage on the input pin. |
|
| HIPOT | Abbreviation for high potential, and generally refers to the high voltages used to test dielectric withstand capability for regulatory agency electrical safety requirements. |
|
| HOLDUP CAPACITOR | A capacitor whose energy is used to provide output voltage for a period after the removal of input voltage. |
|
| HOLDUP TIME | The length of time a power supply can operate in regulation after failure of the AC input. Linears have very short holdup times due to the CV 2 energy storage product of their low voltage secondary side output capacitors. Switchers have longer times due to higher voltage primary side energy storage capacitors. |
|
| HOT SWAP | Insertion and extraction of a power supply into a system while power is applied. |
| I-GRADE | Industry standard where the operation temperature of a device does not drop below –40 degrees Celsius. |
|
| IMPEDANCE | The ratio of voltage to current at a specified frequency. |
|
| INDUCED NOISE | Noise generated in a circuit by varying a magnetic field produced by another circuit. |
|
| INPUT LINE FILTER | An internally or externally mounted lowpass or band-reject filter at the power supply input that reduces the noise fed into the power supply. |
|
| INRUSH CURRENT | The peak current flowing into a power supply the instant AC power is applied. This peak may be much higher than the steady state input current due to the charging of the input filter capacitors. |
|
| INRUSH CURRENT LIMITING | A circuit that limits the amount of inrush current when a power supply is turned on. |
|
| INTERMEDIATE BUS ARCHITECTURE | IBA | Typified by the distribution of a lower voltage generally produced at the board level by an IBC. Characterized by the use of niPOLs. |
| INTERMEDIATE BUS CONVERTER | IBC | Available from several manufacturers, an IBC is generally a brick converter providing an unregulated and isolated intermediate voltage from a pre-regulated DC bus. Typical intermediate voltages provided are 12, 8, 5 or 3 Vdc and typical loads are niPOLs. |
| ISOLATION | Two circuits that are completely electrically separated with respect to DC potentials, and almost always AC potentials. In power supplies, it is defined as the electrical separation of the input and output via the transformer. |
|
| ISOLATION VOLTAGE | The maximum AC or DC voltage that may be continuously applied from input to output and/or chassis of a power supply. |
| LEAKAGE CURRENT | A term relating to current flowing between the AC supply wires and earth ground. The term does not necessarily denote a fault condition. In power supplies, leakage current usually refers to the 60 Hz current that flows through the EMC filter capacitors connected between the AC lines and ground (Y caps). |
|
| LINEAR REGULATOR | A regulating technique where a dissipative active device such as a transistor is placed in series with a power supply output to regulate the output voltage. |
|
| LINE REGULATION | The change in output voltage when the AC input voltage is changed from minimum to maximum specified. |
|
| LINE VOLTAGE (Mains) | The sine wave voltage provided to the power supply, usually expressed in volts rms. |
|
| LOAD REGULATION | The change in output voltage when the load on the output is changed. |
|
| LOCAL SENSING | Using the voltage output terminals of the power supply as sense points for voltage regulation. |
|
| LONG TERM STABILITY | Power supply output voltage change due to time with all other factors held constant. This is expressed in percent and is a function of component aging. |
|
| LOW LINE | The minimum steady state voltage that can be applied between the + and - input pins of a converter and still maintain output regulation. |
| MAINS | The utility AC power distribution wires. |
|
| MARGINING | Adjusting a power supply output voltage up or down from its nominal setting in order to verify system performance margin with respect to supply voltage. This is usually done electrically by a system-generated control signal. |
|
| MEGA MODULES | A chassis mount packaging option that incorporates one, two, or three VI/MI-200 Family converters for single, dual or triple outputs having a combined power of up to 600W. |
|
| M-GRADE | An industry standard where the operating temperature of a device does not drop below –55 degrees Celsius. |
|
| MILSPECS | Military standards that a device must meet to be used in military environments. |
|
| MINIMOD | A junior size (VI-J00) version of the VI/MI-200 Family of DC-DC converters offering up to half the power in a 2.28" x 2.4" x 0.5" package. |
|
| MINIMUM LOAD | The minimum load current/power that must be drawn from the power supply in order for the supply to meet its performance specifications. Less frequently, a minimum load is required to prevent the power supply from failing. |
|
| MODULE EVALUATION BOARD | A test fixture used to evaluate Vicor modules. AC and DC input versions are available. |
|
| MEAN TIME BETWEEN FAILURE | MTBF | MTBF is the point at which 63% of a given population no longer meet specification. It can either be calculated or demonstrated. The usual calculation is per MIL-STD-217 Rev. E. Demonstrated reliability is usually determined by temperature accelerated life testing and is usually greater than calculated MTBF. |
| NOMINAL INPUT | The center value for the input voltage range. |
|
| NOMINAL VALUE | A usual, average, normal, or expected operating condition. This stated value will probably not be equal to the value actually measured. |
|
| NON-ISOLATED POINT-OF-LOAD CONVERTER | niPOL | Available from many manufacturers in many configurations, typical niPOLs are simple buck converters providing low Vouts from an intermediate bus. |
| OFF LINE | A power supply that receives its input power from the AC line, without using a 50/60 Hz power transformer prior to rectification and filtering; hence the term “off–line” power supply. |
|
| OPEN FRAME | A power supply where there is no external metal chassis; the power supply is provided to the end user essentially as a printed circuit board that provides mechanical support as well as supporting the components and making electrical connections. |
|
| OPERATING TEMPERATURE | The range of temperatures in which a unit can operate within specifications. |
|
| OPTOISOLATOR | An electro-optical device that transmits a signal across a DC isolation boundary. |
|
| OR’ING DIODES | Diodes used to isolate supplies from one another under a fault condition. |
|
| OUTPUT FILTERING | Filter used to reduce switching power supply noise and ripple. |
|
| OUTPUT GOOD | A power supply status signal that indicates the output voltage is within a certain tolerance. An output that is either too high or too low will deactivate the Output Good signal. |
|
| OUTPUT IMPEDANCE | The ratio of change in output voltage to change in load current. |
|
| OUTPUT NOISE | The AC component that may be present on the DC output of a power supply. Switch-mode power supply output noise usually has two components: a lower frequency component at the switching frequency of the converter and a high frequency component due to fast edges of the converter switching transitions. Noise should always be measured directly at the output terminals with a scope probe having an extremely short grounding lead. |
|
| OUTPUT POWER RATING | The maximum power in watts that the power supply can provide and still maintain safety agency approvals. |
|
| OUTPUT VOLTAGE ACCURACY | See Setpoint Accuracy |
|
| OVERLOAD PROTECTION | A power supply protection circuit that limits the output current under overload conditions. |
|
| OVERTEMP WARNING | A TTL– compatible signal that indicates an overtemperature condition exists in the power supply. |
|
| OVERVOLTAGE PROTECTION | OVP | A circuit that either shuts down the power supply or crowbars the output in the event of an output overvoltage condition. |
| PARALLEL BOOST | VI/MI-200 Family booster modules may be added to a driver to create multi-kilowatt arrays. Boosters do not contain any feedback or control circuitry. |
|
| PARALLEL OPERATION | Connecting the outputs of two or more power supplies together for the purpose of obtaining a higher output current. This requires power supplies specially designed for load sharing. |
|
| PERIODIC AND RANDOM DEVIATION | PARD | Periodic And Random Deviation, referring to the sum of all ripple and noise components on the DC output of a power supply, regardless of nature or source. |
| PEAK POWER | The absolute maximum output power that a power supply can produce without immediate damage. Peak power capability is typically well beyond the continuous output power capability and the resulting average power should not exceed rated specifications. |
|
| POST REGULATOR | A secondary regulating circuit on an auxiliary output of a power supply that provides regulation on that output. |
|
| POWER CONVERSION | Is the process of converting power from one form into another. |
|
| POWER FAIL | A power supply interface signal that gives a warning that the input voltage will no longer sustain full power regulated output. |
|
| POWER FACTOR | The ratio of true power to apparent power in an AC circuit. In power conversion technology, power factor is used in conjunction with describing AC input current to the power supply. |
|
| POWER SUPPLY | A source of electrical energy employed to furnish the tubes and semiconductor devices of an electronic circuit with the proper electric voltages and currents for their operation. |
|
| PRELOAD | A small amount of current drawn from a power supply to stabilize its operation. |
|
| PRE-REGULATOR MODULE | PRM | A V•I Chip that takes an unregulated, wide range (up to 5:1) DC bus (e.g. a 36–75V bus used in 48V telecom systems) and produces a Factorized Bus output to drive VTMs or other FPA products. The PRM is a very high efficiency (up to 99%) non–isolated buck/boost converter that can control the Factorized Bus. |
| PRIMARY | The input section of an isolated power supply. It is connected to the AC mains and, hence, has dangerous voltage levels present. |
|
| PRODUCT GRADE | The environmental and acceptance tests performed on Vicor products. |
|
| PULSE–WIDTH MODULATION | PWM | A switching power conversion technique where the on-time (or width) of a duty cycle is modulated to control power transfer for regulating power supply outputs. |
| PUSH-PULL CONVERTER | A switch–mode power supply topology that utilizes a center-tapped transformer and two power switches. The two switches are alternately driven on and off. |
| QUASI-REGULATED OUTPUT | The regulation of an auxiliary output that is accomplished by regulation of the main output. A transformer turns ratio, commensurate with the desired auxiliary output voltage, is used in conjunction with the output around which the main control loop is closed. Quasi-regulated outputs are significantly affected by second–order effects in the converter. |
| RATED OUTPUT CURRENT | The maximum load current that a power supply can provide at a specified ambient temperature. |
|
| REFLECTED RIPPLE CURRENT | The rms or peak-to-peak AC current present at the input of the power supply that is a result of the switching frequency of the converter. |
|
| REGULATION | The ability of a power supply to maintain an output voltage within a specified tolerance as referenced to changing conditions of input voltage and/or load. |
|
| REGULATION BAND | The total error band allowable for an output voltage. This includes the effects of all of the types of regulation: line, load, temperature, and time. |
|
| REGULATORY AGENCIES | CSA: Canadian Standards Association; FCC: Federal Communications Commission; FTZ: Fernmelde Technisches Zentralamt; TÜV: Technischer Überwachungs Verein; U.L.: Underwriters Laboratory; VDE: Verband Deutscher Electrotechniker. |
|
| REMOTE INHIBIT | A power supply interface signal, usually TTL compatible, that commands the power supply to shut down one or all outputs. |
|
| REMOTE ON/OFF | Enables power supply to be remotely turned on or off. Turn-on is typically performed by open circuit or TTL logic “1”, and turn-off by switch closure or TTL logic “0”. |
|
| REMOTE SENSE | Wires connected in parallel with power supply output cables such that the power supply can sense the actual voltage at the load to compensate for voltage drops in the output cables and/or isolation devices. |
|
| RETURN | The designation of the common terminal for the power supply outputs. It carries the return current for the outputs. |
|
| REVERSE VOLTAGE PROTECTION | A protection circuit that prevents the power supply from being damaged in the event that a reverse voltage is applied at the input or output terminals. |
|
| RADIO FREQUENCY INTERFERENCE | RFI | An abbreviation for Radio Frequency Interference, undesirable noise produced by a power supply or other electrical or electronic device during its operation. In power supply technology, RFI is usually taken to mean the same thing as EMC. |
| RIPPLE AND NOISE | The amplitude of the AC component on the DC output of a power supply usually expressed in millivolts peak-to-peak or rms. For a linear power supply it is usually at the frequency of the AC mains. For a switching power supply, it is usually at the switching frequency of the converter stage. |
| SAFETY GROUND | A conductive path to earth that is designed to protect persons from electrical shock by shunting away any dangerous currents that might occur due to malfunction or accident. |
|
| SECONDARY | The output section of an isolated power supply, it is isolated from the AC mains and specially designed for safety of personnel who might be working with power on the system. |
|
| SAFETY EXTRA LOW VOLTAGE | SELV | A term generally defined by the regulatory agencies as the highest voltage that can be contacted by a person and not cause injury. It is often specifically defined as 30Vac or 42.4Vdc. |
| SETPOINT ACCURACY | Ratio of actual to specified output voltage. |
|
| SEQUENCING | The technique of establishing a desired order of activating the outputs of a multiple output power supply. |
|
| SOFT START | A technique for gradually activating a power supply circuit when the power supply is first turned on. This technique is generally used to provide a gradual rise in output voltages and inrush current limiting. |
|
| SOFT LINE | A condition where there is substantial impedance present in the AC mains feeding input power to a power supply. The input voltage to the power supply drops significantly with increasing load. |
|
| SPLIT BOBBIN WINDING | A transformer winding technique where the primary and secondary are wound side-by-side on a bobbin with an insulation barrier between them. |
|
| STANDBY CURRENT | The input current drawn by a power supply when shut down by a control input (remote inhibit) or under no load. |
|
| STIFF LINE | A condition where there is no significant impedance present in the AC mains feeding input power to a power supply. The input voltage to the power supply does not change appreciably with load. |
|
| SWITCHING FREQUENCY | The rate at which the DC voltage is switched on and off in a switching power supply. |
| TEMPERATURE COEFFICIENT | The average output voltage change expressed as a percent per degree Celsius of ambient temperature change. This is usually specified for a predetermined temperature range. |
|
| TEMPERATURE DERATING | Reducing the output power of a power supply with increasing temperature to maintain reliable operation. |
|
| THERMAL PAD | A graphite laminate used as a thermal interface between the converter and a heatsink or chassis. |
|
| THERMAL PROTECTION | A power supply protection circuit that shuts the power supply down in the event of unacceptably high internal temperatures. |
|
| TOPOLOGY | The design type of a converter, indicative of the configuration of switching transistors, utilization of the transformer, and type of filtering. Examples of topologies are the Flyback, Forward, Half Bridge, Full Bridge, Resonant and Zero-Current-Switching. |
|
| TRACKING | A characteristic in a multiple output power supply where any changes in the output voltage of one output caused by line, load, and/or temperature are proportional to similar changes in accompanying outputs. |
|
| TRANSIENT RECOVERY TIME | The time required for an output voltage to be within specified accuracy limits after a step change in line or load conditions. |
|
| TRUE POWER | In an AC circuit, true power is the actual power consumed. It is distinguished from apparent power by eliminating the reactive power component that may be present. |
| UNDERSHOOT | A transient output voltage change which does not meet the low limit of the voltage accuracy specification and is caused by turning the power supply on or off, or abruptly changing line or load conditions. |
|
| UNIVERSAL INPUT | An AC input capable of operating from major AC lines worldwide, without straps or switches. |
| V•I CHIP | The physical embodiment of FPA technology in power component form. V•I Chips are available in different sizes (“Double”, “Full” and “Half”), in SMT (J-lead) or through-hole options and with various heatsinking options. |
|
| VI-HAM HARMONIC ATTENUATOR MODULE | HAM | The VI-HAM is a component level front end that accommodates universal input voltage (85-264), provides line rectification, filtering, transient protection, unity power factor, inrush limiting, and a DC output compatible with the 300V input families of DC-DC converters. |
| VI-IAM INPUT ATTENUATOR MODULE | IAM | A Vicor filter module used to provide EMC conducted noise filtering and transient protection. |
| VOLTAGE BALANCE | The difference in magnitudes, in percent, of two output voltages that have equal nominal voltage magnitudes but opposite polarities. |
|
| VOLTAGE MODE | A method of closed loop control of a switching converter to correct for changes in the output voltage. |
|
| VOLTAGE TRANSFORMATION MODULE | VTM | A V•I Chip that takes a Factorized Bus voltage and provides galvanic isolation and either a step-up or step-down function (depending on application) . The output voltage is determined by the VTM's k factor: Vout = Vin * k. The VTM performs its power conversion function at high efficiency (up to 96%) and has exceptional dynamic response and noise characteristics. |
| WARM-UP DRIFT | The initial change in the output voltage of a power supply in the time period between turn-on and when the power supply reaches thermal equilibrium at 25 degrees Celsius, full load and nominal line. |
|
| WARM-UP TIME | The time required after initial turn-on for a power supply to achieve compliance to its performance specifications. |
| X-CAPACITOR | A capacitor connected across the supply lines to suppress normal mode interference. |
| Y-CAPACITOR | Power conversion modules generally require bypass capacitors from line to chassis (earth ground) to shunt common mode noise currents and keep them local to the converter. In cases where the converters are operating from rectified AC line voltage, the failure of a bypass capacitor could result in excessive leakage current to the equipment chassis thus creating a ground fault and shock hazard. For this reason, a special classification of capacitor, referred to as a Y-capacitor, is recommended. These capacitors contain a dielectric with unique “self-healing” properties to help prevent against excessive leakage. To meet general EMC requirements (see chapter 10 of the Vicor Applications Manual), Vicor recommends the use of Y-capacitors with all power conversion modules. Y-capacitors meet IEC384-14, EN132400, an UL 1283 standards. |
| ZERO-CURRENT-SWITCHING | The turn-on and turn-off of a switch at zero current, resulting in essentially lossless switching. The zero-current-switching topology allows Vicor converters to operate at frequencies in excess of 1 MHz, with efficiencies greater than 80% and power densities ten or more times greater than conventional topologies. |