Media Alert

Today Vicor released four new DCM products in the VIA package

001x001px_alpha.png
001x001px_alpha.png
001x001px_alpha.png

DCMAndover, MA – June 07, 2016 – Today Vicor released four additional DC-DC converters that are
deployed in the rugged, chassis-mountable versions of its DCM™ family of isolated, regulated DC-DC converters. These new products extend the family by adding two 270V and two 28V nominal products
to the family. (See Table 1)

 

Applications: DCMs are commonly used in industrial and process control markets, distributed power, ATE, communications, defense/aerospace, semiconductor manufacturing equipment (SME), and transportation.

 

What’s unique?
The DCM family provides the highest densities in a smaller footprint than competitors.
 

Input Voltage Input Voltage Range Output Voltage
5V 12V 15V 24V 28V 48V
300V 200 – 420V   400W   600W   500W
270V 160 – 420V   500W     500W  
28V 16 – 50V 180W 320W 320W 320W 320W  


Table 1 – Vicor's DCM Family – Green are products released today


Vicor's DCM Family Offering
The DCM in a VIA package is an isolated, regulated DC-DC converter, operating from an unregulated, wide range input to generate an isolated and regulated output. With its high frequency zero-voltage switching (ZVS) topology, the DCM converter consistently delivers high efficiency across the input line range. The DCM provides tight output voltage regulation and offers a secondary-referenced control interface for trim, enable, and remote sense operation. DCM converters and downstream DC-DC products support efficient power distribution, providing superior power system performance and connectivity from a variety of unregulated power sources to the
point of load.

 

Learn more about these products at:
http://www.vicorpower.com/new-products/dcm

 

001x001px_alpha.png
001x001px_alpha.png
001x001px_alpha.png
PR-Wordmark.jpg
 
Follow Vicor on Social Media
Twitter: @VicorPower »
Vicor Corporation on LinkedIn »
Vicor PowerBlog »
001x001px_alpha.png

About Vicor Corporation
Headquartered in Andover, Massachusetts, Vicor Corporation designs, manufactures and markets innovative, high-performance modular power components, from bricks to semiconductor-centric solutions, to enable customers to efficiently convert and manage power from the power source to the point of load. www.vicorpower.com

###

Vicor and DCM are trademarks of Vicor Corporation.


Contact
Colin Boroski
Rainier Communications
508-475-0025 x 142
cboroski@rainierco.com