Skip to main content
Santa Clara October 3, 2019
High-Performance Power Conversion Seminar & Workshops View Agenda Register now

Keynote speaker:
Dr. Ray Ridley

President, Ridley Engineering, Inc.

Dr. Ridley has been designing, researching, and teaching power electronics for over 40 years. His teaching style is renowned for applying advanced theory to practical design. He is very active in creating software and hardware development tools for designers. Thousands of engineers in 72 countries have taken his courses and use his products in the design process. His landmark work on current-mode control defined how the system should be analyzed and has remained the standard for over 30 years. Learn more

Dr. Ray Ridley

開催にあたり

開催にあたり

電源システム設計は、年々複雑さを増し続けており、高性能な電力変換を実現するためには、最新の設計手法の理解が不可欠です。本セミナーのワークショップでは、DC-DC設計、AC-DCフロントエンドの設計、EMI対策、放熱設計、PCBレイアウトなどに関する最新技術を、実際のアプリケーション事例を用いながら解説します。最先端の電源システムを設計するノウハウを、ぜひこの機会にご体験ください。

また、基調講演として

大阪会場では、長崎総合科学大学 学術教授・黒川 不二雄 氏

東京会場では、神戸大学 教授・牧野 淳一郎 氏 にご講演いただきます。皆様のご来場を心よりお待ちしております。

Agenda

October 3, 2019

Marriott Santa Clara, 2700 Mission College Boulevard, Santa Clara, CA 95054


9:00 to 9:30 AM

Registration


9:30 to 9:45 AM

Welcome


9:45 to 10:45 AM

Keynote by Dr. Ray Ridley


10:45 to 11:00 AM

Coffee break


11:00 AM to 12:00 PM

Track A - Santa Barbara Room

Workshop: EMI challenges and troubleshooting techniques

Presented by Applications Engineering

Without proper consideration, EMI can derail projects and create costly delays. With a real-world troubleshooting example, you will learn about basic EMI measurement, common and differential noise sources and identification methods, conducted EMI pre-compliance testing, layout issues, etc.

Track B - Newport Beach Room

Workshop: Modular DC-DC system design done right

Presented by Applications Engineering

Real-world systems comprise more than just the DC-DC converter itself. Using a case study to examine the requirements of module integration into a DC-DC system, you will learn topics such as input and output filtering, protections, compatibility with the source and load dynamics.


12:00 to 12:45 PM

Lunch


12:45 to 1:45 PM

Track A - Santa Barbara Room

Workshop: Avoiding common AC-DC design pitfalls

Presented by Applications Engineering

Design-in of AC-DC front end modules can be complicated. This session will provide a straightforward approach for success, covering such topics as source impedance considerations, inrush current, filter resonance and damping, PFC, faults, fusing, system stability and safety.

Track B - Newport Beach Room

Workshop: High-performance PCB layout and thermal design techniques

Presented by Applications Engineering

Our experts will share their optimization techniques addressing the following topics: applying thermal models and simulation, PCB layout for effective thermal management, power/signal routing and integrity in high density, high current applications to minimize board losses and maximize performance.


1:45 to 2:00 PM

Coffee break


2:00 to 3:00 PM

Track A - Santa Barbara Room

Workshop: Avoiding common AC-DC design pitfalls

Presented by Applications Engineering

Design-in of AC-DC front end modules can be complicated. This session will provide a straightforward approach for success, covering such topics as source impedance considerations, inrush current, filter resonance and damping, PFC, faults, fusing, system stability and safety.

Track B - Newport Beach Room

Workshop: Modular DC-DC system design done right

Presented by Applications Engineering

Real-world systems comprise more than just the DC-DC converter itself. Using a case study to examine the requirements of module integration into a DC-DC system, you will learn topics such as input and output filtering, protections, compatibility with the source and load dynamics.


3:00 to 3:30 PM

Wrap up & Networking


協賛

Mouser

Registration

Registration is now closed for this event.