Skip to main content
Osaka 2019 October 7
High-Performance Power Conversion Seminar & Workshops View Agenda Register now

Keynote speaker:
Prof. KUROKAWA, Fujio

Nagasaki Institute of Applied Science

Institute for Innovative Science and Technology

Professor Kurokawa is an accomplished teacher and researcher in the areas of dc-dc converters, ac-dc converters, inverters and their digital control, renewable energy technologies, power electronics technologies in aerospace and automobile and switching power supplies for lighting system. He has served as General Chair of 1st ICRERA (International Conference on Renewable Energy Research and Applications) 2012 and the  Organizing Committee Chair of IEEE INTELEC 2015. Dr. Kurokawa is a Fellow Member of the Institute of Electronics, Information and Communication Engineers of Japan, and also the IEEE Fellow. Learn more

Prof. KUROKAWA, Fujio

本次活动专业且免费开放,不容错过

本次活动专业且免费开放,不容错过

设计高性能电源系统的复杂性逐年增加。使用可靠的设计方法来实现高性能电源转换,是一次性获得成功的关键。您将了解全新的技术,其可满足 EMI 降低、热建模、PCB 布局、DC-DC 设计以及实现 AC-DC 前端的需求。我们在研讨会上将为您展示真实案例,与您共同探讨。

在本次的活动中,行业专家和 Vicor 应用工程师将为您带来新的技术。在设计高性能电源系统时,他们将帮助您识别常见的设计缺陷,引导您走上成功之路。

Agenda

2019 October 7

Hilton Plaza West Office Tower 8th floor – Daini Yoshimoto Building, 2-2-2 Umeda, Kita-ku Osaka-shi, Osaka, 530-0001 Japan


12:30 to 13:00

Registration and Technical Booth Open


13:00 to 13:30

Opening Speech


13:30 to 14:00

Keynote: Trends and Challenges of Future Oriented Power Converters

Presented by Prof. KUROKAWA, Fujio

In the society of Society 5.0 based on IoT and AI technology, the increase in power consumption along with the increase in data volume of information communication has become a big problem. Therefore, smart cities that use energy management technology such as VPP and ERAB that incorporate solar cells and EV batteries are attracting attention. Here, the development of model-based design and digital twin technology is required, and further, it is necessary to devise to use renewable energy that is not stable. In the future power system, the EV battery is included, so the charge / discharge device is also important. I will explain the research trends and challenges of future-oriented power supply system that controls and develops these multiple complex elements well.


14:00 to 14:15

Tea Break


14:15 to 15:00

Workshop: Avoiding common AC-DC design pitfalls

Presented by Applications Engineering

Design-in of AC-DC front end modules can be complicated. This session will provide a straightforward approach for success, covering such topics as source impedance considerations, inrush current, filter resonance and damping, PFC, faults, fusing, system stability and safety.


15:15 to 15:45

Workshop: EMI challenges and troubleshooting techniques

Presented by Applications Engineering

Without proper consideration, EMI can derail projects and create costly delays. With a real-world troubleshooting example, you will learn about basic EMI measurement, common and differential noise sources and identification methods, conducted EMI pre-compliance testing, layout issues, etc.


15:45 to 16:00

Tea Break


16:00 to 16:45

Workshop: Modular DC-DC system design done right

Presented by Applications Engineering

Real-world systems comprise more than just the DC-DC converter itself. Using a case study to examine the requirements of module integration into a DC-DC system, you will learn topics such as input and output filtering, protections, compatibility with the source and load dynamics.


16:45 to 17:30

Workshop: High-performance PCB layout and thermal design techniques

Presented by Applications Engineering

Our experts will share their optimization techniques addressing the following topics: applying thermal models and simulation, PCB layout for effective thermal management, power/signal routing and integrity in high density, high current applications to minimize board losses and maximize performance.


17:30 to 17:45 

Q&A and Closing


Our sponsor

Techstar

Registration

Registration is now closed for this event.