最適なPCBレイアウトと放熱設計技術
This workshop will cover important aspects of PCB design to maximize heat transfer and minimize power delivery impedance and losses
最適なPCBレイアウトと放熱設計技術
This workshop will cover important aspects of PCB design to maximize heat transfer and minimize power delivery impedance and losses
モジュールで構成するDC-DC電源システムの最適な設計手法
You will learn topics such as input and output filtering, protections, compatibility with the source and load dynamics
Ampaire社の環境に優しい空の旅
Ampaire社は、CO²排出量を削減する、環境に優しいハイブリッド電動航空機を開発しています。
Ampaire社の環境に優しい空の旅
Ampaire社は、CO²排出量を削減する、環境に優しいハイブリッド電動航空機を開発しています。
VoltServer社のデジタル・トランスフォーメーション
Voltserver社のDigital Electricity™が真のDXを実現
VITA62 3U Evaluation Board
Power converters enable innovation in robotics applications
Minimizing size and weight are important in robotics design, but increasing power is essential for supporting new sensors, peripherals and features.
OLogic, Vicor help Dusty Robotics optimize power for construction robots
OLogic, Vicor collaborate to optimize power and systems functionality for Dusty Robotics FieldPrinter
In the age of electrification, is the 12V battery still necessary?
Today’s BEVs are powered by 400 or 800V batteries. So is a 12V battery still needed? Learn how small, power modules can replace the 12V battery.
High-density power modules boost performance for a new generation of mobile robots
Minimizing size and weight are important in robotics design, but increasing power is essential for supporting new sensors, peripherals and features.
MOSA power supplies, custom components, engineering talent: Q & A with Vicor's John Sturm
SOSA provides a level of standardization. MOSA looks from a system standpoint to assure compatibility & interoperability in hardware & software development
High-performance power modules drive mission critical ‘seeing’ sensors
Kodiak Robotics’ self-driving technology to revitalize trucking industry. Learn why Vicor power modules were selected to power the mission critical sensors.
CCell社、Elektra Award にてパワーシステム・プロダクト・オブ・ザ・イヤーを受賞
CCell社は、再生可能エネルギーとVicorの電源モジュールを用いて、新しいサンゴ礁の成長を加速させ、世界中の海岸浸食を軽減しています。
Radiation-tolerant power electronic systems are hard to design
Optimizing the power distribution network (PDN) is very critical when dealing with high currents consumed by modern ASICs, FPGAs, CPUs and GPUs
Power modules offer new possibilities for uncharted EV power challenges
Economically, there is a lot hanging in the balance with automotive electrification. It may be the most important power challenge of our time
New developments are challenging power system designers with managing PDN impedance voltage drops, transient performance specifications and power loss
Vicor Corporation is named 2022 Massachusetts Manufacturer of the Year
Vicor recognized as a leader in Massachusetts manufacturing following the opening of the first-ever ChiP™ fabrication facility.
The future of standardized defense platforms using MOSA, SOSA and VPX open architectures
Using open standards to increase interoperability, scalability, reliability, reduce system costs, and minimize the number of custom electronics designs
Dragonfly社は、海上通信の構築に、新しい有線ドローンでどのように挑んだのか
DPI社の有線ドローンは、最高500フィートの高度で運用でき、船舶無線の見通し距離を8マイルから最大30マイルまで延ばすことができます。
電動化/大電力化が進む産業機器市場に、先端の電源技術で対応するVicor
Vicor responds with cutting-edge power supply technology to the industrial equipment market where electrification/higher power is progressing
Aerospace and defense power FAQs
A compilation of commonly asked questions about Vicor power solutions in aerospace and defense applications
Aerospace and defense glossary of terms
A comprehensive list of commonly used aerospace and defense terminology
Vicor delivers power conversion breakthroughs to fuel a robot revolution
OLogic incorporates advanced, integrated power modules from Vicor to ignite a new generation of mobile robots
OCP China Day 2022
オンボードチャージャーで(400/800V)両方のバッテリーに対応する
Range anxiety is the biggest inhibitor to EV adoption. Learn how this is best solved by an onboard power converter, not more charging stations
Redefining how electricity is distributed
Voltserver employs Vicor’s BCM6123 fixed ratio bus converter in the receiver portion of the Digital voltage system
Redefining automotive power delivery networks
Conversion of an EV’s HV battery using a high-density automotive-qualified DC-DC module offers weight and space savings for automotive manufacturers
Combating coastal erosion using renewable energy to expedite coral growth
The combo of the PRM and VTM allows for reasonably high-voltage DC to convert to quite low-voltage DC at relatively high current in a very efficient way
Vicor power modules boost satellite internet constellations
Vicor high-efficiency, high-density and high-current solutions play well into the new space model
Pump the brakes when it comes to EV fast-charging stations
Grappling with the EV 400V and 800V charging dilemma? Vicor deliver the surest way to eliminate compatible with any DC fast-charging station
Vicor touts its american “ChiP” fab as the industry’s first
Vicor ChiP power devices such as this are also able to flourish even in the toughest environments
Vicor ChiP™ fab – Automated and sustainable manufacturing
Vicor's vertically integrated fab uses patented processes enabling Vicor to produce high-quality, low-cost & reliable power module manufacturing
World's first ChiP manufacturing facility
Vicor completes 95,000 s/f ChiP fab expansion
The new ChiP fab uses patented fabrication processes that differentiate Vicor power modules by enabling the most power-dense & energy efficient solutions
モジュールで構成する高電力密度の電源システムに適した、PCBレイアウトと放熱設計
High-density loads like processors for artificial intelligence & supercomputing have become sophisticated & fast, pushing power components to capacity
Defense-electronics spending seeks to overcome COVID-19 setbacks in key applications
With COVID and the concerns over global economy and security, Vicor expects growth and R&D investment in unmanned vehicle deployment and ISR technology
幅広い専門技術と高い電力密度による、自走式ロボットの革新
Ologic and Vicor partner on robot design. Learn how high-density power modules from Vicor are the key to driving a new mobile robot innovation
Where fixed-ratio converters fit in high-power delivery systems
The density and efficiency of a fixed-ratio converter plays a critical role in enabling PDN architecture to deliver high performance
Life-saving tethered drones get a power and comms boost
The initial DC-DC converter design was heavy & consumed too much space. The lightweight DCM by Vicor provided the ideal power & weight for the application
Unlocking super compute performance
For legacy systems where more efficiency and power are needed, Vicor provides a simple option using a bidirectional NBM™ non-isolated bus converter
How to replicate the automotive 12V battery
Vicor high-density bus converter module technology enables ideal EV architecture
Accelerate vehicle electrification with the smallest, lightest power modules
EV sales for both pure battery electric vehicles and plug-in hybrid electric vehicles are accelerating rapidly
High-density power for New Space missions needed as demand booms, study predicts
Satellite power designers must deliver 20-30 times more current than legacy systems, while reducing the size, weight, & cost of the power delivery network
Rob Russell shares his industry insights into the future of LEO and MEO satellite deployments
Rob Russell discusses the trends in the LEO and MEO satellite market with Pat Hindle at Microwave Journal
Edge computing leverages modular power in scalable micro data centers
HIRO edge computing application delivers real time data to enhance brain surgery. Learn how Vicor’s power modules meet the high performance demands
Optimizing power delivery networks
Optimizing power delivery networks (PDNs) inevitably ends in system tradeoffs. Using power modules, the concessions are smaller and performance is better
Building Better UAVs using Modular Power
Vicor modules are power dense and lightweight, can easily scale as well as being flexible, while optimizing payloads and increasing flight times for UAVs
Global connectivity becoming a reality with the help of new, high density, power solutions
Terrestrial broadband can’t keep up with demand for internet bandwidth. Learn how power modules are enabling Satellites to fill this gap
Space and satellite frequently asked questions (FAQs)
Trust the power experts at Vicor to help you solve your toughest LEO and MEO satellite power design challenges in space
Engineering a sea change in ocean wave energy harvesting
Harvesting wave energy to provide reliable, cost-effective energy generation and storage, data, and communication services for offshore assets
Power density: the inconspicuous key to delivering worldwide internet coverage
Learn from the experts the rapidly evolving trends in powering LEO and MEO satellites for today's advanced communication networks in space
2022年4月5日~7日開催 World Congress Experience WCX 2022
Vicor presented three new power-dense approaches for powering xEVs
Delivering higher power density and low noise for New Space applications
Patented power design techniques and architectures needed to deliver optimal power and low noise for space communications applications
自然災害時の通信を支える、有線ドローンによる通信基地局
Fukaden's drones are delivering fast, reliable mobile service for first responders
Auto electrification boosted by modular designs
Like power-over-ethernet, digital electricity safely transmits up to 2kW of power across long distances (2km) using low-cost, off-the-shelf data cables
Challenges and design considerations for designing a power delivery network for New Space
Learn the basics to designing a better more reliable power delivery network that will deliver peak performance for LEO and MEO communication satellites
Vicor partners with Voltserver™ for Digital Electricity™
Digital Electricity enables operators to safely transmit as much 2kW of power across 2km using off-the-shelf data cabling. Vicor delivers DC-DC conversion
2022 energy forecast: Ultra-dense power delivery networks are re-shaping the future
UAV and robots are being deployed for more hazardous types of mobile jobs. Vicor power-dense modules make it easy to power these applications
Digital electricity brings intelligence and safety into power transmission
Digital Electricity™ offers the benefits of low-voltage with the power and distance capabilities (2km) of AC. Vicor provides DC-DC power conversion
High-density power is needed to keep pace with projected 20X growth in New Space
What will it take to achieve global Internet coverage? A lot of power. Learn how Vicor is helping increase internet bandwidth 20x over the next 10 years
Radiation-tolerant power electronics key to filling satellite infrastructure gap
Vicor’s innovative power solutions help to deliver broadband connectivity to billions of people with limited or no access to high-speed internet
Helping the U.S. Navy convert ocean waves into perpetual power
Vicor and C-Power unlock new opportunities for U.S. Navy using C-Power’s SeaRAY which provides localized power-generation and data services at sea
Shrink the 12V battery by half and maintain cold crank?
How much space and weight could you save by sizing the 12V battery correctly to meet your always-on use cases? Learn how much when using power modules
Space glossary of terms
Learn the language of the stars with this handy space and satellite glossary of terms
Optimizing high-density power design: modular vs. discrete
There are several important design variables to consider when evaluating the power module design process
Capturing the power of the ocean
Ocean waves breaking around the world’s coastline can deliver as much as the 2 – 3 million megawatts of total power
The new wave in energy generation
Wave power has lagged behind solar and wind, but it has perhaps the greatest potential
HIRO社の小型で拡張性が高いエッジコンピューティング
Edge computing is critical to realizing the full potential of artificial intelligence (AI), machine learning and Internet of Things (IoT)
Achieving higher power density with good-old Si MOSFETs
Minimizing tradeoffs and workarounds using high voltages and modular power approach to power systems design give longevity to the Si MOSFET
Collaborate with Vicor to accelerate vehicle electrification
Overcoming hurdles with fast charging, converting high voltage and bridging 12V and 48V applications
Powering clustered AI processors
Vertical power enables up to 100kA of current and multi-rail core voltage delivery
C-Power and Vicor deliver efficient, renewable energy for offshore applications
Power systems that perpetually generate and store 10W to 1MW from ocean waves
Is the 12V lead-acid battery dead?
Leveraging an EV’s high voltage battery to deliver 12V more efficiently
Compact, high-density, high-efficiency DC-DCs for New Space applications
Satellite operators are offering sophisticated on-board processing capabilities
Digital Electricity™ delivers true digital transformation
The digitalization of buildings, agriculture and outdoor stadiums require intelligent edge-sensors to facilitate real-time data transmission to the cloud
Electrified vehicles: 48V is the new 12V
A vehicle has many different power requirements. A modular power approach is inherently more flexible and scalable, able to address these challenges
Advancements in UAV capabilities using modular power delivery networks
The growth of UAVs is also being driven by new applications, with both commercial and defense UAVs requiring more functionality to meet these needs
Eliminate the 12V battery and increase EV performance
Vicor power module transient response (75A/10µs), is three times faster than 12V, in essence creating a virtual battery
Preparing the way ahead for a compatible EV infrastructure
Onboard conversion enables EVs to charge any station
Modular power delivery networks for UAVs
The key challenge we see facing engineers today is the demand for smaller, lighter-weight designs that deliver higher power
Powering high performance computing
Factorized Power Architecture delivers lower core voltages and higher core currents while providing lower losses and higher efficiency
xEV開発を加速する電源モジュール
Overcome three key hurdles to electrification, including decentralized 48V power distribution and 400V/800V charging compatibility
DCM for tethered UAV applications
Tethered drones can be demanding as weight reduction is a critical requirement. Vicor DCMs create an optimum solution for this type of application
海洋のアプリケーションに給電する波力発電
Oceanographic exploration is challenging because of unpredictable environmental conditions
モバイルロボットのパフォーマンスを向上する次世代の電源システム
Real-word examples of using modular power in robots
Dragonfly UAVs extends ship radio line-of-site from communication nearly 4x
Deploying 800V high voltage power enabled the tethered UAV to minimize losses and drag by using a thinner, lighter tether cable power
Fuel cell powered drones deliver humanitarian supplies
Hydrogen fuel-cell-powered drones use high density power modules for overseas humanitarian missions. The innovative PDN provides 4x flight times.
Six questions to consider before designing your robot’s power architecture
Power dense modules are the optimal robotics solution that deliver compact, lightweight and scalable power that is efficient and flexible
The race to automotive electrification: what it takes to win
To achieve their aggressive electrification goals, OEMs need to innovate their power delivery networks using high density, scalable power modules
Innovating power module packaging
Power module packaging is a unique differentiator that has enable Vicor to increase power density by more than 500x in 40 years
モバイルロボットに最適な電力供給ネットワーク(英)
Guide to developing better PDNs to meet the needs of today’s robotics systems
Enables quick and easy configuration of complete, high efficiency, compact, multi-output power systems.
Designing your power system and/or choosing the right module is as easy as entering your input and output power and your basic system requirements
WiBotic and Vicor automate wireless charging for robots
Wibotic’s adaptive matching system underpins innovative approach to enable more robotic fleet productivity. Vicor power modules support wireless charging
Hydrogen fuel cell power extends drone range by 4x
Hydrogen fuel cell drones deliver 4x duration of lithium ion batteries. Vicor power modules enable Doosan’s innovative, efficient power delivery network
Power solution reduces downtime for ultrasonic pipeline inspection
Power solution reduces downtime by upgrading the sensors, cameras and onboard processors
Vicor supports robust power demands of next generation wireless charging for mobile robots and drones
The next generation of robotic productivity replies on power dense modules to support autonomous, wireless charging
Overcoming tethered UAV challenges with a high-voltage, compact module-based power delivery network
Optimizing tethered UAV performance by deploying compact, module-based power delivery network. High voltage enables thinner, lighter tethered cable
Autonomous wireless charging keeps robots moving
Wibotic and Vicor partner to deliver enhanced power systems that drive autonomous wireless charging for optimal robot and UAV performance
過酷な水中ミッションに対応するモジュールで構成する水中ドローン (ROV)
VideoRay’s modular design approach offers unprecedented flexibility to quickly design ROVs for custom missions
モジュールで構成するDC-DCシステムの設計手法 第2回:フィルタの設計
モジュールで構成するDC-DCシステムの設計手法 第1回:4つの設計ステージ
モジュールで構成するDC-DCシステムの設計手法 第5回:負荷に関する考慮
モジュールで構成するDC‑DCシステムの設計手法 第4回:安全と保護の機能
モジュールで構成するDC-DCシステムの設計手法 第3回:安定性解析とデカップリング
High-density, modular power delivery networks optimize mobile robot performance
Fixed-ratio and high-efficiency buck and buck-boost converters enable more range, duration and payload
More power within the same space for machine vision systems
Machine vision systems have dramatically increased the throughput and quality of products built on automated production lines by improving accuracy
Improving the ergonomics of hand-held tools with medical robots
Miniature robotic tools can facilitate a reduction in the scope of medical surgery
Wide input voltage facilitates contactless power solution for overhead gantry robots
Many factories specializing in the fabrication of heavy objects can benefit from an overhead gantry with robots
High efficiency converters help maximize run-time for autonomous warehouse robots
High efficiency converters help maximize run-time
Low-weight, low-noise solution for sewer inspection robots
Power more sensors without increasing weight to improve autonomy, mobility and AI (allowing deep learning) is enabling inspection robots to replace humans
More patrolling, less recharging for security robots
The addition of sensors like LIDAR, together with sophisticated onboard AI processors, has allowed autonomous robots to interact more safely with humans
Lighter cables enable new markets for tethered drones
Power modules support high efficiency tethered surveillance drone that can detach and fly free to track and chase
Environmentally friendly electric power systems for the airline industry
高性能電源モジュールのパッケージング技術(日)
Power module packaging, has been a unique differentiator for Vicor since its inception
Aircraft gets an 11kW power supply the size of a tablet computer
An upgrade to a high-altitude long endurance (HALE) UAV platform included fitting a new, higher-resolution, longer-range radar and improving the telemetry
Power averaging saves cost for weaving looms
Power averaging saves cost
Reliable operation in a tough environment for ore prospecting instrumentation
When drilling for ore at shallower sites complexity and cost can be significantly reduced using a motor driven helical screw drill bit
DC-DC transformer facilitates implementation of longer tether for underwater ROV
DC-DC transformer facilitates implementation of longer tether
Delivering high current at very low voltage for satellite antennas
Delivering high current at very low voltage suits the need for a small, robust and reliable low profile power solution for antennas
Bi-directional converter shrinks battery array to one cell for portable x-rays
Solid-state X-ray technology allows X-ray scanners to be portable and battery operated, enabling medical staff to check patients in any location
High density power allows for unobtrusive 5G indoor small-cell base station
High density power allows for unobtrusive base station
日経X-TECH:高度な電力供給ネットワークがあらゆる業界、特にHPC、自動車、産業市場に新たな可能性を生み出す
世界初、UAV向け水素燃料電池パワーパックを製品化
Industry-leading UAV flight range
モジュール型設計の強み(英)
Power delivery networks are rapidly changing, and their power requirements require a wide portfolio of modules to enable the maximum.
Meeting the challenges of power-hungry Aerospace and Defense applications with modular power
航空宇宙・防衛:エッジコンピューティングに必要な電力供給をSWaP(サイズ・重力・消費電力)の制約下で実現
メジャーツーリングカー選手権で世界初のハイブリッドシステム導入へ(日)
New hybrid engine features an innovative, ultra-lightweight, 48V lithium-ion-based battery pack and intelligent power management system
400VをSELVシステムの電源に(英)
Ian Mazsa sits down with EE Journal to discuss best practices and benefits of using high voltage power
革新した電力供給ネットワーク (PDN) (英)
Every electronic piece of equipment or system has a power delivery network (PDN)
Tethered UAV power matching
Discover new techniques using real-world applications to develop system architecture and select power components to fulfill conversion needs
Today’s vehicles require higher power and less weight
機動性とリモート通信を革新する、新しい有線ドローン
Tethered multi-rotor drones are designed to track and follow mobile host platforms under the most extreme weather conditions
Designing high-power parallel arrays with PRMs
BCMs transform high-voltage batteries into SELV systems
Eliminate intermediate energy storage in EV power architectures. Read this Vicor white paper on BCM Selve systems
Design guide to powering tethered UAVs
To upgrade features in a UAV increases the payload weight, so your power supply need to be power dense, scalable flexible to accommodate change
航空業界向けの環境に優しい電源システム(英)
EETimes Japan: 自動車業界に新しい設計概念を、モジュールを組み合わせてあらゆる電力レベルに対応
失敗しないAC-DC設計
This webinar focuses on AC-DC front-end considerations, inrush current considerations, requirements of PFC, and passive and active PFC
テスラとVicorが、自動車の電源システムを設計するうえで重要なトレードオフについて意見交換
Electric vehicles can use up to 20X more electrical power than a traditional internal combustion engine vehicle
Eliminate intermediate energy storage in EV power architectures
High-density DC-DC delivers 22A, with Sn/Pb BGA option
サンゴ礁の復元と拡大して、海岸の浸食を防止し海洋生体系を保つ
Precise power conversion and regulation of renewable energy
Vicor power modules support charging, delivery and conversion for electrified vehicles
Power delivery networks at a crossroads
ロボットのための高効率給電システム
Learn how Vicor delivers high power with efficiency and reduced weight for various robots
ロボットのための高効率給電システム
Learn how to overcome hurdles with fast charging, converting high voltage and bridging 12V and 48V applications
Factorized Power 技術を用いて、モバイル衛星ブロードバンド接続の信頼性を大幅に改善して、より高性能なモバイル通信を実現
Phasor delivers robust mobile broadband connectivity using Factorized Power
Factorized Power Accelerates Coral Reef Restoration
PSDcast – Autonomous wireless charging of robot and drone fleets will reshape the future of automation and production
How to build and power autonomous wireless charging for robots or battery at any station, enabling the maximum up time
Electric-powered aviation with high-efficiency, scalable power components
Escalating concern over rising carbon dioxide (CO2) emissions is driving worldwide demand for more pure electric vehicle and hybrid electric vehicles
The future of automotive power is 48V
Wireless charging delivers next generation productivity for robotics and UAVs
Robotic and unmanned vehicle (UV) fleets are reshaping the future of automation and production
What are the advantages of a decentralized power architecture in automotive?
Decentralized power is a phenomenon that's starting to hit the automotive sector
電力供給ネットワークを刷新する電圧変換比固定DC-DCコンバータ
This white paper discusses the fixed ratio, DC DC converter and why designers should consider it an essential part of the power delivery architecture
Power Electronic Tips: Where fixed-ratio converters fit in high-power delivery systems
回路モデルを用いた熱シミュレーション
Power Electronic Tips: Where fixed-ratio converters fit in high-power delivery systems
Electronic Specifier: Power electronics at a crossroads
Mouser: DC-DC converters provide superior power system performance and connectivity
With its high frequency zero voltage switching (ZVS) topology, DCMs consistently deliver high efficiency across their specified input line range
Mouser: High-power, zero-voltage switching DC-DC converters consistently deliver high efficiency
The Vicor DCM3623 family are isolated, regulated DC-DC converters, operating from an unregulated, wide range input to generate an isolated output
Mouser: New class of DC-DC power converters meet the rigors of onboard rail applications
The Vicor DCM2322 family of isolated and regulated DC-DC converters provide high efficiency and high power density for rail, defense, aerospace, and more
Digi-Key: Powering modern rail systems
The DCM2322 is an isolated, regulated DC-DC converter enabling high-frequency, zero-voltage switching that has a low-profile design with high-density filtering
Mouser: 48V/12Vを双方向変換・98%の高効率
The NBM2317 bridging converter for 12v and 48v systems enables cost-effective high-density and high-efficiency
Mouser: High-efficiency point-of-load regulators
The PI3523 ZVS Switching Regulators are high-efficiency and integrate the controller, switches, amplifiers and support components in a high-density LGA system
Mouser: Wide range direct to point-of-load regulators
Digi-Key: DC-DC converters that provide all the necessary performance and features needed to create smaller, lighter and less costly power systems
The DCM3623T75H53 module leverages the thermal and density benefits of Vicor ChiP packaging technology, allowing customers to achieve cost effective power solutions with previously...
Digi-Key: High‑performance buck regulators achieve size reduction
PI3325 ZVS buck regulators are highly integrated system-in-package regulators that integrate the controller, power switches, and support components in a 10 x 14mm LGA package
Electronic Design: Solve auto electrification challenges with a decentralized 48V power architecture
High-density, modular power delivery networks optimize mobile robot performance
Factorized power is shorthand for a Factorized Power Architecture (FPA) used when high-current board-mounted power is needed
Power System Design: When less is more
Bodos: Disrupting Conventional Electrical Power within Automotive
Adopting the 48V battery
Vehicle electrical requirements for modern EVs and hybrids adopt the 48V battery
Meeting the Power Challenges for Today’s Modern Rail
Michael Schipani sits down with Amelia Dalton, Host of Chalk Talk (EE Journal) to discuss the power challenges and trends within the rail industry
Digi-Key: Efficiently Bridging 12V to 48V
Bridging 12V to 48V, the Vicor NBM2317 is a non-isolated, fixed ratio, DC-DC bidirectional converter that uses a unique switching topology and packaging
大容量コンデンサを削除することにより 小型/ 軽量なシステムを構築
Vicor's Factorized Power Architecture™ (FPA) delivers significant reductions in both size and weight
DCM Design Guide
DCM family
SM-ChiP™ reflow soldering recommendations
Power averaging with regulation: a smart solution for pulsed loads
Power averaging for configuring a system to power pulsed loads allows the designer to build a system that is small, power dense and very efficient
An easier and more efficient way to keep your LEDs running brighter, longer!
LED video wall technology is expensive to deploy and maintain. But better power design can improve performance, efficiency and long-term success
Designing rapid-start power applications that never fail
Rapid-start power systems operate at daunting speeds as fast as 10ms
VITA 62 increases existing power specs necessary for aircraft pod-mounted power supply
VITA 62 3U power supply parallel operation
EDN: Vicor Powers AI and Automotive
VIA™ Package PMBus® Interface and Accessories User Guide
PMBus® Interface and Accessories User Guide (For use with adapter part number I2C-ADAPTER-A02)
GQFN SiP soldering recommendations
ECN: Requirements increase for smaller, high-performance power supplies and modules
Dr. Vinciarelli receiving the prestigious 2019 IEEE William E. Newell Power Electronics Award
PI358x-00-EVAL1 ZVS Regulators 30 – 60VIN ZVS Buck evaluation board
Assembly guideline for ZVS Buck and Buck‑Boost, 10 x 10mm and 10 x 14mm LGA/BGA package
複数のコンバータを使用した ワイド入力 DC-DC 電源ソリューション
One-size-fits-all typically simplifies situations. However, this approach does not deliver the best results when selecting an ultra-wide DC-DC power supply
Designing military-grade, rapid-start power applications
In the field of battle milliseconds can be the difference between success and failure. Learn what it takes to design a flawless rapid-start power system
PFC MicroSTMPower Factor Corrected AC-DC Switcher
PFC MicroTM Power Factor Corrected AC-DC Switcher
QPI-x-EVAL1
QPO-1-EVAL1
QPO-2-EVAL1
PFC MiniTM Power Factor Corrected AC-DC Switcher
QPI-12-CB1-EVAL board
Image stability for the gimbal system improves vehicle-mounted optical sights
Compact vehicle power supply
Why are power designs moving to 48V?
To power the next generation of data centers, electric vehicles and AI-driven technologies, industries are moving to 48V power
鉄道アプリケーション向けの電源システム設計
This webinar explains the market pressures on engineers developing power systems for the rail industry and ways to overcome the technical challenges
Your Power System Failed its Conducted EMI Test – Now What?
This webinar focuses on techniques to help identify the real source for EMI test failure quickly, and how to reduce their noise spectrum
Thermal management for VIA™ and ChiP™ modules
Scalable, low-weight DC-DC solution for high-capacitive loads in airborne radar
DC-DC Solution for a unique power system challenge
NBM2317 SM‑ChiP™ (non-isolated bus converter module) evaluation board
Direct infrared countermeasure's optical circuitry runs cooler while meeting stringent EMI specs
When size and weight matters
Supply voltage for the RF amplifier is well regulated during frequency-hopping, providing secure communication in portable radios
Providing secure, encrypted communication to minimize espionage
This paper explains how power designers can use these steps to remove the stress of safety certifications for their next design
The need for greater energy efficiency, higher output and increased density must be met despite reducing design cycle times to shorten time-to-market
Bodos: Handling Late Changes in Power System Designs
High-density, modular power delivery networks optimize mobile robot performance
New AC-DC system architecture based on fixed-ratio bus converters is described and analyzed along with its benefits and trade-offs
In critical applications, where power supply failure can be catastrophic, fault-tolerant power supplies use N+1 similar converters to provide a very high level of reliability
Electronic Specifier: Package Prepares for AI Computing
PFC single-conversion line ripple cancellation using the Yeaman topology
The main characteristic of this topology is to separate the output voltage regulation function from the bulk power‑conversion function, as it is used in DC‑DC converters
How Vicor power components enable power averaging
As system power levels increase, many power designers are finding it difficult to stay within space and weight constraints. Designing the power system for the average power can be ...
Leveraging bus converters in regulated DC-DC applications
FPA™ (Factorized Power Architecture™) has provided leverage in solving demanding power challenges which call for high levels of efficiency, power density and superior power handlin...
Practical EMI control in a power component design space
This article attempts to address the notion of control of conducted emissions in the context of applying Vicor Power Components in a customer application
A wide-input voltage range allows full utilization of the battery, which extended the range of the UAVs
Facilitating battery upgrade to extend range
Different power requirements are handled so that UAVs adapt to different required payloads
Scalable solutions for maximum functionality
PI31xx-xx-EVAL1 ZVS isolated DC-DC converter evaluation board
電源設計における分かりやすい安全規格
This webinar presents a checklist of things to consider about safety when working on your next power design
The Power Dilemma for the Next Generation of Automobiles
Electric, hybrid electric, driver assistance systems and infotainment are creating new power demands for automotive manufacturers
High-density, modular power delivery networks optimize mobile robot performance
The top reasons for not completing designs on time include the demand for increasingly higher-performance and a lack of engineering resources and skills
Recommendations for Maximum Compressive Force of Heat Sinks
High-performance zvs buck regulator removes barriers to increased power throughput in wide input range point-of-load applications
Today's higher performance applications require more than what conventional regulators can offer
Control of a discontinuous-conduction-mode ZVS Buck-Boost topology for microprocessor core power
In this paper, the authors navigate the design challenges one encounters implementing such a voltage regulation scheme that are not seen in the traditional continuous‑conduction‑mo...
Thermal models of Vicor power components
This paper describes the circuit models that have been created for Vicor products to allow engineers to estimate the maximum internal temperature of the power component
Creating high-voltage outputs for the Micro, Mini, Maxi; VI-200, MI-200; VI-J00, MI-J00 converter families only
A growing number of industries are moving to higher-voltage, 48V distribution versus conventional 12V distribution
Reverse-mode application of Sine Amplitude Converters
The power electronics industry is seeing the re-emergence of DC high-voltage distribution in place of AC systems of power transmission within advanced machines and installations
How to avoid the "hidden costs" of power system design
Is designing your power system costing too much? Discrete designs can be more costly. Learn more about the benefits of a modular approach to design
PFC MegaPAC-ELTM PFC MegaPAC-HPELTM Power Factor Corrected AC-DC Switchers
PFC MegaPAC™ power factor corrected AC-DC switchers
HV ChiP BCM® reverse start-up circuit
Power on Package and 3M Demonstration
Vicor and 3M demonstrate the benefits of liquid immersion cooling
Power System Designer User Guide
Filter considerations for the IBC™
Micro DC-DC converter family isolated remote sense
Improving the light-load efficiency of a VI Chip® Bus Converter array
Offline power supply using the FARM AC front-end module
Fault-management circuit
Designing a BCM® pre‑charge circuit
Gyoukou Supercomputer Leveraging 48V Factorized Power
Watch the demonstration of Gyoukou, the ExaScaler/PEZY ZettaScaler-2.2 liquid immersion cooling supercomputer
DC MegaPAC™ DC-DC switcher
Decreased weight and size of the power source enables the payload increase of tethered robots
Multiple power source, rugged vehicle robots
Power sharing among converters simplifies remote upgrading of optical packet transport systems
Field upgradable power
AC line input replaces an existing DC solution in an existing PBX system
Flexible telephone system
Distributed antenna system redesign is now powered over ethernet
Powering an invisible DAS solution
High power supply efficiency provides reliable power over ethernet
Power over ethernet (POE) distribution
Powering high-tech 4K cameras overcomes size, weight and EMI requirements
More bits, less weight
Remote radio units better distribute traffic while operating under fault conditions
Keeping one step ahead in a fast changing market
100% reliable backhaul communications uses an array with a footprint of just 52.97cm2
Unique paralleling capability for 100% reliability
4G remote radio unit extends mobile signal coverage in remote areas
Facilitating a base station performance upgrade
Conduction-cooling solution allows for truly portable network test equipment
High-performance, lightweight AC to load solution
A complete N+1 solution maintains uptime for network security AC-DC power supply
Network security redundant AC-DC supply for secure power
Low-profile AC-DC solution allows distributed antenna system to run at high temps without fans
Low-profile AC-DC solution for flexible installation
A fanless power solution gives antenna array fast, reliable data coverage.
Hidden power for antenna arrays
Industrial flow meters are more accurate while working over wider flow ranges
Power components simplify source redundancy
Explosive-proof camera images in variable lighting conditions become more clear, sharp and accurate with AC-DC solution
Low-noise AC-DC solution for harsh environments
Maxi, Mini, Micro DC-DC converters parallel bus: PR pin
The rugged environment for Bus Wi‑Fi gets an efficient and reliable power
Flexible solution reduces system size
Different vehicle voltages is accommodated by one solution for digital video recorders
Single-BOM solution for multiple input voltage requirements
Automated test equipment’s speed and throughput improves with factorized power architecture
Increase speed & throughput of an automated test station
Fire alarm control unit uses DC-DC supply and battery backup while increasing functionality
Maximizing available operational time under battery
Industrial welding laser speed and accuracy improves using factorized power architecture
Maximizing laser speed & accuracy through innovative power solutions
Scalable power solutions allow marine instrumentation to keep precision while operating in extreme environments
Adding more and more capabilities into increasingly smaller spaces
Bidirectional DC-DC converters conveniently transfer power between the grid and batteries in home energy storage
The future of home energy
Handling a variety of user-defined output power requirements for medical carts
Minimizing lead times through scalable power design
Power supply size reduction allows for additional medical diagnostic equipment functionality within the same footprint
Re-architecting the power solution to reduce system size and cost
Scalable power solution matches specific power levels for various machines in optical sorting
Reducing design complexity and costs
Power solution operates in extreme temperatures for LEDs to display brighter lights, longer
Same colors all the time
High-voltage bus converters significantly reduce installation costs for outdoor stadium lighting
Power transmission for outdoor lighting with lower-weight power cables
Scientific instrumentation gets twice the power without impacting the size of the equipment
Simple, hassle-free power design
HVDC facilitates higher performance
Managing the heat of the power supply makes rail signaling more reliable
High-density power chain provides redundancy in the same space
Slowed ramp-up process relieves stress of the power supply during startup in vehicle mounted advertising displays
Reliable solution at high temperatures
Speed, precision, resolution and contrast of engraving lasers is improved using wide-input and output-range regulators
Fast and dynamic power for speed and precision
5kW tethered UAVs fly higher and longer using increased voltage on the tether
Increasing payload with HVDC and power-dense components
Separating the functions of a traditional DC converter improves the speed and accuracy for 3D printers
Factorized power in a 3D printer application
Enormous video wall display becomes feasible with a move to component-enabled, higher voltage bus
HVDC reduces cabling weight and distribution losses
PI31xx product family reflow soldering guidelines
Powering a smart control upgrade minimizes wasted head in hydraulic pumps
Freeing up the space to go smart
A third more power in just 20% of the space for vehicle GPS applications
Vehicle GPS location systems reduce operational costs and provide control over their most remote assets
Accurate point-of-load voltage regulation using simple adaptive-loop feedback
Using BCM® Bus Converters in high-power arrays
VI Chip® BCM® Bus Converter thermal management
FPA printed circuit board layout guidelines
PRM™and VTM™ parallel array operation
Through-hole ChiP™ package soldering guidelines
Filter network design for VI Chip® DC-DC Converter Modules
RoHS-compliant through-hole VI Chip® soldering recommendations
SMT J-Lead VI Chip® soldering recommendations
PI3325-00-EVAL1 ZVS Switching Regulators 60VIN Buck Customer Eval Board User Guide
Providing a constant current for powering LEDs using the PRM™ and VTM™
Optimize battery charging and control motor start-up allows longer time in flight for inspection UAVs
Light, compact power supply increases UAV payload
Flexible power solution with different outputs allows for easily-upgraded flight simulators
Simple upgrade capability
Lightweight and small-sized power solution for thermal imaging camera supports increasing power and complexity
Maximizing resolution and range
Enhanced onboard satellite voice and data communications takes advantage of maximized power amplifier efficiency
Power density facilitates upgrade
More power supports more functionality in the same space used across different platforms in sub sonar systems
Flexible, low-noise approach for improved detection effectiveness
Minimal distortion and power supply noise helps achieve maximum range in portable ground radar
Power averaging for a 64% reduction in power requirements
Multiple power supplies paralleled together provided 9kW high-output power
Ultra-low-profile 8kW high-power array
Low levels of conducted and radiated EMI enable detection of signals outside the aircraft in airborne electronic countermeasure
Low-noise airborne power solution
Dual-sided cooling of power supplies on vertically-mounted racks improves thermal performance for sub-combat control
Compact rack power supply
Improved efficiency of the power supply allows high temp operation in RF signal intelligence
High-performance dual-source architecture for signal detection and identification
MIL-STD power components withstand mechanical stresses caused by vibration and acceleration in helicopter gearboxes
Size, weight and high reliability must be ensured under extreme operating conditions
MIL EMI and transient solutions
Achieving high-accuracy voltage (or current) regulation with the DCM™ Up to ±1% regulation
Configuring Vicor IBC converters with niPOLs
Under/overvoltage lockout for VI‑200/VI‑J00 and Maxi, Mini, Micro converters
PCB mount VIA soldering guidelines
Parallel DCMs™
Current share boards
Meeting transient specifications for electrical systems in military vehicles
Thermal considerations: assuring performance of the Vicor Maxi, Mini, Micro series high‑density DC-DC Converter Modules
Creating Higher Voltage Outputs Using Series Connected Sine Amplitude Converters
Single DCM™as an Isolated, Regulated DC-DC Converter
Soldering Methods and Procedures for Vicor Power Modules
Surviving Load Dumps on Military Vehicles
Wide Range Trimming with Variable Loads
Designing High-Power Arrays Using Maxi, Mini and Micro Family DC-DC Converters
Using Modular DC-DC Converters to Meet European Standards for Railway Applications
High Efficiency Battery Charger using Power Components
Constant Current Control for DC-DC Converters
Adjustable Latching Output Overcurrent Circuit
Hot Swap Capability Eliminates Down Time
Meeting the demands of SWaP-C for defense and aerospace
Designing products for aerospace and defense exposes us to unique engineering challenges
Back to basics: choosing the perfect regulator
Spec changes top list of power designers’ challenges
A Vicor survey revealed that power designers face many challenges. Learn what they are and how they can be overcome
Additional electronics for passenger seat actuators are solved with smaller, lighter components
Improving passenger comfort with additional electronics
防衛アプリケーションのためのDC-DC電源システムの要求仕様
Topics include: meeting standards, applications and test results, reducing noise with filters, using power components optimized for defense applications
More Answers to Your Bi-Directional Power Design Questions
バッテリー・アプリケーション向けパワーコンポーネント
This webinar explains how flexible power components shorten the design cycle, reduce cost, weight and size while increasing efficiency
Scalability of bi-directional power design: your questions answered
PI352x-0x-EVAL1 ZVS Switching Regulators 60VIN Buck Customer Eval Board
PI3740-00-EVAL1, -EVAL2 ZVS Switching Regulators Buck-Boost Evaluation Board
The challenges of high power LED design
Understanding how LED power designs affect LED performance is essential for success
ExaScaler and PEZY Computing unveil the first super computer
ExaScaler/PEZY ZettaScaler-1.8 Super Computer pushes the limits in computing performance
Scalable, low weight DC-DC solution with high capacitive loads
Engineers who are designing LED power system applications face a number of challenges to develop systems that offer advantages over competitors’ products
PI3741-0x-EVAL1 ZVS Switching Regulators Buck-Boost Evaluation Board
Simple Ideas to Make EMI Issues a Thing of the Past
The webinar covers the causes of EMI issues in power systems
Vicor ZVS regulators = > the sweet spot in integration
The easiest way to design the proper thermal management system
Thermal Simulation for Cooler Power Systems
This webinar describes the info you need from data sheets and app notes, and then shows how to make accurate thermal calculations by hand
Maximum Load: The Wrong Specification for Pulsed Power
This webinar explains why peak power is the wrong metric and introduces a different technique – power averaging
Enabling Bi-Directional Energy Flow Using DC Power Transformers
Learn about designing for bi-directional DC-DC power flow and how you can use DC power transformers to simplify power system design
How to increase efficiency of large displays
28VDC MIL-COTS VIPAC™ family
Power system design: Save time using Vicor's Power System Designer tool
New tool enables designers to quickly and easily architect, analyze and configure complete, optimized, compact, multi-output power systems in minutes
Power system design: Get to market fast
Learn how the Power Component Design Methodology can get you to market quickly
Distributing power to HEV/EV electrical systems with DCMs
Newer Hybrid-Electric Vehicles and Battery-Electric Vehicles increase the demand for safe-to-touch 12V power
Development Kit User Guide
PI3749-x0-EVAL1 ZVS Switching Regulators Buck-Boost Evaluation Board
NBM6123 ChiP™Analog Low-Voltage Non-Isolated Bus Converter Module Evaluation Board
PI354X-00 Evaluation Board 36V to 60VIN, 2.5, 3.3, 5.0 and 12VOUT Buck Regulator & LED Driver
PMBus® 2361 and 6123 ChiP™ BCM® Bus Converter Evaluation Board
7 ways to shrink your power system
As electronic products have grown in complexity with highly-evolved feature sets, designers have developed sophisticated schemes for power management
Analog HV and LV 6123 ChiP™ BCM® Bus Converter Evaluation Board
Capacitance at the input of the DC-DC converter plays a vital role in keeping the converter stable and playing a role in input EMI filtering
VIPAC™ family
3-Phase MegaPAC-ELTM (Low Noise), 4kW MegaPAC-ELTM (Low Noise), AC-DC Switchers
Sine amplitude converters provide design flexibility
Analog Control 3623 and 4623 ChiP DCMs™Evaluation Board
Online Vicor tools: simulators
Online Vicor tools: thermal calculator
Full-chip PRM™-RS Customer Board
VI Chip® BCM® Evaluation Board
Packaging innovations: doubling the surface area for cooling
VI Chip® Remote-Sense PRM™ Evaluation Board (For use with PCB part numbers 39537 and 38693)
PI33xx-xx-EVAL1 & PI34xx-xx-EVAL1 ZVS Buck Regulator Evaluation Board
Adaptive loop control provides improved regulation over simple local loop control – within +/- 1%
Thermal testing of high density power components
This white paper looks at the issues and circumstances that can lead to damaging harmonic generation, and practical approaches to reducing it
Specialized test systems for high performance power components
Back to basics: how do I ensure correct power rail sequencing in a multi-rail power architecture?
Power Distribution Network design for automated test equipment
As instrumentation card requirements grew in terms diversification of channels and loads, distributed power architectures became a necessary choice
PRM-AL Customer Evaluation Boards
Half-Chip PRM-RS Customer Evaluation Board (For use with PCB part number 35307)
VI Chip® VTM™ Evaluation Board
Back to basics: the importance of switching frequency
VI Chip® High-Voltage BCM® Customer Evaluation Board
High-voltage DC distribution is key to increased system efficiency and renewable energy opportunities
A transition to 400VDC in power distribution and conversion will help meet greenhouse gas, efficiency and renewable-energy goals
How to meet European standards for rail applications
Watch how Marco explains how to meet the European railway standards EN50155 and RIA12
Back to basics: what are Y-capacitors?
Back to basics: zero-voltage switching – what it is and why it’s important for buck-voltage regulation
VI Chip® PRM™ Evaluation Board
The characteristics of the DC-DC converter, the load, the electrical characteristics of the passive components and the available PCB area all present additional design constraints ...
350 – 12VDC “Yeaman Topology” power system
Active filters control EMI, save PCB space and enhance airflow
Smaller size saves valuable board real estate and the reduced height enhances airflow for better heat management
Dual-stage feedback technique for single-pole feedback compensation
The PI33xx: Zero-voltage switching applied to buck regulation
This unique, high-density buck regulator integrates a high-performance Zero-Voltage Switching (ZVS) topology along with power and support components all within a surface-mount pack...
An Introduction to Vicor's PRM® Modules
This video introduces Vicor's PRM Modules with user-configurable capabilities
What to consider when choosing a buck regulator
DC-DC converters and power conversion devices play a key role in conducting electrical power from the edge of a PCB to its onboard components efficiently
An introduction to ZVS Buck Regulators
Learn how the simple-to-use PI33XX Series of ZVS Buck Regulators can provide the high efficiency, high density and flexibility
How to Use the 24 V ZVS Buck Evaluation Board
Listen to Chester Firek introduce our ZVS Buck Evaluation Board
Thermal and mechanical considerations
This video looks at efficiency, heat, cooling by conduction, convection and radiation
Output Voltage Trimming
This video presents the benefits of voltage trimming, i.e., creating non-standard output voltages and voltage controlled current sources
Protecting your system against transients is not only a fundamental part of the development, it can also become a major challenge during the design cycle
Back to basics: meeting EMI for AC-DC systems
EMI is seen as one of the key challenges of power conversion design and system integration, particularly for AC-DC systems
Meeting conducted noise standards
Constant-Current (CC) Evaluation Board
Solving SWaP-C power challenges for MIL-COTS applications
High-performance power supplies to solve the toughest problems
UAV・ドローンの
積載量と飛行時間を増やす
ロボットのための
高効率給電システム
A better way to deliver power for high speed, low latency network coverage for the world
Military Embedded Systems: Innovation in military power supplies: Intelligence, standardization, efficiency
Power Electronic Tips: Vicor bus converter earns coveted 2019 Leap Award
Power Electronic Tips: Boosting performance in 48V power distribution
5 minutes on AI with Robert Gendron
Robert Gendron discusses power and Artificial Intelligence (AI).
5 minutes on AI with Ian Mazsa
What does it take to power Artificial Intelligence Systems and GPUs?
Reducing energy costs for AI systems
EDN: Data center power in 2019
EDN: Power supply management in quantum computers
Military & Aerospace Electronics: Military power electronics seeks to increase voltage and efficiency
Avionic equipment operates simultaneously from multiple power sources in extreme temps without fans
Triple redundancy for avionics equipment to help pilots navigate and control their airplane safely
Pulsed energy demands of airborne infrared countermeasures are averaged out to avoid system interference
Pulsed load driver for lasers
VIPAC Array™ family
モジュールで構成する
高効率・高電力密度の
電源システム
The need for new AI processor power delivery
Learn about an innovative new approach to powering AI applications that can reduce motherboard copper and processor interconnect resistances by up to 50X