从派克峰到 Bonneville 盐滩,Lightning 的速度超越内燃机摩托车 Lightning Motorcycles 设计的纯电动摩托车在各个领域都表现出色。了解 Vicor 电源模块如何助力这款新一代摩托车
48V 电源系统: 汽车制造商告别 12V 时您需要了解的信息 随着汽车制造商走向电动汽车 48V 电源,越来越多的汽车制造商开始考虑采用区域电源架构。48V 电源领域的领导者 Vicor 使用电源模块优化供电网络
Vicor 工程师 Chris Swartz 入选电气电子工程师协会高级会员 Chris Swartz 荣获 IEEE 高级会员称号。这是只有 10% 的会员才能拥有的精英地位。Chris 在 Vicor 任职 15 年
Vicor 将在慕尼黑举行的汽车高压电源系统大会上介绍如何利用 48V 电源加速 xEV 设计 Vicor 在慕尼黑汽车高压电源系统大会上发表演讲。了解高密度电源模块如何利用 48V 电源加速 xEV 设计
Patrizio Vinciarelli 创立 Vicor,解决电源转换难题 40 多年来,Patrizio Vinciarelli 一直是电源电子领域的创新者。如今,他正在应对这个时代最紧迫的电源挑战
国防与航空航天:为具有尺寸、重量及功耗限制的前沿技术提供强劲动力 Standardizing MILCOTS for VPX. Explore how Vicor is exceeds today's need for rugged power supplies that deliver the power while being optimized for size and weight
当今的汽车需要更大的电源和更轻的重量 Read how Vicor is addressing the need and demand for smaller, lighter vehicles to achieve lower CO2 emissions
航空产业的环保电源系统 The airline industry is undergoing an evolution of aircraft electrification, to analyze the cost/performance benefits of electric-powered aviation
如何在汽车电源系统设计中做出重要利弊权衡 Electric vehicles can use up to 20X more electrical power than a traditional internal combustion engine vehicle
消除电动汽车供电架构的中间储能 Vicor fixed ratio converters transform high-voltage batteries into 48V and 12V SELV systems
高密度 DC-DC 转换器提供 22A 的电流,可为 MIL-COTS 提供 Sn/Pb BGA 选项 Vicor has added a Pb-inclusive version of its 3V-ouput buck controllers for MIL-COTS applications
Vicor 电源模块为电动汽车提供充电、供电和转换支持 Power delivery to the various loads in the vehicle is changing from 12 to 48V as a means of reducing vehicle weight
收割、搬运和配送机器人的最高效供电 Learn how Vicor delivers high power with efficiency and reduced weight for various robots
用更小、更轻的电源模块加速汽车电气化 Learn how to overcome hurdles with fast charging, converting high voltage and bridging 12V and 48V applications
PSDcast – 机器人和无人机产品的自主无线充电将重塑自动化生产的未来 How to build and power autonomous wireless charging for robots or battery at any station, enabling the maximum up time
Mouser: DC-DC 转换器提供优异的电源系统性能和连接性 With its high frequency zero voltage switching (ZVS) topology, DCMs consistently deliver high efficiency across their specified input line range
Mouser: 高功率、零电压开关 DC-DC 转换器始终提供高效率 The Vicor DCM3623 family are isolated, regulated DC-DC converters, operating from an unregulated, wide range input to generate an isolated output
Mouser: 新型 DC-DC 电源转换器充分满足最严格的轨道交通车载应用需求 The Vicor DCM2322 family of isolated and regulated DC-DC converters provide high efficiency and high power density for rail, defense, aerospace, and more
Digi-Key: 为现代轨道系统供电 The DCM2322 is an isolated, regulated DC-DC converter enabling high-frequency, zero-voltage switching that has a low-profile design with high-density filtering
Mouser: 双向 48V 至 12V 转换支持 98% 的峰值效率 The NBM2317 bridging converter for 12v and 48v systems enables cost-effective high-density and high-efficiency
Mouser: 高效率负载点稳压器 The PI3523 ZVS Switching Regulators are high-efficiency and integrate the controller, switches, amplifiers and support components in a high-density LGA system
Digi-Key: DC-DC 转换器,可为创建更小、更轻、成本更低的电源系统提供所有必要的性能及特性 The DCM3623T75H53 module leverages the thermal and density benefits of Vicor ChiP packaging technology, allowing customers to achieve cost effective power solutions with previously...
Digi-Key: 高性能降压稳压器可在不降低吞吐量的情况下缩小尺寸 PI3325 ZVS buck regulators are highly integrated system-in-package regulators that integrate the controller, power switches, and support components in a 10 x 14mm LGA package
迎接现代铁路的电源挑战 Michael Schipani sits down with Amelia Dalton, Host of Chalk Talk (EE Journal) to discuss the power challenges and trends within the rail industry
Digi-Key: 将 12V 高效桥接至 48V Bridging 12V to 48V, the Vicor NBM2317 is a non-isolated, fixed ratio, DC-DC bidirectional converter that uses a unique switching topology and packaging
为什么电源设计要转为 48V? To power the next generation of data centers, electric vehicles and AI-driven technologies, industries are moving to 48V power
电源系统设计人员的逐步安全设计 This paper explains how power designers can use these steps to remove the stress of safety certifications for their next design
在并行DC-DC转换器阵列中减少不需要的输入拍频 In critical applications, where power supply failure can be catastrophic, fault-tolerant power supplies use N+1 similar converters to provide a very high level of reliability
使用 Yeaman 拓扑消除 PFC 单转换线路纹波 The main characteristic of this topology is to separate the output voltage regulation function from the bulk power‑conversion function, as it is used in DC‑DC converters
母线转换器在稳压 DC-DC 应用中的使用 FPA™ (Factorized Power Architecture™) has provided leverage in solving demanding power challenges which call for high levels of efficiency, power density and superior power handlin...
Vicor 电源组件如何实现功率平均 As system power levels increase, many power designers are finding it difficult to stay within space and weight constraints. Designing the power system for the average power can be ...
下一代汽车的动力困境 Electric, hybrid electric, driver assistance systems and infotainment are creating new power demands for automotive manufacturers
微处理机核电源中不连续导电模式 ZVS 升降压拓扑的控制 In this paper, the authors navigate the design challenges one encounters implementing such a voltage regulation scheme that are not seen in the traditional continuous‑conduction‑mo...
正弦幅度转换器的逆向模式应用 The power electronics industry is seeing the re-emergence of DC high-voltage distribution in place of AC systems of power transmission within advanced machines and installations
Gyoukou 超级计算机采用 48V 分比式电源 Watch the demonstration of Gyoukou, the ExaScaler/PEZY ZettaScaler-2.2 liquid immersion cooling supercomputer
满足航空航天及国防产品的严格 SWaP-C 要求 Designing products for aerospace and defense exposes us to unique engineering challenges
ExaScaler 和 PEZY Computing 推出第一台超级计算机 ExaScaler/PEZY ZettaScaler-1.8 Super Computer pushes the limits in computing performance
电源系统设计:使用 Vicor 电源系统设计工具节省时间 New tool enables designers to quickly and easily architect, analyze and configure complete, optimized, compact, multi-output power systems in minutes
Back to basics: zero-voltage switching – what it is and why it’s important for buck-voltage regulation
回到基础:理解和降低严重的配电耗损问题 DC-DC converters and power conversion devices play a key role in conducting electrical power from the edge of a PCB to its onboard components efficiently
ZVS 降压稳压器介绍 Learn how the simple-to-use PI33XX Series of ZVS Buck Regulators can provide the high efficiency, high density and flexibility
输出电压微调 This video presents the benefits of voltage trimming, i.e., creating non-standard output voltages and voltage controlled current sources
最新人工智能处理器供电需求 Learn about an innovative new approach to powering AI applications that can reduce motherboard copper and processor interconnect resistances by up to 50X