Skip to main content

World’s first hybrid touring car championship to use new Delta Motorsport intelligent power-dense battery pack

Media Alert

Powering Innovation: World’s first hybrid touring car championship to use new Delta Motorsport intelligent power-dense battery pack

High-power source density and functionality eliminates vehicle alternator, reducing weight and increasing reliability

October 29, 2020

Delta Motorsport was given the responsibility to design a new battery pack and associated electronics for the “tactical boost” for the British Touring Car Championship. Using a modular power delivery network (PDN), the system delivers high performance using 48VDC power source.

Delta Motorsport was given the responsibility to design a new battery pack and associated electronics for the “tactical boost” for the British Touring Car Championship. Using a modular power delivery network (PDN), the system delivers high performance using 48VDC power source.

The high-profile British Touring Car Championship (BTCC) has been a tradition since 1958 and is a great spectacle of 30+ highly-engineered road cars battling to win. In 2022 the championship will add a new dimension and will become the world’s first major touring car championship to feature high-performance mild-hybrid vehicles. 

The BTCC has specified that an electric motor can be used tactically by drivers to boost performance and enhance vehicle acceleration. This contract was awarded to Cosworth Electronics, which subcontracted this highly-specialized endeavour to Delta Motorsport. Due to their multidisciplinary engineering reputation and expertise in electronics, Delta Motorsport agreed to design a new battery pack and associated electronics for the “tactical boost.”

The new 48V lithium-ion-based battery pack has an innovative intelligent power management and high-power-density DCDC converter and regulation system. The battery pack powers the inverter-motor combination and also accepts regenerated power from it, while the high-power-density converter solution powers all the car’s electrical circuits and devices. The level of power density and power management achieved by this architecture allowed the alternator system to be removed, further improving weight, performance and reliability.

The system achieves compact size, light weight and high performance by utilizing a modular power delivery network (PDN) that incorporates the 48VDC power source that is fed to four DC-DC converters connected in parallel, which together supply regulated 13.8V power at up to 92 amps (approximately 1.2 kilowatts of power). The load is shared by the four converters, although it can be fully supported by just three, i.e., N+1, or aviation-level redundancy.

The hybrid system’s 3-phase brushless motor connects to the battery through a bidirectional inverter that routes battery power to the motor and regenerated power from the motor back to the battery.

The motor drives the vehicle in pure-EV mode (motor only, no ICE) during its initial, speed-limited journey down the pit lane, then in mild-hybrid mode (together with the ICE) when the driver demands a performance boost during the race. 

Innovative battery-pack intelligence and management

The battery pack includes a battery management system that controls all the cell voltages and ensures that the battery handles the maximum possible charge and discharge voltages at all times while communicating with the motor-inverter controller. It continuously calculates and updates the controller on how much current the battery can supply or accept, based on its state of charge (SoC). Power demand must be reduced at a low SoC, while regeneration must be limited at a higher SoC.

The system also monitors the temperatures of all available cells in real time and feeds the results into the available power calculations. Additionally, it can open contactors to isolate the battery pack safely if a problem arises.

Vicor-article-Delta-Motorsports.jpg

Delta Motorsport designed a power delivery network that uses a 48VDC power source feeding four DC‑DC converters connected in parallel, which together supply regulated 13.8V power at up to 92 amps (approximately 1.2 kilowatts of power). The load is shared by the four converters, although it can be fully supported by just three, i.e., N+1, or aviation-level redundancy.

The battery management system supports data logging and diagnostics, to log the DC-DC converter’s performance. This is not only to check fault status but also to provide feedback on the exact amount of current being delivered on all vehicles.

Vicor DC-DC converter power modules

The DC-DC converter power system uses four Vicor DCM3623 isolated, regulated DCDC converter ChiP power modules to deliver a regulated 13.8V output from the battery pack with current levels up to 92 amps. Due to their low profile and small footprint, they are mounted in direct thermal contact with the micro-bore cooling plates that extend between the battery cells.

Vicor power delivery network as designed by Delta Motorsport

This was a critical advantage, as it was essential to devote maximum volume to the productive battery cells rather than on power electronics ‘overhead’. The DCM modules’ scalability and ease of paralleling enabled the modular power architecture, allowing Delta to customise the DCDC PDN to the small footprint they needed without sacrificing power. 

Vicor modular power components excelled during initial battery pack tests, with no de-rating necessary and no voltage sags. Future electric vehicles will inevitably need smaller, lighter and higher-efficiency power electronics to handle increasing performance demands. As manufacturers migrate to 48V batteries to handle this elevated power, the Vicor modular approach can improve power delivery network efficiency, reducing power losses and weight with smaller, lighter cable and connectors.

Delta Motorsport also used a Vicor PI3105, a small 60W isolated converter for an uninterruptable power supply (UPS), which supplies power to the battery pack electronics in order to maintain the safety systems when isolated from the vehicle power supply. The UPS also allows the electronics to be powered independently of the vehicle, enabling remote connection for systems checks.

“British Touring Car Championship… Start your HYBRID engines”!

Learn more about Delta Motorsport’s innovative battery pack.

About Vicor

Vicor Corporation designs, develops, manufactures and markets modular power components and complete power systems based upon a portfolio of patented technologies. Headquartered in Andover, Massachusetts, Vicor sells its products to the power systems market, including enterprise and high performance computing, industrial equipment and automation, telecommunications and network infrastructure, vehicles and transportation, aerospace and defense. www.vicorpower.com

Vicor, DCM™ and ChiP™ are trademarks of Vicor Corporation.

    About Delta Motorsport 

Delta is an innovative and creative engineering business, based at the world-famous Silverstone Circuit, in the heart of the UK's high-performance technology cluster.

Delta has three main development streams; battery systems, its catalytic generator and platform master control. Each is approached with the same robust but lightweight methodology, honed through decades spent in the high-pressure motorsport sector.

Wrapped around these three streams is also a vehicle engineering and integration capability that has seen Delta deliver many whole vehicle projects, for start-ups and OEMs alike.

Delta's multidisciplinary team supports a wide range of sectors and its capability covers services from initial concept through to low volume production.

www.delta-motorsport.com

Contact Stephen Germino Media Relations & PR, Director/Vicor Corporation 978 749.8243 sgermino@vicorpower.com