Automotive Innovation Day 2026
Vicor presented innovative benefits of using compact, power dense DC-DC conversion
Power designs are moving from 12V to 48V because of the competitive advantage it provides. Vicor power modules support this trend with smaller and more efficient power delivery networks. Listen to the podcast.
Podcast with Patrick Wadden, Global Vice President, Vicor Automotive Business Unit
One of the more interesting trends to emerge in the automotive landscape is the broader availability of active suspension systems. While the idea, itself, was tossed around as far back as the 1950s, it didn’t become a thing until 80’s, though it was cost-prohibitive. And even today, being able to adjust suspension in real-time is mostly a luxury feature, though Hongfa and Vicor aim to change that.
Automotive Innovation Day 2026
Vicor presented innovative benefits of using compact, power dense DC-DC conversion
48V instead of 12V: DC‑DC converters in focus of the SDV
Future vehicles use 12V, 48V, and HV rails. Vicor experts discuss the vital role of DC-DC converters in SDVs, focusing on energy efficiency and safety
Automotive Engineering Exposition 2026
Solving automotive electrification challenges with the highest efficiency and highest power density power modules
How are automotive electronics evolving?
Power delivery networks in automotive are being taxed more than ever today. Learn how Vicor is helping design more efficient power systems