Skip to main content

Vicor BCM® bus converter wins Product of the Year at the 2025 World Electronics Achievement Awards.

Media Alert

Vicor BCM® bus converter wins Product of the Year at the 2025 World Electronics Achievement Awards

BCM6135 bidirectional 800V-to-48V DC-DC bus converter enables breakthrough innovation for next-generation EV automotive architectures

February 04, 2026
BCM6135 800V product image

Figure 1: The BCM6135 is a breakthrough bidirectional 800V to 48V converter that enables lighter, smaller and more efficient electric vehicles.

BCM6135 800V product image

Figure 1: The BCM6135 is a breakthrough bidirectional 800V to 48V converter that enables lighter, smaller and more efficient electric vehicles.

Andover, MA, January 22 – Vicor Corporation announced it has won the 2025 Product of the Year Award for the BCM6135 DC-DC bidirectional power converter presented at World Electronics Achievement Awards (WEAA). The BCM6135, which won in the category of Power Management/Voltage Converter, was selected by AspenCore global senior analysts and its worldwide user community for its impact on the electrification of automobiles and eMobility. The prestigious award celebrates innovative product design for applications that had significant impact within the automotive industry.

The BCM6135 is transforming eMobility and enabling breakthrough innovations in automotive electrification. It is the most power dense and fastest (top transient response) DC-DC converter in automotive today. It is enabling OEMs and Tier Ones to design the smallest active suspension power systems, optimize a 48V zonal power architecture and remove a 48V battery altogether. The BCM’s compact size and weigh can reduce power system volume by nearly 50% in a vehicle enabling greater range or innovation.

“As vehicle electrification accelerates, traditional power architectures are becoming an impediment to performance, efficiency and design flexibility,” said Eric Wong, Vicor Vice President for Sales Asia Pacific at Vicor. “The BCM6135 fundamentally changes what is possible in automotive power conversion by delivering unmatched power density, bidirectional operation, and ultra-fast transient response in a miniature, production-ready module. The compact size enables unprecedented design flexibility and scalability.”

Enabling a new era of automotive innovation and architectures

The BCM6135 is a breakthrough bidirectional 800V-to-48V converter that enables lighter, smaller and more efficient electric vehicles. It is a power-dense, isolated DC-DC converter, delivering up to 2.5kW from a compact, 58-gram module. Its flexibility and scalability are unmatched in the market, and it is a catalyst to next-generation power system design concepts. It addresses the challenges of growing electrical loads by enabling 48V zonal architectures, simplifying system design and potentially eliminating the need for a dedicated 48V or 12V battery.

About Vicor

Vicor Corporation (NASDAQ:VICR) is an American manufacturer of advanced 48V-centric DC-DC converter power modules with the highest power and current density, enabling breakthrough power delivery network performance and a competitive advantage for our customers power systems. Vicor combines innovative topologies, control systems, components and packaging into modular solutions that drive advancements in data centers, automation, robotics, mobility, test equipment and aerospace and defense applications. Vicor ensures supply chain resiliency via its vertically integrated ChiP™ fab and OEM IP licensing practice. www.vicorpower.com

Vicor, BCM®, and ChiP™ are registered trademarks of Vicor Corporation.

About World Electronics Achievement Awards (WEAA)

The WEAA, presented by AspenCore, honors the companies and individuals who have made outstanding contributions to the innovation and the development of electronics industry worldwide. WEAA are praised by many and represent one's leadership and excellent performance within the electronics industry.

Contact Stephen Germino Media Relations & PR, Director/Vicor Corporation 978-749-8243 sgermino@vicorpower.com