Skip to main content

Industrial Event

Techno-Frontier 2026

Techno Frontier event image

Vicor showcased advanced next-generation power systems across diverse industries

Vicor serves a broad range of power systems markets, including enterprise and high-performance computing, industrial equipment and automation, telecommunications and network infrastructure, automotive and transportation, as well as aerospace and defense.

At Techno Frontier 2026, Vicor showcased a wide range of high-density DC-DC converter modules supporting the growing transition to 48V power architectures across multiple industries. We also exhibited automotive power units co-developed with Japanese customers.

Vicor presented at three Techno-Frontier sessions

Vicor high-performance 48V power solutions for industrial equipment, material handling systems, and collaborative robots

Presented by Koji Nishikawa, Senior Applications Engineer, Vicor K.K.

In industrial equipment, material handling systems, and collaborative robotics, adoption of 48V power architectures is accelerating to achieve higher efficiency and smaller system size.

This seminar introduced high-performance power solutions leveraging Vicor’s broad range of 48V power technologies and explain approaches to optimizing the entire power delivery network (PDN) across a variety of applications.

Through application examples including logistics systems, AGVs, UAVs, transport robots, sorting robots, and contactless power supply systems (rail power supply), we showcased how Vicor power modules enable higher efficiency and space-saving system designs.

Photo of Koji Nishikawa

After earning a bachelor's degree from Tokyo University of Science, Koji gained over 26 years of experience at semiconductor and electronics manufacturers such as ROHM Semiconductor and ON Semiconductor before joining Vicor in 2022. Currently, as a Senior Applications Engineer, Koji is involved in the development of cutting-edge power systems with customers in a wide range of applications including industrial equipment, robotics, and aerospace and defense.

Vicor high-performance power solutions for next-generation aircraft

Presented by Koji Nishikawa, Senior Applications Engineer, Vicor K.K.

In the aerospace and defense industry, increasing system performance demands are driving the need for power systems with even higher power density, greater reliability, and reduced size and weight.

This seminar introduced Vicor’s high-performance power approaches for next-generation aircraft, focusing on 270V and 28V power solutions.

Using next-generation aircraft application examples, Vicor covered compliance with commercial aircraft power system standards, as well as system configurations incorporating high-performance filter products.

Vicor also explained how high-power-density, defense-standard-compliant power modules help improve system efficiency while reducing size and weight.

In addition, Vicor offers VPX-standard power units compliant with VITA and SOSA specifications, which was also introduced during the seminar.

Photo of Koji Nishikawa

After earning a bachelor's degree from Tokyo University of Science, Koji gained over 26 years of experience at semiconductor and electronics manufacturers such as ROHM Semiconductor and ON Semiconductor before joining Vicor in 2022. Currently, as a Senior Applications Engineer, Koji is involved in the development of cutting-edge power systems with customers in a wide range of applications including industrial equipment, robotics, and aerospace and defense.

Vicor high-performance HV – 48V and 48V – 12V power solutions for automotive and mobility applications

Presented by Tetsuo Haoka, Principal Field Applications Engineer, Vicor K.K.

This seminar introduced design approaches for compact and lightweight power units that enable higher value-added vehicle systems by leveraging Vicor’s high power density and high efficiency power solutions.

The seminar covered two main topics:

The first topic focused on enhancing vehicle functionality through 48V high-power actuators. Vicor’s BCM, which is compact, lightweight, and effectively functions as a 48V battery, eliminates the need for a large 48V battery and makes the implementation of 48V actuators more practical.

The second topic introduced design approaches for compact and lightweight power units using Vicor’s high power-density, high-efficiency power solutions. Two prototype automotive DC-DC converter units jointly developed with a domestic automotive parts manufacturer — a 400V – 800V converter and a 400V – 12V converter — will be presented. The seminar provided detailed explanations ranging from circuit configuration to mechanical structure.

Photo of Tetsuo Haoka

After receiving his Master's degree in Engineering from the Tokyo Institute of Technology, Tetsuo worked for over 10 years at Texas Instruments Japan, LLC and Renesas Electronics Corporation (formerly IDT Japan, LLC), where he was involved in embedded software design, ASIC logic circuit design, and technical support as a FAE (field application engineer).

Tetsuo joined Vicor in 2020. As a Principal Field Application Engineer, he is responsible for technical support for a wide range of applications, including semiconductor inspection equipment, data centers, and automotive.

About Techno-Frontier

Techno-Frontier is where professionals search clues for the future. Visitors know that the latest technologies & products in Electronics and Mechatronics gather here. Each clearly-focused exhibition enables the professionals to locate what they need, and the wide range of the products sparks ideas on possibilities of technical coordination.