使用 MOSA、SOSA 和 VPX 开放式架构的未来标准化防御平台
使用 MOSA、SOSA 和 VPX 开放式架构的未来标准化防御平台
使用 MOSA、SOSA 和 VPX 开放式架构的未来标准化防御平台
使用 MOSA、SOSA 和 VPX 开放式架构的未来标准化防御平台
为新太空应用提供更高的功率密度和低噪声
为太空通信应用提供最佳功率和低噪声所需的专利电源设计技术和架构
优化 DC-DC 转换器稳定性:源阻抗效应的 AC 与瞬态仿真分析
探讨如何通过频域 AC 小信号分析和时域瞬态分析来优化 DC‑DC 转换器的稳定性
Innovating the electrification of high-voltage mobile power delivery
ReVolt is electrifying film sets! See how they use Vicor high-density power modules to swap diesel for clean, mobile energy
Why power architectures constrain New Space AI missions
Satellite AI outpaces legacy power systems. Modern compute needs sub-volt, high-amp power that traditional architectures simply can't deliver until now
Automotive Innovation Day 2026
Vicor to present innovative benefits of using compact, power dense DC-DC conversion
2026 慕尼黑上海电子展
Vicor 将展出面向汽车、工业及 HPC 领域的 48V 高性能创新电源解决方案
Quickly modifying a standard SOSA supply to meet an applications hold-up requirements for vehicle protection and countermeasures
Learn how Vicor delivers power to vehicle protection and countermeasures systems using a configured SOSA aligned power supply
Adjusting one of the VITA supply voltage outputs easily and quickly for ground mobile radar
Learn how Vicor delivers power to ground mobile radar using time- and cost-effective Vicor VPX solutions
High reliability VITA 62 supply that handles unique current requirements for aircraft radar
Learn how Vicor delivers power to aircraft radar using high power and high current delivery of Vicor VPX products
A rugged, plug and play solution that satisfies multiple voltages in a single package for display control unit for armored vehicles
Learn how Vicor delivers power to the display control unit for armored vehicles using strong thermal performance power modules
A modular VPX solution providing reduced time to market for coastal surveillance radar
Learn how Vicor delivers power to coastal surveillance radars using its VITA 62 power supply to provide real time operation status monitoring
Eliminating the detectable heat signature from a SOSA supply when it’s not in use for radio frequency countermeasures
Learn how Vicor delivers power to radio frequency countermeasures using its VPX solutions which are both time- and cost-efficient
Techno Frontier 2026
展示面向多行业的先进新一代电源系统
A single 6U multiple power, high efficiency qualified to meet MIL-STD operational requirements for electronic warfare suite for aircraft
Learn how Vicor delivers power in an electronic warfare suite for aircraft using superior density VITA 62 power supply
Meeting a short qualification window when upgrading to a VPX power supply for multi-mode radar
Learn how Vicor delivers power to multi-mode radars using high performance power modules nested in the VPX power supply
Implementing a common power supply across several types of vehicles
Learn how Vicor delivers power to military ground vehicles using SOSA aligned power supplies
AI 在太空赋能快速通信,开启创新新纪元
Spacechips 携手 Vicor 打造了 AI1 应答器,这是目前在轨运行中功率密度最高的处理器板。分比式电源架构可提供 133 TOPS 算力用于实时卫星自主运行和 130A 处理
A configurable VITA 62 supply that mitigates engineering efforts for long range surface mapping radar
Learn how Vicor delivers power to long range surface mapping radar using VITA 62 compliant power converter
48V 取代 12V:DC‑DC 转换器成为软件定义汽车(SDV)电源架构的焦点
未来汽车将集成多个电压等级。12V、48V 以及 400V 和 800V 高压系统正使电气架构日趋复杂
Digitimes 无人载具技术关键路径研讨会
了解更多关于无人机高密度电源转换的详情
加速向 48V 电源系统过渡
过渡至 48V 电源系统时需要考虑的六件事
DC-DC 电源模块助力桥接 48V 至 12V 转换
供电网络(PDN)正在从 12V 至 48V 架构发生决定性转变
汽车电子正如何发展?
如今,汽车供电网络的征税比以往任何时候都要高。了解 Vicor 如何助力设计更高效的电力系统
2026 年汽车工程展览会
以最高效率和最高功率密度电源模块,应对汽车电气化挑战
设计 48V 供电网络时需考虑并攻克的 15 项技术挑战
为帮助您全面备战 48V 系统迁移,在开启您的第一个 48V 设计时,请考虑以下 15 项技术挑战
面向未来的汽车高压转 SELV 方案
传统的 12V 架构已无法承受车载电子负载的不断增加。了解电源模块如何加速向 48V 的转型
ReVolt 清洁电力系统使传统的重污柴油发电机组变得安静
ReVolt 通过 48V 和高密度电源模块为好莱坞清洁能源的雄心壮志充电。便携式可再生能源为片场提供更清洁、更安静的电力
用于太空应用的人工智能(AI)
人工智能(AI)正以真正产生现实影响的应用程序重塑我们的世界。了解 Spacechips 如何为新一代太空人工智能提供动力
电源模块助力简化电动汽车的爬电距离与电气间隙设计
包覆成型是解决 48V 汽车电源系统中电弧问题的关键
压力下的动力:满足军事领域激增的电力需求
军事电源系统设计者需要更多的性能(功率)和兼容性。了解 Vicor SOSA 电源如何解决难题
48 伏脉冲功率技术可在 60 秒内为汽车玻璃除霜
Betterfrost 实现在不到 60 秒内使用适当的脉冲功率完成汽车玻璃除霜。了解更多关于 Vicor 电源模块如何实现 48V 创新的详情
ReVolt – 技术问答
ReVolt 正在解决好莱坞片场的排放问题,下一步将把便携式 DC 电源应用于建筑工地、应急响应事件等领域
双向供电与快速瞬态响应能力赋能可扩展的主动悬架系统
正弦振幅转换器™(SAC™)模块凭借其独特的双向供电功能与瞬态响应速度组合,为主动悬架系统开辟了全新可能性
提供更高的峰值功率和更快的动态瞬态响应,实现更轻、更强大的电动汽车架构
随着时间的推移,市场上的电动汽车 (EV) 对电驱动系统的依赖程度日益加深,例如线控转向、线控制动以及主动悬架系统等
Spacechips 大电流处理器为在轨 AI 驱动通信供电
小型卫星亟需具备精密计算能力。了解更多低噪声、AI 赋能的电源如何推动创新应用
电流倍增器:为 AI 处理器及其他严苛应用供电的明智之选
AI 处理器需要解决低电压、高电流的严苛挑战,这将会导致电源系统设计产生瓶颈。了解 Vicor 的电流倍增技术如何改变这一现状
应对数据中心 AI 电源挑战
随着 GPU 服务器消耗的电力越来越多,面临的一大挑战就是在提升供电能力的同时将损耗、噪声或停机时间降至最低。
ReVolt 如何利用 Vicor 技术实现电影拍摄的碳中和
Vicor 电源转换器提供清洁、可移动的不间断电源
助力好莱坞实现其绿色愿景
ReVolt 是当今电影片场使用大型化石燃料燃烧发电机的更清洁、更环保的解决方案。了解 Vicor 如何为 ReVolt 助力
2025 年第 16 届电源技术发展论坛
Vicor 展示了高密度 DC-DC 电源模块如何最大限度提升 ATE 吞吐量
加速进入高性能 48V 供电网络
本电子书提供 48V 供电网络的实用设计指南,旨在提升工业产品性能、效率与可靠性
高性能 ZVS 降压稳压器消除在宽输入范围负载点应用中提高功率吞吐量的障碍
当今高性能应用的需求已超越传统调节器所能提供的能力。了解零电压开关拓扑如何助您提升性能
利用固定比率转换器重新定义供电架构
本篇白皮书讨论了固定比率 DC-DC 转换器,及设计人员应该将其视为功率传输架构的重要组成部分的原因
使用多个部件构建更智能的超宽 DC-DC 转换器解决方案
一体通用通常会简化情况。然而,在选择超宽 DC-DC 电源时,这种方法不能提供最佳结果
高性能电源模块封装的特性
电源模块封装技术自创立之初便成为维科公司的独特差异化优势。
创新供电网络
关于 Vicor 如何创新供电网络领域的白皮书。提升终端系统性能所需的电源技术
2025 年第五届中国汽车智能底盘大会
Vicor 展示了在汽车应用中 DC-DC 模块化转换器减轻重量的优势
消除大容量电容,构建更轻的小型电源系统
Vicor 的分比式电源架构™(FPA)在尺寸和重量上都有了明显减少
ReVolt 无碳电力平台为电影拍摄现场供电
拍摄现场的用电强度越来越高,使用发电机组可能会导致工程限制和环境问题
好莱坞进入清洁能源时代:Vicor 电源模块通过 ReVolt 为电影拍摄现场供电
ReVolt 开发了一种更好的方法,通过提供清洁、可移动及不间断的电力,为电影拍摄现场和摄影棚外景地供电
在电动汽车中将高压转换为安全特低电压的 8 大挑战
汽车与轻型电动车出行领域正在面临对于更小、更轻的电源解决方案的需求挑战
问答:Vicor 赋能新一代主动悬架系统
电动汽车不断进化以支持更高性能、更轻重量和更佳驾乘动态,电源系统设计正被推向新的极限
清洁电能减少好莱坞片场的二氧化碳排放
ReVolt 以 48V 高压与高密度电源模块为好莱坞带来清洁能源新动力。便携电源为片场提供更清洁、更安静的电源解决方案
双向桥接转换器解决 12V 转 48V DC 电源转换难题
过渡至 48V 电源分配系统比重新设计传统的 12V 设计更具优势
助力地球上最大的光学望远镜观测浩瀚宇宙
Microgate 开发了自适应光学技术,帮助人们更清晰地观测深空。了解 Vicor 电源模块如何支持他们的任务
汽车主动悬挂系统
48V 电源系统可减少损耗并缩小电源设计。Vicor 使 12V 至 48V 的过渡变得更容易,获得 竞争优势
DC-DC 电源模块助力实现 48V/12V 转换
电动汽车和数据中心已经过渡至 48V 架构以提高电源性能。全新的 Vicor 系列 DC-DC 转换器有助于实现这一转变
精密的自适应光学技术揭开宇宙的秘密
采用 Vicor 功率密度模块的自适应光学系统助力 Microgate 对望远镜的镜面进行机械变形,更好地解析深空的图像
电源模块优化了电动汽车的性能和效率,用于高压到 SELV 的转换
Vicor 将在高功率元件暨转换技术研讨会(Tech Taipei)上分享将高压转换至 SELV 的最佳实践
电源模块加速汽车从 800V 到 48V SELV 的转变之路
Vicor BCM6135 为主动悬挂系统解决了历史性的电源设计问题。双向并快速瞬变的 DC-DC 转换器对全新的设计至关重要
使用模块化电源建构更好的无人机
基于 Vicor 高性能电源模块的供电网络 (PDN) 可为下一代无人机的开发提供创新设计
Vicor 无人机电源模块解决方案技术及应用/案例介绍
Vicor 高性能电源模块如何助力无人机在运输、农业、检查、监视、通信和系留无人机等各个应用领域实现创新
数据中心电力分解
高密度电源模块将在实现人工智能(AI)超级计算机数据中心架构的高压直流配电中发挥关键作用
Vicor 介绍了使用模块化电源实现高效、高密度和可扩展的边缘计算 PDN 的最佳实践
高密度模块电源为边缘计算节省空间并提升成本效益
用于电动汽车供电网络(PDN)的高压母线转换器 48V 电源模块
48V 架构可减少损耗,有助于实现更小、更轻的电源系统。Vicor DC-DC 转换器超越分立式设计,优化电源系统
Vicor 在 2025 年汽车创新日活动展示了高压至安全特低电压(SELV)转换
将高压转换至 SELV 时,软开关拓扑结构和更高频的开关技术可减轻封装重量并减小尺寸。了解有关 Vicor 电源模块的更多信息
纯电动汽车的技术进步正推动销量增长,但车辆安全性和可靠性才是长期生存的关键
Vicor BCM 和 DCM 可轻松实现并联,从而减少 DC-DC 转换器的尺寸,其高效率和高密度可提升性能
2025 中国国际低空经济产业创新发展大会
Vicor 电源模块和专有拓扑结构为 eVTOL 提供顶级的电源系统性能
成功应对汽车电磁干扰(EMI)挑战:问与答
EMI 对车辆性能水平的发展至关重要
这是一个疯狂的 48V 世界
48V 日益普及在以更高效率、功率密度和结构紧凑为优先考虑因素的领域
电源模块助力 Microgate 自适应光学技术聚焦宇宙
Microgate 使用 Vicor DCM3623 系列 DC-DC 电源模块对反射镜进行机械变形并校正大气干扰
DC-DC 转换器赋能网络交换机,实现可靠供电
Vicor DCM3623 通过其专有的控制环路技术,在宽范围输入电压变化下实现了高输出电压稳定性
48V 与高功率密度模块相结合,化解由来已久的主动悬架功率挑战
Hongfa 与 Vicor 合作设计世界上最小的主动悬架功率系统。电源模块与 48V 改变汽车格局
优化高压至 SELV 转换,无需电池和超级电容
了解如何通过快速双向转换将高压电池电源有效转换至 SELV 以支持再生负载
Vicor 出席 Mouser 边缘计算活动
边缘计算对电源的需求产生了诸多挑战。高密度电源模块实现创新和更高的效率
Vicor 在 2025 EEHE 大会发表了混合动力和纯电动汽车电子技术演讲
高功率密度 DC-DC 转换器模块和正弦振幅转换器可实现顶级的系统性能和小型化,以满足最具挑战性的用电情况
轻型电动车:高密度电源转换延长运行时间
了解如何开发更好的供电网络,以提高轻型电动车产品的性能、效率和可靠性
Vicor 展示了电动汽车高压转换至 SELV 的创新方案
高密度模块缩小了供电网络,提高效率以及改善整体性能
高密度功率模块简化和缩小电动汽车电源系统设计
Vicor 电源模块为电动汽车应用注入创新。了解三款汽车级新产品将如何彻底改变未来的电源设计
高密度电源模块推动主动悬架技术日趋成熟
主动悬挂系统已从 20 世纪 90 年代的测试版发展成为今天的 48V 驱动系统。了解电源模块对电源系统设计的影响
世界上最大的望远镜正在帮助人们揭开宇宙的起源
极大望远镜采用由高密度模块驱动的精密自适应光学技术,实现改变世界的发现
2025 台北无人机产业链趋势暨电源系统研讨会,台湾
电源模块为当今先进的无人机提供卓越的性能和创新
先进的电源模块封装优化了自动驾驶电动穿梭车的可用功率、可靠性和安全性
Vicor 的高效电源模块确保最少的散热,降低对复杂冷却解决方案的需求,并最大限度地提升功率输出
为燃料电池供电的 eVTOL 的辅助系统提供千瓦级功率
Vicor 高密度电源模块可有效管理千瓦级功率,减少飞行所需的能量
利用极大望远镜进行深空探索
了解高密度电源模块如何帮助极大地球望远镜增强深空图像
基于 MHz 开关频率的器件助力实现 DC-DC 转换器和 EMI 滤波器的小型化
想象一下,使用 DC-DC 转换器解决方案来利用高频开关的优势,而不会发生传统解決方案的缺点
先进电力电子设备在下一代电动汽车中的重要性
汽车电气化是现下最严峻的电力挑战。高密度电源模块正如何改变着局势
边缘计算的重要性
更快的速度正变得无比重要。了解哪些应用正在蓬勃发展,以及为什么功率密度对未来的发展至关重要
为未来提供动力: GenAI 供电创新
大型语言模型的功耗要求有多惊人?如何降低功耗?了解模块化电源的作用
采用 48V 区域架构,打造面向未来的先进电动汽车
随着原始设备制造商(OEM)采用 48V 电源架构,他们正努力优化其电源系统设计。Vicor 的高功率密度模块可为 48V 区域架构提供峰值效率
助力清洁航空计划
全球范围内,商业航空仍以 4.3% 的速度增长。这对环境造成了许多影响。电源模块正在解决这一难题
提供超过 1kW 的稳定 48V 电压
了解 Vicor 如何高效、轻量化提供 1kW 电压
减少 I2R 损耗,延长任务执行时间
了解 Vicor 如何为系留空中水下无人机 (UAV/UUV/ROV) 提供高功率、高效率和更轻的重量
紧凑、高效的电源解决方案助力增强对抗能力
探索 Vicor 用于电子战对抗系统的高效、轻量化供电网络
支持更多功能、增加有效载荷并延长运行时间
了解 Vicor 如何提供高效的大功率并减轻重量,支持更大的有效载荷,从而助力成功完成任务
高效地为日益增长的先进车载传感器供电
了解 Vicor 如何为空对地 (ASM) 导弹提供高功率、高效率和更轻的重量
采用先进的电源模块,告别电动汽车高压预充电电路
借助高密度电源模块,工程师就可以设计创新的架构,在与车辆预充电相关的各种因素间实现完美平衡
亚洲电源技术发展论坛
了解如何使用高密度电源模块来减小尺寸和重量,同时提供更高的功率和可靠性
高效率、高密度模块为先进的通信技术腾出了空间,并扩大了通信范围
高效型无人机依靠太阳能满足长航时要求
高密度、高功率模块实现更轻巧、安全、经济的线缆设计,延长任务续航能力
这类无人机通过线缆与地面电源连接实现供电和控制,延长任务续航能力
DCM DC-DC 转换器可将内置母线功率增加一倍,有助于最大限度减轻飞机重量
高空长航时(HALE)无人机实际上就是飞行的卫星,设计用于在极高海拔长期运行
在新的 800V 架构中支持传统辅助设备
Vicor 利用单一电源模块进行高密度电源转换,提供了体积最小、重量最轻、效率,将 800V 电压转换为 400V 电压
高密度电源转换使主动悬架成为可能
高密度电源转换器使主动悬挂应用在纯电动汽车全部的四个车轮上成为现实
显著减少 DC-DC 转换装置的尺寸并减轻重量
传统的银盒电源体积庞大、重量较大,工程师难以实现增加续航里程的目标。电源模块可减小尺寸、降低复杂性,同时降低成本,缩短时间,以便为不同平台增减功率
延长配送任务航程、节省空间,增加更多有效载荷
配送无人机必须足够安全可靠,将货物送达目标收件人所在的位置
提升功能性,保障可靠性与生产力
农业无人机面临独特的挑战,需要在各种天气条件下携带重型负载执行长时间喷洒作业
轻型供电网络助力灵活机动的无人机实现远程、大范围巡检作业
巡检无人机用于确保基础设施的完整性、安全性和功能性
灵活、可扩展的供电网络可满足各类视听设备的供电需求
媒体和娱乐无人机必须能够承载重型负载,并尽可能延长飞行时间,确保安全和紧凑
紧凑型电源模块为先进传感器预留空间,提升安全性和性能
巡检机器人能够更频繁地监测基础设施,在问题发生前及时补救,从而挽救生命、节约时间和成本
灵活可扩展的模块化方案支持多系统运作,打造更健康、清洁的空间
这类机器人使用紫外线灯或消毒喷雾来消除学校、仓库、医院和酒店等大型场所中的危险病原体和细菌
高效电源模块实现系统运行时间最大化,提升工作效率
自主移动机器人(AMR)和无人搬运车(AGV)等物流机器人在大型仓储环境中执行库存管理和订单履行任务
采用坚固可靠、高效率的电源模块,最大限度延长恶劣环境下运行时间
收割机器人在农场执行各种任务,通常可以自主运行。配备传感器、摄像头和 GPS 系统进行环境导航
轻巧高效的电源模块延长配送路线并节省空间以装载更多货物
为消费者提供杂货、外卖食品和网购商品的 “最后一公里”配送服务是自主机器人的核心任务
延长飞行时间,支持高性能监控设备,确保安全防护
有效的监控需要不间断的传感和通信能力,以确保重要财产、设备和资产的安全和安防
Vicor 在 Mouser 台北智慧电源管理论坛展示了用于先进测试和测量系统的高功率密度模块解决方案
Vicor 为 ATE 和 BFT OEM 展示了其突破性的高功率模块解决方案
SeaRAY 利用 Vicor 技术转换波浪能
C-Power 提供可靠、经济高效的海浪能发电和储存。Vicor 电源模块支持高效的动能转换
利用高密度电源模块,减轻电动汽车(EV)重量
电动汽车(EV)存在重量问题。Vicor 高密度功率模块与 48V 区域架构相结合,可显著减轻重量并提升效率
随着人工智能(AI)的发展,电力挑战也随之而来
生成式人工智能(genAI)正在给软件、硬件和环境基础设施带来巨大压力。采用电源模块有助于实现更高的电流密度,从而将整体影响降至最低
用于新太空的供电网络
太空环境十分严酷,要求完美的可靠性。Vicor 耐辐射电源模块能承受新太空的严酷考验
固定比率转换器提升电池生命周期效率
功率转换技术限制了电池生命周期的生产率。Vicor 高密度固定比率转换器可实现更高的效率
微型数据中心引领边缘计算未来发展
HIRO 正在实现边缘计算的承诺。使用 Vicor 电源模块的医疗保健、教育和人工智能应用正在欧洲产生影响力
圆桌讨论:SOSA 对军事项目需求和商业实践的影响
航空航天和国防业务部副总裁 John Sturm 在三年后对 SOSA(传感器开放系统架构)技术标准 1.0 进行了评估
面向新太空应用的 DC-DC 转换器
较小的卫星使用模块化方法获取较少的能量,以最大限度减少 I2R 分配损失,最大限度提高效率并改善瞬态响应
固定比率转换器在电池生命周期中释放创新动力
双向 DC-DC 转换器在不断发展的电池生态系统中起着至关重要的作用。了解高密度电源模块如何推动新的生产力
Saab 实现创新使深海勘探更安全、更高效
Vicor 为 Saab UK 最先进的全电动工作级 ROV 提供动力。高密度功率模块实现了紧凑、散热性能强的电源设计
汽车电源向 48V 转型的绝佳时机
对于正在将其车队电动化的汽车原始设备制造商(OEM)来说,减轻重量至关重要。了解如何通过采用 48V 和 Vicor 电源模块来帮助实现这一转变
应对生成式人工智能(genAI)数据中心的电力挑战
AI 训练要求采用一种全新的配电方法以实现最佳性能。Vicor 的垂直供电是最佳方案
Vicor 出席高效率电源与 WBG 技术应用研讨会
高效率电源与 WBG 技术应用研讨会
Vicor 的电源模块赋能全球最先进的全电动工作级水下机器人(eWROV)
Saab UK 推出多功能且环保的 eWROV,使用紧凑、高热效能的电源模块实现世界级的性能
Vicor 提供最大限度减轻车辆重量和 48V 区域架构的解决方案
使用高效率和高功率密度的电源模块化解汽车电气化挑战
Vicor 分享了在电动垂直起降飞行器(eVTOL)中使用其电源模块的可靠性和安全性优势
功率效率和可靠性对于设计高性能的 eVTOLS 至关重要。了解电源模块如何助力设计更小、更轻的 eVTOLS 供电网络
48V 的高科技快捷方式
Vicor 公司的 Greg Green 向 Autoline TV 的 John McElroy 阐述了在 48V 区域架构中使用电源模块的优势
先进的电力电子技术在新一代电动汽车中的重要性
Vicor 的汽车营销总监 Greg Green 分享了为什么在未来的电动汽车设计中,更节能的系统至关重要
生成式人工智能(GenAI)— 助力优化全球功率最密集的计算应用
满足生成式人工智能(GenAI) 的电源需求非常复杂。如今,Vicor 电源模块与垂直供电架构相结合,提供最佳的解决方案
为 48V 后装市场负载供电的未来走向
Vicor 战略客户经理 David McChesney 对这一过渡可能需要的时间提出了一些令人惊讶的见解。以及后装市场负载供电与向 48V 过渡将产生哪些短期和长期影响
设计 48V 区域架构,确保纯电动汽车(BEV)电池组持续提供高压电源
Vicor 现场应用工程师 YK Choi 和 INFAC 首席工程师 YoungJae Kang 讨论了将 48V 转换器集成到电池组中会如何在 48V 分区架构中减轻热量、成本和重量
在纯电动汽车(BEV)中利用现有硬件消除高压预充电
Vicor 汽车首席现场应用工程师 Patrick Kowalyk 将讲述任何高压母线都需要一个预充电电路来减少一段时间内的电流变化(称为 dv/dt)以保护纯电动汽车中的电子设备
为开关频率高于 1.3MHz 的高压转换实现 EM 传导辐射合规性
Vicor 高级战略应用与系统工程师 Nicola Rosano 解释了在采用高频 DC-DC 转换器电源系统中,由于其固有特性,要解决电磁干扰 (EMI) 问题是一项严峻的挑战
MOSA(模块化开放系统方法)行业与政府峰会暨博览会,2024 年 6 月 17 日至 18 日
MOSA 峰会探讨了用于设计 SOSA 标准和 VITA 62 电源的开放式标准架构
电源驱动创新电子书:第 2 卷 — 保护并挽救生命
保护和提供救生材料和服务的创新解决方案
电源驱动创新电子书:第 1 卷 — 拯救生态环境
保护和维护环境的技术突破
电源驱动创新电子书:第 3 卷 — 改变一切可能
挑战设计和性能界限的技术进步
探索水下机器人(ROV)的电源动力学
在水下应用激增的推动下,水下机器人(ROV)市场迅速增长。Vicor 电源模块帮助客户创新,支持全新应用
电源模块推动创新
Vicor 电源模块使用创新的拓扑结构、架构和封装解决了当今最严峻的电源挑战
EEHE 2024 国际大会,德国
Vicor 在德国班贝格举行的 EEHE 2024 上发表技术演讲和海报演示,介绍了使用高密度电源模块的优势
从派克峰到 Bonneville 盐滩,Lightning 的速度超越内燃机摩托车
Lightning Motorcycles 所设计的全电动摩托车在各个领域表现出色。了解 Vicor 电源模块如何支持这款新一代摩托车
高性能电源模块推动电池生命周期的发展
了解电池的生命周期,以及如何使用高性能、功率密度高的模块来降低成本、减小体积和提高效率
2024 年 WXC 国际汽车设计工程展
Vicor 将在 2024 年国际汽车设计工程展 (WCX™) 上发表五篇论文,详细介绍其 800V 和 48V 电源转换的创新方案
应对电动摩托车电源转换挑战
在结构紧凑、轻量级的车辆中管理电气噪声是一个长期存在的阻碍
自主安防机器人
Knightscope 为公共安全提供突破性技术
特约播客: 国防工业采用的标准化电源优势
在此前,一旦您了解了电源模块的设计优势,认真考虑供电网络可能成为您的优势
紧凑型电源模块推动汽车电气化
电源模块可应对复杂的电气化挑战,为解决当今最严峻的电源挑战提供创新的空间
48V 电源系统: 汽车制造商告别 12V 时您需要了解的信息
随着汽车制造商走向电动汽车 48V 电源,越来越多的汽车制造商开始考虑采用区域电源架构。48V 电源领域的领导者 Vicor 使用电源模块优化供电网络
Vicor 的 48V 供电架构可以支持 12V 系统
原始设备制造商无需立即升级 12V 设备,即可享受 48V 的优势。多功能电源模块可轻松实现 48V 至 12V 的转换
特斯拉宣布采用 48V 汽车电源系统
特斯拉认为 48V 电源很快就成为新的 12V 电源。缩小尺寸、减轻重量和提高功率效率是其中的几个优势
高带宽电源模块消除高压线路纹波抑制的干扰
与传统解决方案相比,Vicor DC-DC 转换器结合了高带宽和软开关拓扑结构,可更有效地降低电动汽车纹波抑制
传统方法无法解决纯电动汽车的重量问题
纯电动汽车越来越重,采用 48V 区域架构可以减轻重量。高密度电源模块可最大限度地减轻重量并提高效率
HIRO 利用高性能微型数据中心将欧洲推向边缘计算的前沿
从支持脑部手术到推动节省成本的智能工厂 —— HIRO 正在利用创新的计算概念将欧洲推向边缘计算的前沿
电动汽车(EV)双向供电:实用且创新的电源模块使用机会
双向电源模块可实现车辆到电网的能量流和其他富有想象力的供电机会。了解有关 Vicor 电动汽车电源模块的更多信息
耐辐射性已成为新太空卫星设计的新难题
Vicor 电源模块功率密度高、可靠且可扩展。此外,软开关在耐辐射电源系统具备诸多优势
实现电气化转型的创新电源解决方案
在本电子书中您将了解到 Vicor 创新电源解决方案如何助力电气化转型
亚洲电源技术发展论坛
利用电源模块打造更高效的新能源应用
电源模块为电动汽车提供 400V 与 800V 系统的高效转换
保时捷、现代和通用今天都在以截然不同的方式实现 400 — 800V 的转换。进一步了解电源模块堆叠至这些分立式设计的方式
VideoRay 利用 AI 及当前最新技术推动安全、高效的水下探索
Vicor 电源驱动创新播客讨论了水下机器人应用的激增以及 VideoRay 如何应对新的水下任务
第六十届 AOC 国际研讨会暨大会
本年度首屈一指的电子战/雷达技术盛会
更好的设计 - 电源管理架构
电源管理及其效率新型电源管理架构的需求及其承诺的改善
2023 年电力电子技术研讨会
了解 Vicor 电源模块如何支持各种电源组合,并具有可扩展性和热适应性
Vicor 电源模块为卫星通信设立了新的标准
在 Space Tech Expo Europe 上探索尖端电源解决方案
为什么要选择电源模块,而不是分立式电源解决方案?
与 home-grown 的分立解决方案相比,使用电源模块有很多优势。了解电源模块如何让您的下一次设计更简单、更快速。
Greg Green 谈“下一代电动汽车技术革新”行业见解
EETimes 主办了一场关于“下一代电动汽车技术革新”的专题讨论会。了解 Vicor 的 Greg Green 对于使用电源模块的看法
地球上最好的电池是免费的,它正在为蓝色新经济提供动力
C-Power 自主海上发电系统 (AOPS) 漂浮在海面上,捕捉机械波能并将其转化为可用的电能
高性能计算电源常见问题
高性能计算中 Vicor 电源解决方案的常见问题汇编
Vicor 在 Tech Taipei 上展示了电流倍增器技术如何最大限度提高运算性能
了解使用电流倍增技术最大限度提升计算性能的优势
Embedded Executive:与 Patrick Kowalyk 讨论汽车
优化电动汽车高压(800V/400V)供电网络面临诸多挑战。了解高功率密度电源模块如何创造新可能
Lightning Motorcycles 加速进入电动车赛事世界纪录榜单
Lightning Motorcycle 打造了全球最快的电动摩托车
电池化成与测试
高压电池制造面临着一系列经济挑战。了解 Vicor 解决方案如何缩短电池化成与测试时间,同时降低成本
2023 IT Media 线上大会
Vicor 分享了利用高密度电源模块设计创新且高效的供电网络方案
汽车行业是否为模块化动力系统及 48V 电池做好了准备?
在汽车电气化的竞争中,模块化电源设计正获得更多青睐。尺寸、重量和设计灵活性使它们成为完美的选择
Vicor 工程师 Chris Swartz 入选电气电子工程师协会高级会员
Chris Swartz 荣获 IEEE 高级会员称号。这是只有 10% 的会员才能拥有的精英地位。Chris 在 Vicor 任职 15 年
模块化方法解决 48V 电源架构电气化难题
Vicor 功率密度型电源模块是加速汽车电气化的最佳途径。它们灵活、轻便且易于使用,了解更多详情
为高性能计算市场提供动力
Vicor 人工智能和高性能计算副总裁 Ajith Jain 在 Electronic Specifier 播客中谈论了高性能计算市场电源的趋势和发展
轻量高效的 LED 电源设计采用 48V 电源模块
LED 显示屏的尺寸越来越大、价格越来越高,运行成本越来越高。Vicor 功率密度模块体积更小、重量更轻、运行效率更高
为变革提供动力
Vicor 公司首席执行官 Patrizio Vinciarelli 悄悄地解决了地球上最棘手的电源困境——汽车电气化以及为人工智能提供动力
Vicor 在 NSREC 2023 上展示了业内领先的低地轨道和中地轨道卫星电源解决方案
Vicor 耐辐射 COTS 电源模块经优化,可为当今更先进、更高功率的 ASIC 和处理器供电
Vicor 将在慕尼黑举行的汽车高压电源系统大会上介绍如何利用 48V 电源加速 xEV 设计
Vicor 在慕尼黑汽车高压电源系统大会上发表演讲。了解高密度电源模块如何利用 48V 电源加速 xEV 设计
Patrizio Vinciarelli 创立 Vicor,解决电源转换难题
40 多年来,Patrizio Vinciarelli 一直是电源电子领域的创新者。如今,他正在应对这个时代最紧迫的电源挑战
Vicor 针对逆变器纹波电流推出突破性模块化解决方案
Vicor 在 EEHE 大会上介绍了减轻电动汽车逆变器纹波电流和电压的解决方案
新一代氢动力无人机正在进行搜索救援,挽救生命
斗山救生无人机使用氢燃料电池和高密度电源模块,使飞行时间比使用锂离子电池长 5 倍之多
为关键任务型应用提供创新的可靠电源解决方案
技术资源合集,旨在教育用户在航空航天、国防和太空应用中使用模块化电源的优势
测试与仪器仪表术语表
常用的测试与仪器术语综合清单
电池化成和测试术语表
常用的的电池化成和测试术语综合清单
ATE 术语表
常用的自动测试设备术语综合清单
自主安防机器人以超人的灵敏度及探测能力进行巡逻
公共安全的风险正在上升,机器人提供的更好的监视和拦截就是答案。了解 Knightscope 公司选择 Vicor 电源模块为安防机器人供电的原因
从玩具到建筑工地工具,OLogic 加速机器人构想从概念到生产的进程
OLogic 称赞高密度电源模块将推动当前机器人变革
Vicor 在 Dixie Crow 研讨会上展示了世界级的电源解决方案
Vicor 电源解决方案提供了更高的功率密度,军事设计师可在电源尺寸和重量预算上花费更少
2023 年 WXC 国际汽车设计工程展
Vicor 展示了多功能电源模块如何应对汽车电气化挑战
VITA62 3U 评估板
OLogic 与 Vicor 助力 Dusty Robotics 优化建筑机器人电源
OLogic 与 Vicor 合作优化 Dusty Robotics FieldPrinter 的电源和系统功能
电源转换器实现了机器人应用的创新
最大限度减少尺寸和重量在机器人设计中十分重要,但提高功率对于支持新的传感器、外设和功能来说至关重要
电气化时代是否仍然离不开 12V 电池?
目前的纯电动汽车由 400V 或 800V 的电池供电。 那么还需要 12V 的电池吗? 了解小巧的电源模块如何取代 12V 电池
CCell 公司的可再生能源正在扭转海岸侵蚀,同时加强海洋自然生态系统
CCell 以生态友好的方式种植珊瑚礁,这比自然生长出珊瑚礁的速度更快
高密度电源模块提升新一代移动机器人性能
在机器人设计中,最大限度缩减尺寸和重量相当重要,但是为了支持新的传感器、外设和功能,提高功率是必不可少的
MOSA 电源、定制组件、工程人才:与 Vicor 的 John Sturm 的问答
SOSA 提供了一定程度的标准化。MOSA 从系统的角度能够确保硬件与软件开发的兼容性和互操作性
CCell 荣获 2022 年 Elektra 年度最佳电源系统产品大奖
CCell 正在通过使用可再生能源和 Vicor 电源模块加速新珊瑚礁的生长,扭转全球海岸侵蚀的局面
如何应对艰巨的耐辐射电源电子系统设计
在处理现代 ASIC、FPGA、CPU 和 GPU 消耗的大电流时,优化配电网络(PDN)非常关键
电源模块为未知的电动汽车电源挑战提供了全新可能
在经济上,汽车电气化有众多悬而未决的问题。这可能是我们这个时代最重要的电源挑战
垂直供电助力尖端数据处理
新的发展对电源系统设计者提出了管理 PDN 阻抗压降、瞬态性能规范和功率损耗的挑战
Vicor 公司荣获“2022 马萨诸塞州年度制造商”称号
在首座 ChiP™ 制造工厂开业后,Vicor 已成为马萨诸塞州公认的制造领先企业
什么是 "数字电力"?它与 Tesla 和 Edison 的交 – 直流电相比有何优势?
Voltserver 通过数字电力™ 实现真正的数字化转型
现在启程登上通往未来的航班,乘坐碳排放更低的 Ampaire 混合动力飞机
Ampaire 正在开发将引领行业走向全电动未来的混合型电动飞机,实现零碳排放和更绿色的未来
Dragonfly 公司的新型悬停系留无人机如何突破海上通信限制?
DPI 系留式无人机将通信天线提升至 500 多英尺高,将海上通信线路从 8 英里增加到近 30 英里,提升至 3 倍之多
Vicor 凭借尖端电源技术,积极应对工业设备市场电气化/高功率化的发展趋势
Vicor 凭借尖端电源技术,积极应对工业设备市场电气化/高功率化的发展趋势
航空航天与国防的常见问题
关于 Vicor 电源解决方案在航空航天与国防应用中的常见问题汇编
航空航天与国防术语表
一份全面的常用航空航天与国防术语表
Vicor 提供电源转换突破,为机器人革命提供动力
OLogic 结合 Vicor 公司先进的集成式电源模块推动新一代移动机器人
2022 开放计算中国技术峰会
电流倍增技术的进步可实现新的人工智能处理器电源解决方案
车载充电器是双赢解决方案
续航焦虑是采用电动车的最大障碍。 了解如何通过车载电源转换器而非建设更多充电站来解决这一问题
重新定义电力分配方式
Voltserver 在数字电压系统的接收部分采用 Vicor BCM6123 固定比率母线转换器
重新定义汽车供电网络
使用符合车标的高密度 DC-DC 模块对电动车的高压电池进行转换,为汽车制造商节省了重量和空间
利用可再生能源加速珊瑚礁生长应对海岸侵蚀
PRM 和 VTM 组合可让合理的高压 DC 以高效的方式在相对较高的电流下转换为相当低的 DC 电压
Vicor 电源模块推动卫星互联网星座
Vicor 高效率、高密度、大电流的解决方案在新的太空模型中发挥了良好的作用
解决新能源车快速充电站的兼容问题
您正应对电动汽车 400V 和 800V 充电困境吗?Vicor 提供最可靠的方式来消除任何 DC 快速充电站的兼容难题
Vicor 称其美国 "ChiP "工厂为行业首家
即使在最恶劣的环境中,像这样的 Vicor ChiP 电源设备也能持久耐用
Vicor ChiP 工厂 - 自动化与可持续生产
Vicor 垂直集成工厂采用专利工艺,使 Vicor 能够生产制造高质量、低成本和可靠的电源模块
世界首座 ChiP 制造工厂
Vicor 正为我们的员工与客户向未来投资
Vicor 完成 95,000 平方英尺的 ChiP 工厂扩建
新的 ChiP 工厂采用拥有专利的制造工艺使 Vicor 电源模块与众不同,实现最密集电源和能源效率解决方案
高密度模块化电源系统的 PCB 布局与散热设计
用于人工智能处理器的高密度负载以及超级计算已经变得成熟和快速,我们必须继续推进电源组件的容量
国防电子支出寻求在关键应用领域克服 COVID-19 挫折的方法
随对 COVID 以及全球经济与安全的关注,Vicor 预计无人驾驶车辆部署和 ISR 技术方的研发投资将增长
跨学科的专业知识和强大的功率密度推动新的移动机器人技术革命
Ologic 和 Vicor 合作进行机器人设计
固定比率转换器在大功率供电系统中的用武之地
固定比率转换器的密度和效率在实现PDN架构提供高性能方面起着关键作用
救生系留无人机在功率和通信技术上得到提升
最初设计的 DC-DC 转换器很重,消耗过多的空间。Vicor 轻型 DCM 为该应用提供理想的功率和重量
开启超级计算性能
Vicor 为需要更多效率和功率的传统系统提供一个简单的选择:使用双向 NBM™ 非隔离母线转换器
如何复刻 12V 汽车电池
Vicor 高密度母线转换器模块技术实现理想的电动汽车架构
高密度电源转换:更小的体积,更大的功率
纯电动汽车与插电式混合动力电车的销售量正在迅速增长
研究预测:高密度电源需求随着新太空任务而激增
卫星电源设计师必须提供比传统系统多 20-30 倍的电流,同时减少电源传输网络的尺寸、重量和成本
Rob Russell 分享他对近地轨道和中地轨道卫星部署的行业未来见解
Rob Russell 在 Microwave Journal 与 Pat Hindle 讨论近地轨道与中地轨道卫星市场趋势
边缘计算在可扩展的微型数据中心使用模块化电源
HIRO 边缘计算应用提供实时数据以改进脑外手术技术。了解 Vicor 电源模块如何满足高性能需求
优化供电网络
优化供电网络(PDN)不可避免地以系统的让步而告终。使用电源模块,让步更小,性能更佳。
利用模组化电源打造更好的无人机
Vicor 模块化电源优化了有效载荷,增加无人机飞行时间。它们在保证轻量的同时兼备功率密度,灵活,可轻松扩展
新型高密度电源解决方案帮助全球网络连接成为现实
地面宽带无法跟上对互联网带宽的需求。了解电源模块如何使卫星填补这一空白
太空与卫星常见问题(FAQs)
相信电源专家 Vicor 能帮助您解决您在太空中最棘手的 LEO 和 MEO 卫星电源设计难题。
数字电力能够在远距离情況下安全传输电能
与以太网供电相同,Digital Electricity™ 可使用低成本、现成的数据电缆在长距离(长达 2km)内安全地传输高达 2kW 的电力
为海浪能采集实现重大工程突破
采集海洋能,为海上资源提供可靠的、经济的海洋能源发电和存储、海上数据与通信服务
功率密度:实现全球网络覆盖难以察觉的关键技术
从专家那里了解为中低轨道卫星供电的快速发展趋势,用于当今太空中先进的通信网络
2022 年 WCX 国际汽车设计工程展,2022 年 4 月 5 日 - 7 日
Vicor 介绍了三种为 xEV 供电的全新功率密集型方案
无人机在自然灾害中实现救生通信
Fukaden 无人机正在为救生人员提供快速、可靠的移动通信服务
模块化设计促进汽车电气化
类似于以太网供电,数字电力使用经济的、现成的数据电缆能够在长距离(长达 2km)范围内安全传输高达 2kW 电力。
为新太空设计供电网络的挑战与设计考量
了解设计一个更好、更可靠的供电网络的基本知识,为 LEO 和 MEO 通信卫星提供顶尖性能。
Vicor 与 Voltserver™ 合作开发数字电力
数字电力可帮助运营商能够使用现成的数据电缆在 2km 范围内安全传输高达 2kW 的电源。Vicor 提供 DC-DC 转换
2022 年能源预测:超密集供电网络正在重塑未来
无人机和机器人正在被部署到更多危险类型的移动作业中。Vicor 功率密集型模块使这些应用的供电变得容易。
数字电力为电力传输带来智能性与安全性
Digital Electricity™ 提供了低电压的优势,同时具备交流电的功率和远程性能(长达 2km)。Vicor 提供 DC-DC 电源转换
“新太空”需要高密度电源,才能跟上预计 20 倍的增长步伐
实现全球互联网覆盖需要什么?是大量的电力。了解 Vicor 将如何在未来 10 年内使互联网带宽提升至 20 倍
耐辐射的电力电子技术是填补卫星基础设施缺陷的关键
Vicor 的创新电源解决方案帮助数十亿入接入高速互联网,为那些被限制或无法接入网络的人提供宽带连接
帮助美国海军将海浪转化为持续的电能
Vicor 和 C-Power 利用 C-Power 的 SeaRAY 为美国海军开启新机遇,SeaRAY可在海上提供局部发电和数据服务
将 12V 电池缩小一半并保持冷启动?
通过正确调整 12V 电池的尺寸以满足您的持续使用状态,您可以节省多少空间和重量?了解如何使用电源模块
太空术语表
用这个方便的太空、卫星术语词汇表来学习星星的语言
优化高密度电源设计:模块化与分立式孰优孰劣
在评估电源模块设计的过程中,有几个重要的设计变量需要考虑
捕获海洋能
拍打世界各地海岸线的海浪,可产生高达 2 - 300 万兆瓦的总电能。如果我们能利用这种能量,会是什么情况呢
能源发电新浪潮
尽管海洋能落后于太阳能和风能,但它可能具有最大的潜力
HIRO 提供紧凑、可扩展的边缘计算
边缘计算对于充分发挥人工智能(AI)、机器学习和物联网(IoT) 的全部潜能至关重要
使用老式的硅 MOSFET 增加功率密度
使用高压和模块化电源方案来设计电源系统,最大限度减少妥协和折中,使硅 MOSFET 的寿命更长
与 Vicor 合作,加速汽车电气化
克服快速充电障碍,转换高压并桥接 12V 和 48V 应用
集群式 AI 处理器供电方案
垂直电源方案可提供高达 100kA 的电流和多轨核心电压传输
C-Power 和 Vicor 为海上应用提供高效、可再生的能源
C-Power 开发的电力系统可从海浪中持久产生并存储 10W 到 1MW 的能量
12V 铅酸电池即将退出市场?
充分利用电动车高压电池,更有效地提供 12V 电压
面向新太空应用的紧凑、高密度、高效率 DC-DC 转换器
卫星运营商正在提供复杂的机载处理能力
Digital Electricity™ 实现真正的数字化转型
建筑物、农业以及露天体育场的数字化,需要部署智能边缘传感器,以便将实时数据传输至云端
汽车电气化:48V 即为新的 12V
车辆有许多不同的电源要求,更加灵活和更具可扩展性的模块化供电方法能够应对这些挑战
最高功率密度转换打造更好的无人机
自主无人机(UAV)和无人机的激增彻底改变了从农业到紧急响应的各个行业
为兼容电动汽车基础设施铺平道路
车载转换使电动汽车能够在任何电站充电
无人机的模块化供电网络
我们能发现工程师们当下所面临的关键挑战是对能够提供更高功率且更小、更轻的电源设计需求
为高性能计算提供强大动力
分比式电源架构提供更低的内核电压与更高的内核电流,同时提供更低耗损与更高效率
使用模块化电源加速 xEV 发展
克服汽车电气化的三项关键障碍,包括分立式 48V 配电和 400V/800V 充电兼容性
面向系留无人机应用的 DCM
系留无人机的需求十分苛刻,因为减轻重量是一个关键要求。Vicor DCMs 为这种类型的应用提供了最佳解决方案
利用海浪为远程海洋应用供电
由于环境条件不可预测,海洋勘探具有挑战性
使用模块化电源构建更好的机器人
在机器人应用中使用模块化电源的实际案例
Dragonfly Pictures 公司无人机将舰艇直线对传式无线电通信范围扩大近 4 倍
部署 800V 高压电源使系留无人机能够通过使用更薄、更轻的系留电缆,最大限度地减少阻力与损耗
燃料电池无人机运送人道主义物资
氢燃料电池无人机使用高密度电源模块执行海外人道主义救援任务。创新的供电网络可延长 4 倍飞行时间
设计机器人动力架构前需要考虑的六个问题
功率密集型模块是最佳的机器人解决方案,它提供了紧凑、轻型和可扩展的电源,高效灵活
汽车电气化竞争:获胜的途径
为了实现其积极的电气化目标,原始设备制造商需要使用高密度、可扩展的电源模块实现供电网络创新
创新电源模块封装
电源模块封装是一个独特的差异化因素,使 Vicor 在 40 年内将功率密度提高了500 倍以上
在 48V 架构中使用高密度功率转换器构建更好的机器人
本指南的内容涵盖了开发更好的 PDN 以满足当今机器人系统需求
电源系统设计工具: 快速简便地配置完整、高效率、紧凑、多项输出的电源系统
只需填写输入和输出功率及基本系统要求,即可轻松设计电源系统和/或选择合适的模块
WiBotic 和 Vicor 为机器人提供自主无线充电
Wibotic 自适应匹配系统是提高机器人队伍生产力创新方法的基础。Vicor 电源模块支持无线充电
氢燃料电池供电将无人机的飞行半径扩大 4 倍
氢燃料电池无人机的续航时间是锂离子电池的 4 倍。Vicor 电源模块实现了斗山创新、高效的供电网络
电源解决方案减少超声波管道检测停机时间
电源解决方案通过传感器、摄像头和板载处理器的升级减少停工时间
Vicor 为移动机器人及无人机下一代无线充电的强劲电源需求提供有力支持
下一代机器人的生产力依赖于支持自主无线充电的功率密集型模块
基于模块的紧凑型高压供电网络助力克服系留无人机供电系统的挑战
通过部署基于模块的紧凑型电源网络优化系留无人机的性能。高电压使系留电缆更薄、更轻
自主无线充电技术让机器人不断前行
Wibotic 与 Vicor 合作开发增强型电源系统,该系统可提供自主无线充电,优化机器人和无人机的性能
模块化水下机器人迅速适应当前危险的水下任务
VideoRay 的模块化设计方法为快速设计 ROV 提供前所未有的高灵活性,可充分满足定制任务需求
如何设计模块化 DC DC 系统,第 1 部分:四个阶段的设计
如何设计模块化 DC DC 系统,第 2 部分:滤波器设计
如何设计模块化 DC DC 系统,第 5 部分:负载考虑因素
如何设计模块化 DC DC 系统,第 4 部分:安全保护系统
如何设计模块化 DC DC 系统,第 3 部分:稳定性分析与解耦
一款适用于所有机器人的无线充电器
随着机器人队伍重塑物流、配送及检验行业,对更高效、更灵活充电解决方案的需求也在不断提升
高密度、模块化供电网络优化移动机器人性能
高效的固定比率降压与升降压转换器可实现更长的续航时间、更长的持续时间和更大的有效载荷。
机器视觉系统在相同的空间中拥有更大的能量
机器视觉系统通过减少检测时间并提高准确性,显著提高了吞吐量,提高了自动化生产线的产品质量
用医学膝关节手术机器人改进手持工具的人体工程学
微型机器人工具有助于缩小手术范围
宽输入电压为高架龙门吊机器人催生非接触电源解决方案
许多专门制造重型设备的工厂可通过高架龙门机器人获益
高效率转换器助力最大限度延长运行时间
高效率转换器助力最大限度延长运行时间
下水道检查机器人的轻量级低噪声解决方案
在不增加重量的情况下,为更多传感器供电,以提高自主性、移动性和人工智能(允许深度学习),这使得检查机器人能够取代人类
增加巡逻,减少充电的安防机器人
新的传感器的加入,如激光雷达(光探测与测距),再加上先进的板载 AI 处理器,使得自主机器人能够更安全地与人类互动
更轻的电缆为系留无人机开辟全新市场
电源模块可支持高效系留监控无人机,可自由派遣飞行,进行跟踪和追查。
面向航空产业的环保电力系统
平均功率技术为织布机节省成本
平均功率技术节省成本
矿产勘探仪器在恶劣环境下可靠运行
在较浅位置钻矿时,使用电动螺旋钻头可显著降低复杂性和成本
DC-DC 转换器助力实现延长系线
DC-DC 转换器助力实现延长系线
在极低电压下为卫星天线提供大电流
小型、坚固且可靠的纤薄电源解决方案适用于在极低电压下提供大电流的天线需求
双向转换器将电池阵列缩减为一个电池,用于便携式 X 光系统
采用全新固态 X 光技术,医疗 X 光扫描仪不仅可增加便携性,而且还支持电池供电,有助于医疗专业人员在任何地方对患者进行检查
高密度电源助力隐藏 5G 室内小型蜂窝基站
高密度电源助力隐藏 5G 基站
面向 UAV 的全球首款商用氢燃料电池组
业内领先的无人机飞行范围
强大的模块化电源
供电网络正在迅速发生改变,其电力需求需要宽泛的模块组合以实现最大化
采用模块化电源迎接高功率航空航天与国防应用的挑战
航空航天和国防市场继续减小电源系统的尺寸和重量,同时要求满足更大的功率
国防与航空航天:利用 SWaP 限制为边缘技术供电
为 VPX 实现 MILCOTS 标准化。了解 Vicor 如何在提供功率的同时优化尺寸和重量,超越当今对坚固耐用电源的需求
电源系统配置工具用户指南 602
世界首个大型房车锦标赛进入混合动力时代
新型混合动力发动机采用创新超轻的 48V 锂离子电池组以及智能电源管理系统
将 400V 转换为 SELV 系统电源
Vicor 的 Ian Mazsa 与《电子工程师杂志》(EE Journal)一起讨论了使用高压电源的最佳实践与好处
系留无人机电源匹配
利用实际应用探索新技术,开发系统结构和选择功率元件以满足电源转换需求。
当今的汽车需要更大的电源和更轻的重量
了解 Vicor 如何满足对更小、更轻的车辆需求以实现更低的二氧化碳排放量
新型系留无人机彻底改变了机动性和远程通信
系留多旋翼无人机用于在最极端的天气条件下跟踪和跟随移动主机平台
BCM 将高压电池转化为 SELV 系统
消除电动汽车供电架构中的中间储能。阅读 Vicor 有关 BCM Selve 系统的白皮书
系留无人机供电设计指南
升级无人机的功能会增加有效载荷的重量,因此您的电源需要高功率密度且扩展灵活以适应变化
航空产业的环保电源系统
航空业正在经历飞机电气化发展,分析电力航空的性价比优势
提高 48V 配电性能
传统的供电网络(PDN)面临着提供更高性能的巨大压力
避免常见的 AC-DC 设计缺陷
本网络研讨会将提供一个获得成功的简单方法,涵盖诸如电源阻抗注意事项、涌流、滤波器共振和阻尼、PFC、故障、保险装置、系统稳定性和安全性等主题
汽车电源设计中的关键权衡
与传统内燃机汽车相比,电动汽车的耗电量最多可增加 20 倍
消除电动汽车供电架构的中间储能
Vicor 固定比率转换器将高压电池转换为 48V 及 12V SELV 系统
高密度 DC-DC 转换器提供 22A 的电流,可为 MIL-COTS 提供 Sn/Pb BGA 选项
Vicor 为 MIL-COTS 应用增加了一款 3V 输出的降压控制器的 Pb 兼容版本
采用可再生能源和分比式电源加速珊瑚礁的生长
精确的电源转换与可再生能源的调节
Vicor 电源模块为电动汽车提供充电、供电和转换支持
提供给汽车中不同负载的电源从 12V 变为 48V,从而减轻汽车的重量
处于十字路口的供电网络
许多行业所需的功率水平不断提高,电源系统设计人员正在将其 PDN 提高至 12V 以上以缓解电源交付方面的挑战
用更小、更轻的电源模块加速汽车电气化
了解如何通过快速充电、高压转换以及桥接 12V 与 48V 应用克服障碍
收割、搬运和配送机器人的最高效供电
了解 Vicor 如何为各种机器人提供高效并且减轻重量的高功率电源模块
Phasor 使用分比式电源架构实现强大的移动宽带连接
Phasor 使用分比式电源架构实现强大的移动宽带连接
分比式电源加速珊瑚礁恢复
可再生能源的使命是通过大规模恢复和栽种新的保护性珊瑚礁来抗击对海岸的侵蚀,改善海洋生态系统
PSDcast – 机器人和无人机产品的自主无线充电将重塑自动化生产的未来
WiBotic 介绍了如何为任何机器人、任何基站的电池构建自主无线充电平台从而实现更长的运行时间
采用高效、可扩展的电源组件打造电动航空产品
对二氧化碳 (CO2) 排放不断上升的担忧日益加剧,刺激了全球对纯电动汽车及混合动力电动汽车的需求
48V 是汽车电源的未来
在汽车市场上,48V 电源技术正在迅速发展,以充分满足纯电动汽车、混合动力汽车以及轻度混合动力汽车的需求
无线充电为机器人和无人机提高新一代生产力
机器人和无人驾驶车辆(UV)车队正在重塑自动化与生产的未来
分布式电源架构在汽车市场有何优势?
区域式供电是汽车行业开始出现的一种现象
高性能 PCB 布局和散热设计技术
本次研讨会将涵盖 PCB 设计的各个重要方面,旨在最大限度改善热传递,最大限度降低供电阻抗与损耗
利用固定比率转换器重新定义供电架构
日益发展的电源及高级散热技术如何融合,满足人工智能、超级计算及云数据中心的需求?
使用区域电源架构解决汽车电气化难题
电气化有很多选择,大多数制造商都选择 48V 轻混合动力系统,而不是全混合动力系统
Electronic Specifier: 电源产品的十字路口
高性能电源系统的设计复杂性逐年递增,现已达到的程度预示着该行业已到达一个开创性时刻
正确完成模块化 DC-DC 系统设计
您将了解输入输出滤波、保护、与电源的兼容性以及负载动态等主题
Mouser: DC-DC 转换器提供优异的电源系统性能和连接性
DCM 凭借其高频零电压开关(ZVS)拓扑,在其指定的输入线路范围内始终提供高效率
Mouser: 高功率、零电压开关 DC-DC 转换器始终提供高效率
Vicor DCM3623 产品系列是隔离式稳压 DC-DC 转换器,可从未稳压的宽范围输入,生成隔离式输出
Mouser: 新型 DC-DC 电源转换器充分满足最严格的轨道交通车载应用需求
Vicor DCM2322 系列隔离式稳压 DC-DC 转换器可为轨道交通、国防、航空航天、过程控制以及工业应用提供高效率和高功率密度
Digi-Key: 为现代轨道系统供电
DCM2322 是一款隔离式稳压 DC-DC 转换器,其高频零电压开关拓扑可实现支持高密度滤波的纤薄设计
Mouser: 双向 48V 至 12V 转换支持 98% 的峰值效率
NBM2317 是一款用于 48V 及 12V 系统的桥接转换器,实现低成本的高密度和高效率
Mouser: 高效率负载点稳压器
Vicor PI3523 ZVS 开关稳压器为高效率稳压器,在高密度 LGA 系统级封装中高度集成控制器、电源开关、放大器和支持组件
Mouser:直接至负载点的宽范围稳压器
ZVS 架构不仅可在最大限度降低开关损耗的同时,最大限度提高效率,而且还可针对线路及负载瞬态提供快速的动态响应
Digi-Key: DC-DC 转换器,可为创建更小、更轻、成本更低的电源系统提供所有必要的性能及特性
Vicor ChiP 封装技术的散热与高密度优势,可帮助客户实现低成本的电源系统解决方案
Digi-Key: 高性能降压稳压器可在不降低吞吐量的情况下缩小尺寸
PI3325 ZVS 降压稳压器采用 10 x 14 毫米 LGA 封装高度集成控制器、电源开关和支持组件
Electronic Design:采用分布式 48V 电源架构解决汽车电气化难题
这一电气化的新方法可能将是下一个重大突破
分比式电源架构:实现板载电源的高密度和高效率
Factorized power 是分比式电源架构(FPA) 的简称,用于满足大电流板载电源需求
电源系统设计:少即是多
Vicor 提供更小、更高效的模块,帮助设计人员应对这一挑战
Bodos: 打破汽车内部的传统电力供应
为了应对日益复杂的挑战,特别是针对未来的电动汽车,Vicor 提供了一系列适配的转换器
采用 48V 电池
现代电动汽车和混合动力车的车辆电气要求采用 48V 电池
迎接现代铁路的电源挑战
Vicor 的产品市场及商务拓展总监 Michael Schipani 与 Chalk Talk (EE Journal) 的主持人 Amelia Dalton一起坐起来讨论铁路工业的电源挑战和趋势
Digi-Key: 将 12V 高效桥接至 48V
Vicor NBM2317 是一款非隔离式、固定比率 DC-DC 转换器。该双向转换器采用独特的开关拓扑及封装,可将 12V 桥接至 48V
DCM 设计指南
SM-ChiP™ 回流焊接建议
带稳压调节的功率平均设计方法:脉冲负载的理想供电方案
用于配置系统为脉冲负载供电的功率平均设计方法,帮助设计人员设计体积小、功率密度高且非常高效的系统
一种更加简便高效的方法让您的 LED 运行更加明亮,寿命更持久!
LED 视频墙技术的部署和维护成本高昂。更好的电源设计可以提高性能、效率和长期的成功使用
设计永不失效的快速启动电源应用
快速启动电源系统的运行速度可高达10ms
VITA 62 3U 电源并联运行
VITA 62 电源 270VDC 输入 I2C™通讯
EDN: Vicor 为人工智能和汽车提供动力
APEC 2019 在电源管理方面透露了人工智能的善意提醒
VIA™ 封装 PMBus® 接口和配件用户指南
PMBus® 接口和配件用户指南 (用于适配器型号 I2C-ADAPTER-A02)
GQFN SiP 焊接建议
ECN: 对更小、高性能电源和模块的需求增加
先进的封装可最大限度散热,兼容不同的冷却策略,这对于确保成功部署至关重要
Vinciarelli 博士荣获著名的 2019 IEEE William E.Newell 电力电子奖项
PI358x-00-EVAL1 ZVS 稳压器 30 – 60VIN ZVS 降压评估板用户指南
ZVS 降压和升降压稳压器, 10 x 10mm和10 x 14mm LGA/BGA组件的装配指南
设计军用级别的快速启动电源应用
在战场上,毫秒之间就能决定成败。了解如何设计完美的快速启动电源系统
PFC MicroSTM 功率因数校正 AC-DC 转换器
PFC MicroTM 功率因数校正 AC-DC 转换器
QPI-x-EVAL1
QPO-1-EVAL1
QPO-2-EVAL1
PFC MiniTM 功率因数校正 AC-DC 转换器
QPI-12-CB1-评估板
为何电源设计正在向 48V 转型?
为了为下一代数据中心、电动汽车和人工智能驱动技术供电,各行业正在向 48V 电源转型
为现代铁路应用设计电源系统
本次网络研讨会介绍了为铁路行业开发电源系统的工程师们所面临的市场压力,以及如何克服技术上的挑战的方法
网络研讨会:您的电源系统没有通过传导 EMI 测试 — 现在该怎么办?
本网络研讨会重点介绍帮助快速识别 EMI 测试故障真正来源的技术,以及如何降低其噪声频谱
VIA™ 和 ChiP™ 模块的热管理
面向系留无人机应用的 DCM
NBM2317 SM-ChiP™(非隔离母线转换器模块) 评估板用户指南
组件双面散热时代的散热设计
在缩短设计周期以缩短产品上市时间的同时,也必须满足对更高能效、更高输出和更高密度的需求
电源系统设计人员的逐步安全设计
本文介绍了电源设计人员如何利用这些步骤来消除下一个设计的安全认证压力
Bodos: 处理电源系统设计中的中后期变更
工业整流系统创新方案: 通过固定比率母线转换器实现密集、高效和模块化的架构
介绍并分析了基于固定比率母线转换器的新型 AC-DC 系统架构及其优势和权衡
在并行 DC-DC 转换器阵列中减少不需要的输入拍频
在关键应用中,电源故障可能会造成灾难性的后果。因此,冗余电源系统通常使用 N+1 个类似的转换器来提供非常高的可靠性
Electronic Specifier: 为人工智能计算做准备
Vicor 电源组件如何实现功率平均
随着系统功率水平的提高,许多电源设计人员发现很难保持电源在空间和重量的限制范围内。为平均功率设计电源系统可能是更好的选择
母线转换器在稳压 DC-DC 应用中的使用
FPA™(分比式电源架构™)为解决高要求的功率挑战提供了优势,为解决这些挑战需要高水平效率、功率密度和卓越功率处理和动态负载能力
使用 Yeaman 拓扑消除 PFC 单转换线路纹波
这种拓扑结构的主要特点是将输出电压调节功能与大功率转换功能区分,因为它用于 DC-DC 转换器
PI31xx-xx-EVAL1 ZVS 隔离 DC-DC 转换器评估板
电力元件设计空间中的实用的电磁干扰控制
电源设计的电气安全
本次网络研讨会将提出一系列设计新一代电源时所面向的、必须考虑的安全事项
下一代汽车的动力困境
电动、混合动力、驾驶员辅助系统以及信息娱乐系统正在为汽车制造商创造新的电源需求
缺乏资源和技术导致难以成功交付电源系统项目
未能按时交付设计的主要原因包括:对性能的要求越来越高,以及缺乏工程资源和技术
推荐最大压缩力的散热器
微处理机核电源中不连续导电模式 ZVS 升降压拓扑的控制
在这篇论文中,作者们解决了在实施这种电压调节方案时遇到的设计挑战,这种方案在传统的连续导通模式多相降压拓扑中是看不到的
在热计算中使用电路模型
Vicor 电源组件的散热模型
在热计算中使用电路模型
Vicor 电源组件的散热模型
专为 Micro、Mini、Maxi 转换器、VI-200、MI-200、VI-J00、MI-J00 转换器系列创建高压输出
为什么电源设计转用 48V?
正弦幅度转换器的逆向模式应用
The power electronics industry is seeing the re-emergence of DC high-voltage distribution in place of AC systems of power transmission within advanced machines and installations
如何避免电源系统设计的“隐形成本”
设计您的电源系统成本太高了吗?分比式电源设计可能更昂贵。了解使用模块化方法进行设计的更多好处
PFC MegaPAC-ELTM PFC MegaPAC-HPELTM 功率因数校正 AC-DC 转换器
PFC MegaPACTM 功率因数校正 AC-DC 转换器
HV ChiP BCM® 反向启动电路
合封电源和 3M 演示
Vicor 和 3M 公司演示液浸冷却技术的优势
电源系统设计工具用户指南
IBC™ 的筛选注意事项
微型 DC-DC 转换器系列隔离式远端采样补偿
提升 VI Chip® 母线转换器阵列的轻载效率
使用 FARM AC 前端模块的离线供电
设计 BCM® 预充电电路
Gyoukou 超级计算机采用 48V 分比式电源
观看 ExaScaler/PEZY ZettaScaler-2.2 液浸冷却超级计算机 Gyoukou 的演示
DC MegaPACTM DC-DC 转换器
转换器之间的功率共享简化了光分组传输系统的远程升级
减小电源的重量和尺寸可以增加拴系机器人的有效载荷
AC 输入可替代现有 PBX 系统中的现有 DC 解决方案
分布式天线系统 — PoE
完整的N+1解决方案维护了网络安全AC-DC电源的正常运行时间
高电源效率通过以太网提供可靠的电源
为高科技4K摄像机供电克服了尺寸、重量和电磁干扰要求
在故障状态下,远程无线电设备可以更好地分配通信流量
100%可靠回程通信使用的阵列占用面积只有52.97平方厘米
纤薄的 AC-DC 解决方案允许分布式天线系统在无风扇情况下高温运行
无风扇电源解决方案为天线阵列实现快速、可靠的数据覆盖
4G 远程无线电单元扩展了偏远地区的移动信号覆盖
传导冷却解决方案可实现真正便携的网络测试设备
在更宽的流量范围内工作时,工业流量计更精确
AC-DC 解决方案让防爆相机图像在各种照明条件下变得更加清晰、锐利和精确
Maxi、Mini、Micro 转换器:PR 引脚
使用分比式电源架构改善自动测试设备速度及吞吐量
使用分比式电源架构提高工业焊接激光器的速度和精度
双向 DC-DC 转换器可在电网与家用储电电池之间轻松传输电源
电源解决方案可在极端温度下工作,让LED照明更亮、更持久
高压母线转换器大大降低了户外场馆照明的安装成本
科学仪表可在不影响设备尺寸的情况下,获得两倍的电源
最大限度降低大量布线增加的重量、尺寸和输电损耗,可提高系留无人机的性能
车载广告显示屏启动时减缓电流峰值进程可减轻供电压力
将传统 DC 转换器功能分离,可提高 3D 打印机的速度和精度
母线 Wi-Fi 在恶劣环境下仍可获得高效可靠的供电
一种数码摄影机的解决方案可适应不同的车辆电压
火灾控制单元可在提高功能性的同时,使用 DC-DC 电源及电池备份
可扩展电源解决方案可使船舶仪表在极端环境下工作时保持高精度
为医疗手推车处理各种用户定义的输出电源需求
电源尺寸缩小可让医疗诊断设备在相同的空间中提供更多功能
可扩展电源解决方案可为光学分拣中的各种机器匹配特定的功率
管理电源热量可使轨道信号发送更可靠
使用宽输入输出范围稳压器可提高激光雕刻机的速度、精度、分辨率和对比度
5kW 系留无人机在系线上使用更大的电压,可提高飞行高度和飞行范围
巨大的视频墙显示屏使向支持组件的更高电压母线过渡变得可行
PI31xx 产品系列回流焊指南
助力液压泵产品智能升级,减少扬程浪费
在车载 GPS 应用仅 20% 的空间中功率增加 1/3
使用简单自适应回路反馈的负载点电压精确调节
在高功率阵列中使用 BCM® 母线转换器
VI Chip® BCM® 母线转换器热管理
FPA 印刷电路板布局指南
通孔 ChiP™ 封装焊接指南
VI Chip® DC-DC 转换器模块的滤波网络设计
符合 RoHS 标准的通孔 VI Chip® 焊接建议
SMT J-引脚 VI Chip® 焊接建议
PI3325-00-EVAL1 ZVS 开关稳压器 60VIN 降压客户评估板用户指南
使用 PRM™ 和 VTM™ 提供恒定电流为 LED 供电
MIL EMI 和瞬态解决方案
利用 DCM™ 实现精度高达 ±1% 的电压 (或电流)调节
使用 niPOL 配置 Vicor IBC 转换器
VI-200/VI-J00 和 Maxi、Mini、Micro 转换器的欠压/过压锁定
PCB 安装 VIA 焊接指南
并联 DCM™
均流板
满足军用车辆电气系统瞬态规范
热注意事项:确保Vicor Maxi、Mini、Micro 系列高密度 DC-DC 转换器模块的性能
使用串联正弦幅度转换器产生高压输出
单个 DCM™ 作为隔离、稳压 DC-DC 转换器
Vicor 电源模块的焊接方法和流程
应对军用车辆负载突降引起电压突变的解决方案
支持可变负载的宽范围调节
使用 Maxi, Mini 和 Micro 系列 DC-DC 转换器设计高功率阵列
使用模块化 DC-DC 转换器满足欧洲铁路应用标准
使用功率组件的高效率电池充电器
DC-DC 转换器的恒流控制
可调闭锁输出过流电路
热插拔功能消除停机时间
满足航空航天及国防产品的 SWaP-C 要求
为航空航天与国防设计产品,使我们面临独特的工程挑战
回归基础:选择合适的稳压器
规格的改变是电源设计人员最大的挑战
Vicor 的一项调研显示电源设计师面临着许多挑战。了解它们是什么以及如何克服它们
满足国防应用 DC-DC 电源系统需求
涵盖的主题有:DC-DC 系统助力符合 MIL 标准、达到现在及未来要求的典型应用与测试结果、降低滤波器和布局的噪声、使用针对国防应用优化的电源组件
双向供电设计问题的更多答案
适用于电池应用的电源组件
本网络研讨会解释了如何使用灵活的电源组件可以缩短设计周期,简化电源系统,降低成本,重量和尺寸,同时提高效率
可扩展性:工程师希望了解的更多有关提供更高功率及更高电压的详情
可扩展性:工程师希望了解的更多有关提供更高功率及更高电压的详情
PI352x-0x-EVAL1 ZVS 开关稳压器 60VIN 降压客户评估板
PI3740-00-EVAL1, -EVAL2 ZVS 开关稳压器升降压评估板
高功率 LED 设计的挑战
了解 LED 电源设计会对 LED 性能产生怎样的影响,是长期取得成功的关键
ExaScaler 和 PEZY Computing 推出第一台超级计算机
ExaScaler/PEZY ZettaScaler-1.8 超级计算机突破了计算性能的极限
适用于高电容负载的可扩展、低重量 DC-DC 解决方案
通过将 PCDM 与 DCM 结合使用,我们的客户可以创建一个高度灵活且高效的解决方案以实现其性能和目标的上市时间
电源系统组件式设计方法如何实现优化的 LED 电源系统
设计 LED 电源系统应用的工程师要开发比竞争对手产品更具优势的系统将面临许多挑战
PI3741-0x-EVAL1 ZVS 开关稳压器升降压评估板
让 EMI 问题成为过去的简单构想
本网络研讨会涵盖了电力系统电磁干扰问题的原因
Vicor ZVS 稳压器 => 集成最佳点
开关稳压器解决方案具备不同的集成度,可提供各种性能、功能和封装
设计合适的散热系统的最简单的方式
在许多情况下散热是决定项目可行性的关键,因此需要在设计的早期阶段对这些解决方案进行评估
更低温度电源系统的散热仿真
本次网络研讨会先介绍您需要从产品说明书和应用笔记中收集的信息,然后介绍如何人工执行精确的热计算
最大负载:脉冲功率的误区
本网络研讨会不仅将阐述峰值功率是错误指标的原因所在,而且还将介绍一种不同的技术,即“平均功率”
使用 DC 电源变压器实现双向能量流
了解如何设计双向 DC-DC 电源流设计,以及使用 DC 电源变压器简化电源系统设计等
如何提高大型显示器的效率
由于显示器的每个像素是单独驱动的,因此对用于将 AC 功率转换为驱动 LED 所需的恒定电流的电源系统有着极具挑战性的要求
在噪声敏感、高瞬态应用中,通过实施有源滤波来降低负载电容
28VDC MIL-COTS VIPAC 设计指南
电源系统设计:使用 Vicor 电源系统设计工具节省时间
使用新工具,设计人员在几分钟内就能快速轻松地指定、架构、分析和配置性能优化的完整小型多输出电源系统
电源系统设计:加速上市进程
了解电源元件设计方法如何让加速您的上市进程
使用 DCM 为 HEV/EV 电气系统配电
更先进的混合动力汽车和纯电动汽车增大了对安全接触 12V 电源的需求
开发套装用户指南
PI3749-x0-EVAL1 ZVS 开关稳压器升降压评估板
NBM6123 ChiP™模拟低压非隔离母线转换器模块评估板
PI354X-00 评估板 36V 至 60VIN, 2.5, 3.3, 5.0 和 12VOUT 降压稳压器 & LED 驱动
PMBus® 2361 和 6123 ChiP™ BCM® 母线转换器评估板
7 种缩小电源系统的方法
工程师有几种不同的方法可以减少配电所需的空间
优化整合负载点降压转换器
随着电子产品的复杂程度不断提高,功能设计不断升级,设计人员开发了成熟的电源管理方案
模拟高压及低压 6123 ChiP™ BCM® 母线转换器评估板
采用 DC-DC 转换器为大电容负载供电
DC-DC 转换器输入端电容在保持转换器稳定和输入 EMI 滤波方面起着至关重要的作用
VIPACTM 设计指南
三相 MegaPAC-ELTM (低噪声), 4kW MegaPAC-ELTM (低噪声), AC-DC 转换器
正弦振幅转换器提供了设计灵活性
VTM 和 BCM 使用正弦幅度转换器拓扑结构(SAC)来提供隔离和电压转换功能,从而与调节功能分离
PI33xx: 零电压开关在降压调节中的应用
自动测试设备的配电网络设计
模拟控制 3623 和 4623 ChiP DCM™ 评估板
Vicor 在线工具:模拟器
Vicor 模拟器为我们的一系列产品提供了电能和散热的精确建模,使工程师能够准确了解这些产品在实际应用中的运行情况
Vicor 在线工具:散热计算器
选择散热所需的热量计算相对简单,但可能很耗时,尤其是当您想研究某些参数的变化带来的的影响
全 Chip PRM™-RS 客户评估板
VI Chip® BCM® 评估板
封装技术创新:实现散热面积翻倍
封装创新在提升电源系统性能方面发挥着关键作用
VI Chip® 远端采样补偿 PRM™ 评估板 (用于 PCB 型号 39537 和 38693)
PI33xx-xx-EVAL1 & PI34xx-xx-EVAL1 ZVS 降压稳压器评估板
回归基础:使用自适应环路反馈为转换器输出稳压
与简单的局部控制环路相比,自适应控制环路可提供更好的调节效果 - 误差在 +/-1% 的范围内
高密度电源组件散热测试
令人印象深刻的技术确保了 Vicor 模块的散热设计可在业界领先的功率密度下实现可靠的宽温运行
回归基础:功率因数指什么?为什么一定要校正?
本篇白皮书探讨了可能导致产生破坏性谐波的问题和情况,以及减少谐波的实用方法
高性能电源组件专用测试系统
Vicor 致力于开发测试设备的工程师团队,帮助工程师确保生产线上所有产品的卓越质量
回归基础:如何在多轨电源架构中确保正确的电源时序?
典型的电源时序方法有两种:一种基于电源,另一种基于逻辑
PRM-AL 客户评估板
半 Chip PRM-RS 客户评估板 (用于 PCB 型号 35307)
VI Chip® VTM™ 评估板
回归基础:开关频率的重要性
随着对更高性能的持续需求,CPU、DSP 和其他此类设备的功耗变得越来越高
VI Chip® 高压 BCM® 客户评估板
如何达到欧洲铁路应用标准
观看 Marco 如何介绍满足欧洲铁路标准的 EN50155 和 RIA12
回归基础:什么是 Y 电容器?
Y 电容器的可靠性对于设备用户的安全至关重要
回归基础:零电压开关是什么以及其为何对降压电压调节至关重要?
将基于电容器的电力线滤波设计融入系统能够解耦共模噪声
VI Chip® PRM™ 评估板
有源滤波器控制 EMI、节省 PCB 空间、增强气流
有源滤波器控制 EMI、节省 PCB 空间、增强气流
350 – 12VDC “Yeaman 拓扑” 电源系统
针对单极反馈补偿的双级反馈技术
Vicor 的 PRMTM 模块介绍
本视频介绍了具有用户可配置功能的 Vicor PRM 模块
选择降压稳压器时应考虑哪些因素
需要考虑的关键问题:我的电路板有多少空间?我需要哪些功能?在我的设计中,效率有多重要?
回到基础:理解并降低日益严重的配电损耗问题
DC-DC 转换器和功率转换设备在电力从 PCB 边缘传导到板载组件方面发挥着关键作用
ZVS 降压稳压器介绍
了解简单易用的 PI33XX 系列 ZVS 降压稳压器如何提供高效率、高密度和灵活性
如何使用 24V ZVS 降压评估板
请听 Chester Firek 介绍 ZVS Buck 评估板
热量和机械因素考量
本视频关注效率、热量、传导冷却、对流和辐射。
输出电压微调
本视频介绍了电压微调的好处,即创建非标准输出电压和压控电流源
回归基础:处理高输入瞬态问题
保护系统免受瞬态干扰不仅是开发工作的基本组成部分,也可能成为设计周期中的一大挑战
回归基础:到达 AC-DC 系统的 EMI 标准
EMI 被视为电源转换设计和系统集成的主要挑战之一,对于 AC-DC 系统尤其如此
满足传导噪声标准
找到一款高效、紧凑的解决方案来满足 EMI 要求是一项前所未有的挑战
恒流 (CC) 评估板
为机器人提供最高效的电力
优化 48V 供电
解决 MIL-COTS 应用中的 SWaP-C 电源难题
高性能电源可解决最棘手的问题
为全球提供高速、低延迟网络覆盖的更好方式
提升商用无人机的
有效载荷 力和 行时
军用电源创新:智能、标准化、高效率
Power-supply designers for military applications face the same challenges as other military electronics suppliers
Power Electronic Tips: Vicor 母线转换器获得令人向往的 2019 Leap 奖
Vicor 公司凭借 NBM2317 双向母线转换器模块荣获优秀电源电子产品荣誉
Power Electronic Tips: 提高 48V 配电性能
与 Robert Gendron 的 5 分钟 AI 讨论
在这个播客中,Robert Gendron 讨论了电源与人工智能 (AI)
与 Ian Mazsa 的 5 分钟 AI 讨论
为人工智能系统和 GPU 供电需要什么?
人工智能系统降低能源成本
EDN:2019 的数据中心电源
随着 5G 时代的到来,数据中心的建设与部署以及现有老式数据中心的升级工作正在如火如荼地进行
EDN: 量子计算机中的电源管理
量子计算机很可能成为异构多核计算机不可分割的一部分,其中一个经典处理器将多个加速器以及一个量子协处理器交互
军事和航空电子:军事电力电子寻求增加电压和效率
Vicor 将携全新 VITA 62 产品参加 VPX 展示
VIPAC ArrayTM 设计指南
最新人工智能处理器供电需求
了解一种为人工智能应用供电的全新创新方法,可将主板铜箔和处理器互连电阻锐降 50 倍